Perception [BETA]

Note

This is a BETA feature.

Ouster SDK 1.0 introduces the Ouster Perception API, which includes a detection engine interface and implementation to add objects (i.e. features derived from lidar data) to LidarFrame or FrameSet.

At this time, Ouster SDK includes a single detection engine implementation that performs clustering on the lidar data present in a LidarFrame or FrameSet and adds an Object for each cluster. Future releases will add new engines, including those that do object classification.

Key capabilities

  • Cluster-based object detection: Run the built-in DetectionEngine on live or recorded sources to produce cluster-derived Object instances for each frame.

  • OSF persistence for perception outputs: Save frames, detected objects, and related metadata into OSF for reproducible offline workflows.

  • Metadata-aware datasets: Create and attach metadata such as, class maps, through FrameSetSourceMetadataSet via API, and persist it in OSF; CLI preserves existing metadata during OSF save.

  • Integrated visualization: Inspect detections with ouster-cli ... detect ... viz or in Python using SimpleViz.

You can find the getting started guide for CLI at ouster-cli.

Applications

Common applications for Perception in the SDK include:

  • Rapid obstacle discovery and scene triage: Accelerating early-stage development in robotics prototypes by quickly isolating critical objects.

  • Downstream stack integration: Extracting obstacles, bounding boxes, or clusters to serve as clean inputs for tracking, localization, and path-planning modules.

  • Dataset curation and annotation: Saving model inferences and detections directly within OSF files to streamline downstream labeling and data engineering.

  • Baseline benchmarking and regression testing: Evaluating model performance metrics consistently across historical recordings and diverse physical sensor configurations.

  • Visualization and situational awareness: Overlaying perception data for client demos, remote operator interfaces, and visual QA workflows.

Core concepts

  • Object — a generic object, represented by a bounding box, object_to_body and body_to_world poses, velocity, classification, a timestamp, and user-definable set of properties represented by strings.

  • DetectionConfig — base configuration for detection engines. Subclasses such as ClassicDetectionConfig provide settings for the classic cluster-based engine.

  • DetectionEngine — a base class that declares virtual methods for modifying (e.g. by adding objects to) LidarFrame and FrameSet.

  • ClassMap — A mapping from integers to strings, meant to map Object::class_id to a string description.

  • ClassMapSet — A mapping from strings to ClassMap instances, allowing users to specify different descriptions for Object instances derived from different DetectionEngine.

  • FrameSetSourceMetadataSet — A container for instances of ClassMapSet and other metadata a user may want to associate with a FrameSetSource. Currently, because OSF is the only format that supports LidarFrame and FrameSet, the OsfFrameSetSource is the only implementation that supports metadata.

For detailed type definitions and end-to-end examples, see API workflow for application integration, custom logic, and programmatic control.

For fast iteration, using CLI commands, to dataset generate and vizualize data refer to CLI workflow.

Coordinate Frames

The SDK represents all spatial relationships through a chain of named coordinate frames connected by SE(3) transforms. An SE(3) transform is a 4x4 matrix holding a 3D rotation and a 3D translation; it moves a point from one frame into another without changing the object’s shape or size.

Each transform is named a_to_b, which means it takes a point’s coordinates in frame a and gives them back in frame b. Transforms are combined by multiplying their matrices (right-to-left), so a two-step hop a → b → c is:

\[T_{a}^{c} = T_{b}^{c} \cdot T_{a}^{b}\]

To turn a raw measurement into a world point, the SDK walks the chain lidar → sensor → body → world. Every transform can also be inverted, so you can travel the chain in either direction.

Every edge is either static — a single time-invariant matrix that is the same for every frame in a recording — or dynamic — a timestamped sequence of matrices that is interpolated (spherical-linear for the rotation, linear for the translation) to whatever time you ask for. The four kinds of transform are:

  • Firmware calibrated (static) — the sensor’s internal optics and IMU geometry. These come from the per-unit factory calibration shipped in the sensor metadata, so they are accurate to the individual sensor and never change over its lifetime.

  • Per-mounting configuration (static) — how each sensor is positioned on the platform. Supplied once by the user or a calibration routine, this is the piece that lets several independently-calibrated sensors agree on a single shared body frame; it changes only if the hardware is physically re-mounted.

  • Per-detection snapshot (static) — a detected object’s placement relative to body. Each object stores its own matrix, so the value differs from object to object, but for any single detection it is one fixed pose rather than a trajectory.

  • Dynamic trajectory (dynamic) — the platform’s ego motion through the world frame. This is the only quantity that evolves as the recording plays. LidarFrame::body_to_world stores the full timestamped trajectory, one matrix per lidar column; and Object::body_to_world is a single matrix sampled from that trajectory at the object’s detection timestamp.

SDK pose graph: coordinate frames and transforms

SDK pose graph: coordinate frames and transforms

The key coordinate frames used in this pose graph are:

Frame

Description

beam

Raw lidar optics frame, where each laser beam originates. An internal frame, brought into the lidar frame via beam_to_lidar_transform.

lidar

Lidar measurement frame. A fixed, hardware-calibrated frame defined by the sensor’s internal geometry. Transformed to the sensor housing frame via lidar_to_sensor_transform.

sensor

Sensor housing frame. The external coordinate system of one physical sensor unit. Each sensor on the platform has its own sensor frame, transformed to the shared body frame via its own sensor_to_body (per mounting configuration).

imu

IMU measurement frame. Related to the sensor frame by the fixed imu_to_sensor_transform.

body

The single common reference frame shared by all sensors mounted on the platform; measurements from every sensor are fused here.

object

Object-local bounding box frame. The origin is at the center of the detected object’s bounding box, with axes aligned to the object’s principal directions. object_to_body is a per-detection snapshot: fixed for a given Object instance but different across frames as the object moves relative to body.

world

Sequence-local world frame. A fixed reference frame for a recording session; typically the body frame at the start of the sequence. The dynamic body_to_world trajectory expresses the ego-vehicle pose in this frame over time. It stores one SE(3) per lidar column (not just one per frame) because the vehicle keeps moving during the lidar’s sweep (one full frame, e.g. ~100 ms at 10 Hz); using the right per-column pose removes that motion smear — a step known as dewarping (see Motion Compensation).

All of these frames are right-handed. For the exact axis directions and origins of the Ouster sensor, lidar, and imu frames, see the Ouster sensor coordinate frame documentation .

Where poses are stored

Transforms are owned by three data structures:

  • SensorInfo (one per sensor): lidar_to_sensor_transform, imu_to_sensor_transform, and sensor_to_body.

  • LidarFrame: dynamic body_to_world() ego trajectory, one SE(3) per lidar column (shape (w, 4, 4)).

  • Object: per-detection object_to_body and body_to_world. body_to_world is sampled from LidarFrame at Object.timestamp, making each object self-contained.

Object world pose is computed by composing the two Object pose fields (both stored on the Object itself):

\[T_{\text{object}}^{\text{world}} = T_{\text{body}}^{\text{world}} \cdot T_{\text{object}}^{\text{body}}\]

In code: object_in_world = object.body_to_world * object.object_to_body

The velocity field of an Object is expressed in the world frame.