ouster.sdk.osf

Module contents

Copyright (c) 2021, Ouster, Inc. All rights reserved.

This module provides an API for working with OSF (Ouster Sensor Format) files. It includes tools for reading, writing, slicing, encoding, and modifying OSF files and their metadata.

Classes

Functions

AsyncWriter

class AsyncWriter(self, filename: str, info: collections.abc.Sequence[ouster.sdk.core.SensorInfo], fields_to_write: collections.abc.Sequence[str] = [], chunk_size: int = 0, encoder: ouster.sdk.osf.Encoder | None = None)

Creates an AsyncWriter with specified chunk_size.

Default chunk_size is 2MB.

Parameters:
  • filename (str) – The filename to output to.

  • info (List[SensorInfo]) – The sensor info vector to use for a multi stream OSF file.

  • fields_to_write (List[str]) – The fields from frames to actually save into the OSF. If not provided uses the fields from the first saved lidar frame for each stream. This parameter is optional.

  • chunk_size (int) – The chunksize to use for the OSF file, this arg is optional.

  • encoder (Encoder) – an optional encoder instance, used to configure how writer encodes the OSF.

__enter__(self) → ouster.sdk.osf.AsyncWriter

Allow AsyncWriter to work within with blocks.

__exit__(self, exc_type: object | None, exc_value: object | None, traceback: object | None) → object

Allow AsyncWriter to work within with blocks.

__init__(self, filename: str, info: collections.abc.Sequence[ouster.sdk.core.SensorInfo], fields_to_write: collections.abc.Sequence[str] = [], chunk_size: int = 0, encoder: ouster.sdk.osf.Encoder | None = None) → None

Creates an AsyncWriter with specified chunk_size.

Default chunk_size is 2MB.

Parameters:
  • filename (str) – The filename to output to.

  • info (List[SensorInfo]) – The sensor info vector to use for a multi stream OSF file.

  • fields_to_write (List[str]) – The fields from frames to actually save into the OSF. If not provided uses the fields from the first saved lidar frame for each stream. This parameter is optional.

  • chunk_size (int) – The chunksize to use for the OSF file, this arg is optional.

  • encoder (Encoder) – an optional encoder instance, used to configure how writer encodes the OSF.

__module__ = 'ouster.sdk.osf'
__new__(**kwargs)
close(self, fsync: bool = False) → None

Finish OSF file and flush everything to disk.

Encoder

class Encoder(self, lidar_frame_encoder: LidarFrameEncoder)
class Encoder(self, *, lidar_scan_encoder: LidarFrameEncoder)

Used by the Writer class to encode LidarFrames, depending on configuration.

__init__(self, lidar_frame_encoder: LidarFrameEncoder) → None
__init__(self, *, lidar_scan_encoder: LidarFrameEncoder) → None
__module__ = 'ouster.sdk.osf'
__new__(**kwargs)

LidarFrameStream

class LidarFrameStream

Stream of LidarFrame objects from a sensor.

type_id static property is a LidarFrameStream underlying metadata type identifier.

__annotations__ = {'meta': 'LidarFrameStreamMeta', 'type_id': 'str'}
__init__(*args, **kwargs)
__module__ = 'ouster.sdk.osf'
__new__(**kwargs)
property meta: LidarFrameStreamMeta

metadata entry to store LidarFrameStream metadata in an OSF file

type_id: str = 'ouster/v1/os_sensor/LidarScanStream'

LidarSensor

class LidarSensor(self, arg: ouster.sdk.core.SensorInfo, /)
class LidarSensor(self, metadata_json: str)

Ouster Lidar Sensor metadata with sensor intrinsics (i.e. SensorInfo/Metadata)

type_id static property is a LidarSensor metadata type identifier.

Overloaded function.

  1. __init__(self, arg: ouster.sdk.core.SensorInfo, /) -> None

Create from SensorInfo object

  1. __init__(self, metadata_json: str) -> None

Create from metadata_json string representation

__annotations__ = {'info': 'ouster.sdk.core.SensorInfo', 'metadata': 'str', 'type_id': 'str'}
__init__(self, arg: ouster.sdk.core.SensorInfo, /) → None
__init__(self, metadata_json: str) → None

Overloaded function.

  1. __init__(self, arg: ouster.sdk.core.SensorInfo, /) -> None

Create from SensorInfo object

  1. __init__(self, metadata_json: str) -> None

Create from metadata_json string representation

__module__ = 'ouster.sdk.osf'
__new__(**kwargs)
property info: ouster.sdk.core.SensorInfo

SensorInfo stored

property metadata: str

metadata_json string stored

type_id: str = 'ouster/v1/os_sensor/LidarSensor'

OsfDropFrameError

class OsfDropFrameError
__module__ = 'ouster.sdk.osf'
__weakref__

list of weak references to the object

OsfFrameSetSource

class OsfFrameSetSource(self, file: str, **kwargs)
__annotations__ = {'is_collated': 'bool'}
__init__(self, file: str, **kwargs) → None
__module__ = 'ouster.sdk.osf'
__new__(**kwargs)
property is_collated: bool

(self) -> bool

PngLidarFrameEncoder

class PngLidarFrameEncoder(self, compression_amount: int)

Used by the Writer class to encode LidarFrames using PNG compression.

__init__(self, compression_amount: int) → None
__module__ = 'ouster.sdk.osf'
__new__(**kwargs)

Reader

class Reader(self, file: str)
class Reader(self, file: str, error_handler: collections.abc.Callable[[ouster.sdk.core.Severity, str], None] | None = None)

Reader is a main entry point to get any info out of OSF file.

__annotations__ = {'end_ts': 'int', 'has_message_idx': 'bool', 'has_stream_info': 'bool', 'has_timestamp_idx': 'bool', 'meta_store': 'MetadataStore', 'metadata_id': 'str', 'size': 'int', 'start_ts': 'int', 'version': 'ouster.sdk.core.Version'}
__dict__ = mappingproxy({'__new__': <built-in method __new__ of nanobind.nb_type_0 object>, '__init__': <nanobind.nb_method object>, '__dict__': <attribute '__dict__' of 'ouster.sdk.osf.Reader' objects>, '__doc__': '\n        Reader is a main entry point to get any info out of OSF file.\n    ', '__module__': 'ouster.sdk.osf', 'metadata_id': <property object>, 'start_ts': <property object>, 'end_ts': <property object>, 'size': <property object>, 'version': <property object>, 'meta_store': <property object>, 'has_stream_info': <property object>, 'has_message_idx': <property object>, 'has_timestamp_idx': <property object>, 'messages': <nanobind.nb_method object>, 'ts_by_message_idx': <nanobind.nb_method object>, 'chunks': <nanobind.nb_method object>, '__annotations__': {'metadata_id': 'str', 'start_ts': 'int', 'end_ts': 'int', 'size': 'int', 'version': 'ouster.sdk.core.Version', 'meta_store': 'MetadataStore', 'has_stream_info': 'bool', 'has_message_idx': 'bool', 'has_timestamp_idx': 'bool'}})
__init__(self, file: str) → None
__init__(self, file: str, error_handler: collections.abc.Callable[[ouster.sdk.core.Severity, str], None] | None = None) → None
__module__ = 'ouster.sdk.osf'
__new__(**kwargs)
chunks(self) → collections.abc.Iterator[ouster.sdk.osf.ChunkRef]

Creates an iterator to reads chunks as they appear in a file.

property end_ts: int

End timestamp (ns) - the highest message timestamp present in the file

property has_message_idx: bool

Whether OSF contains the message counts that are needed for ts_by_message_idx() (message counts was added a bit later to the OSF core, so this function will be obsolete over time)

property has_stream_info: bool

Whether StreamingInfo metadata is available (i.e. reading messages by timestamp and streams can be performed)

property has_timestamp_idx: bool

Whether OSF contains the message timestamp index in the metadata necessary to quickly collate and jump to a specific message time.

messages(self) → collections.abc.Iterator[ouster.sdk.osf.MessageRef]
messages(self, start_ts: int, end_ts: int) → collections.abc.Iterator[ouster.sdk.osf.MessageRef]
messages(self, stream_ids: collections.abc.Sequence[int] = []) → collections.abc.Iterator[ouster.sdk.osf.MessageRef]
messages(self, stream_ids: collections.abc.Sequence[int], start_ts: int, end_ts: int) → collections.abc.Iterator[ouster.sdk.osf.MessageRef]

Overloaded function.

  1. messages(self) -> collections.abc.Iterator[ouster.sdk.osf.MessageRef]

    Creates an iterator to read messages in default STREAMING layout.

  2. messages(self, start_ts: int, end_ts: int) -> collections.abc.Iterator[ouster.sdk.osf.MessageRef]

    Read messages in [start_ts, end_ts] timestamp range (inclusive)

  3. messages(self, stream_ids: collections.abc.Sequence[int] = []) -> collections.abc.Iterator[ouster.sdk.osf.MessageRef]

    Read messages from only specified [<stream_ids>] list

  4. messages(self, stream_ids: collections.abc.Sequence[int], start_ts: int, end_ts: int) -> collections.abc.Iterator[ouster.sdk.osf.MessageRef]

    Read messages in [start_ts, end_ts] timestamp range (inclusive) of a specified <stream_ids> list

property meta_store: MetadataStore

Returns the metadata store that gives an access to all metadata entries in the file.

property metadata_id: str

Data id string

property size: int

Size of the OSF file in bytes

property start_ts: int

Start timestamp (ns) - the lowest message timestamp present in the file

ts_by_message_idx(self, stream_id: int, message_idx: int) → object

Find the timestamp of the message by its index and stream_id.

Requires the OSF with message_counts inside, i.e. has_message_idx() is True, otherwise return value is always None.

property version: ouster.sdk.core.Version

Version of OSF file format in the file

Writer

class Writer(self, file_name: str, chunk_size: int = 0)
class Writer(self, filename: str, info: ouster.sdk.core.SensorInfo, fields_to_write: collections.abc.Sequence[str] = [], chunk_size: int = 0, encoder: ouster.sdk.osf.Encoder | None = None)
class Writer(self, filename: str, info: collections.abc.Sequence[ouster.sdk.core.SensorInfo], fields_to_write: collections.abc.Sequence[str] = [], chunk_size: int = 0, encoder: ouster.sdk.osf.Encoder | None = None)

Simple writer interface for OSF file

All jobs are done with MetadataStore for adding metadata entries and stream interfaces that encodes messages and passes them to internal chunks writer.

Overloaded function.

  1. __init__(self, file_name: str, chunk_size: int = 0) -> None

    Creates a Writer with specified chunk_size.

    Default chunk_size is 2 MB.

  2. __init__(self, filename: str, info: ouster.sdk.core.SensorInfo, fields_to_write: collections.abc.Sequence[str] = [], chunk_size: int = 0, encoder: ouster.sdk.osf.Encoder | None = None) -> None

    Creates a Writer with deafault STREAMING layout chunks writer.

    Using default chunk_size of 2MB.

    Args:

    filename (str): The filename to output to. info (SensorInfo): The sensor info vector to use for a multi stream OSF

    file.

    chunk_size (int): The chunk size in bytes to use for the OSF file. This arg

    is optional, and if not provided the default value of 2MB is used. If the current chunk being written exceeds the chunk_size, a new chunk will be started on the next call to save. This allows an application to tune the number of messages (e.g. lidar frames) per chunk, which affects the granularity of the message index stored in the StreamingInfo in the file metadata. A smaller chunk_size means more messages are indexed and a larger number of index entries. A more granular index allows for more precise seeking at the slight expense of a larger file.

    fields_to_write (List[str]): The fields from frames to

    actually save into the OSF. If not provided uses the fields from the first saved lidar frame for each stream. This parameter is optional.

  3. __init__(self, filename: str, info: collections.abc.Sequence[ouster.sdk.core.SensorInfo], fields_to_write: collections.abc.Sequence[str] = [], chunk_size: int = 0, encoder: ouster.sdk.osf.Encoder | None = None) -> None

    Creates a Writer with specified chunk_size.

    Default chunk_size is 2MB.

    Args: filename (str): The filename to output to. info (List[SensorInfo]): The sensor info vector to use for a

    multi stream OSF file.

    fields_to_write (List[str]): The fields from frames to

    actually save into the OSF. If not provided uses the fields from the first saved lidar frame for each stream. This parameter is optional.

    chunk_size (int): The chunksize to use for the OSF file, this arg

    is optional.

__annotations__ = {'meta_store': 'MetadataStore'}
__enter__(self) → ouster.sdk.osf.Writer

Allow Writer to work within with blocks.

__exit__(self, exc_type: object | None, exc_value: object | None, traceback: object | None) → object

Allow Writer to work within with blocks.

__init__(self, file_name: str, chunk_size: int = 0) → None
__init__(self, filename: str, info: ouster.sdk.core.SensorInfo, fields_to_write: collections.abc.Sequence[str] = [], chunk_size: int = 0, encoder: ouster.sdk.osf.Encoder | None = None) → None
__init__(self, filename: str, info: collections.abc.Sequence[ouster.sdk.core.SensorInfo], fields_to_write: collections.abc.Sequence[str] = [], chunk_size: int = 0, encoder: ouster.sdk.osf.Encoder | None = None) → None

Overloaded function.

  1. __init__(self, file_name: str, chunk_size: int = 0) -> None

    Creates a Writer with specified chunk_size.

    Default chunk_size is 2 MB.

  2. __init__(self, filename: str, info: ouster.sdk.core.SensorInfo, fields_to_write: collections.abc.Sequence[str] = [], chunk_size: int = 0, encoder: ouster.sdk.osf.Encoder | None = None) -> None

    Creates a Writer with deafault STREAMING layout chunks writer.

    Using default chunk_size of 2MB.

    Args:

    filename (str): The filename to output to. info (SensorInfo): The sensor info vector to use for a multi stream OSF

    file.

    chunk_size (int): The chunk size in bytes to use for the OSF file. This arg

    is optional, and if not provided the default value of 2MB is used. If the current chunk being written exceeds the chunk_size, a new chunk will be started on the next call to save. This allows an application to tune the number of messages (e.g. lidar frames) per chunk, which affects the granularity of the message index stored in the StreamingInfo in the file metadata. A smaller chunk_size means more messages are indexed and a larger number of index entries. A more granular index allows for more precise seeking at the slight expense of a larger file.

    fields_to_write (List[str]): The fields from frames to

    actually save into the OSF. If not provided uses the fields from the first saved lidar frame for each stream. This parameter is optional.

  3. __init__(self, filename: str, info: collections.abc.Sequence[ouster.sdk.core.SensorInfo], fields_to_write: collections.abc.Sequence[str] = [], chunk_size: int = 0, encoder: ouster.sdk.osf.Encoder | None = None) -> None

    Creates a Writer with specified chunk_size.

    Default chunk_size is 2MB.

    Args: filename (str): The filename to output to. info (List[SensorInfo]): The sensor info vector to use for a

    multi stream OSF file.

    fields_to_write (List[str]): The fields from frames to

    actually save into the OSF. If not provided uses the fields from the first saved lidar frame for each stream. This parameter is optional.

    chunk_size (int): The chunksize to use for the OSF file, this arg

    is optional.

__module__ = 'ouster.sdk.osf'
__new__(**kwargs)
add_metadata(self, m: object) → int

Add metadata entry to a file

add_sensor(self, info: ouster.sdk.core.SensorInfo, fields_to_write: collections.abc.Sequence[str] = []) → int

Add a sensor to the OSF file.

Parameters:
  • info (SensorInfo) – Sensor to add.

  • fields_to_write (List[str]) – The fields from frames to actually save into the OSF. If not provided uses the fields from the first saved lidar frame for each stream. This parameter is optional.

Returns (int):

The stream index to use to write frames to this sensor.

close(self, fsync: bool = False) → None

Finish OSF file and flush everything to disk.

filename(self) → str

Return the osf file name.

Returns (str):

The OSF filename.

is_closed(self) → bool

Return the closed status of the writer.

Returns (bool):

The closed status of the writer.

property meta_store: MetadataStore

Returns the metadata store that gives an access to all metadata entries in the file.

metadata_id(self) → str

Return the metadata identifier string.

Returns (str):

The OSF metadata identifier string.

save_message(self, stream_id: int, receive_ts: int, sensor_ts: int, buffer: ndarray[dtype=uint8], type: str) → None
save_message(self, stream_id: int, receive_ts: int, sensor_ts: int, buffer: bytes, type: str) → None
save_message(self, stream_id: int, receive_ts: int, sensor_ts: int, buffer: collections.abc.Sequence[int], type: str) → None

Overloaded function.

  1. save_message(self, stream_id: int, receive_ts: int, sensor_ts: int, buffer: ndarray[dtype=uint8], type: str) -> None

    Low-level save message routine.

    Directly saves the message buffer with id and ts (ns) without any further checks.

  2. save_message(self, stream_id: int, receive_ts: int, sensor_ts: int, buffer: bytes, type: str) -> None

    Low-level save message routine.

    Directly saves the message buffer with id and ts (ns) without any further checks.

  3. save_message(self, stream_id: int, receive_ts: int, sensor_ts: int, buffer: collections.abc.Sequence[int], type: str) -> None

    Low-level save message routine.

    Directly saves the message buffer (from a Python list) with id and ts (ns).

sensor_info(self) → list[ouster.sdk.core.SensorInfo]

Return the sensor info list.

Returns (List[SensorInfo]):

The sensor info list.

set_metadata_id(self, arg: str, /) → None

Set the metadata identifier string.

ZPngLidarFrameEncoder

class ZPngLidarFrameEncoder(self, compression_amount: int)

Used by the Writer class to encode LidarFrames using ZPNG compression.

__annotations__ = {}
__init__(self, compression_amount: int) → None
__module__ = 'ouster.sdk.osf'
__new__(**kwargs)

backup_osf_file_metablob

backup_osf_file_metablob(file: str, backup_file_name: str) → int

Backup the metadata blob in an OSF file.

File:

OSF file path (v1/v2)

Backup_file_name:

Backup path

dump_metadata

dump_metadata(file: str, full: bool = True) → str

Dump OSF metadata/session info in JSON format. (aka osf-metadata)

File:

OSF file path

Returns:

JSON formatted string of OSF metadata + header info

osf_file_modify_metadata

osf_file_modify_metadata(file_name: str, new_metadata: collections.abc.Sequence[ouster.sdk.core.SensorInfo]) → int

Modify an OSF files sensor_info metadata.

File_name:

The OSF file to modify.

New_metadata:

Array containing sensor infos to write to the file.

Returns:

The number of the bytes written to the OSF file.

restore_osf_file_metablob

restore_osf_file_metablob(file: str, backup_file_name: str) → int

Restore an OSF metadata blob from a backup file.

File:

OSF file path (v1/v2)

Backup_file_name:

The backup to use

slice_and_cast

slice_and_cast(*args, **kwargs)
slice_and_cast(lidar_frame: ouster.sdk.core.LidarFrame, field_types: collections.abc.Mapping[str, object]) → ouster.sdk.core.LidarFrame

Copies LidarFrame with new field types

Parameters:
  • args (Any)

  • kwargs (Any)

Return type:

Any