Lidar and IMU Packets¶
The core.PacketSource (previously PacketMultiSource) is the basic interface for sensor packets
and returns Tuple[int, Packet]. It can be advantageous to work with packets directly when latency is a
concern, or when you wish to examine the data packet by packet, e.g., if you wish to examine timestamps of packets.
Let’s make a core.PacketSource from our sample data using pcap.PcapPacketSource:
from ouster.sdk import pcap
source = pcap.PcapPacketSource(pcap_path)
for _, packet in source:
... # a list of packets, with (sensor_idx, Packet)
See FrameSetSource for more details on working with packets.
Now we can read lidar data packets from source with the following code:
# open source
source = pcap.PcapPacketSource(source_file)
metadata = source.sensor_info[0]
packet_format = core.PacketFormat(metadata)
for idx, packet in source:
if isinstance(packet, core.LidarPacket):
# Now we can process the LidarPacket. In this case, we access
measurement_ids = packet_format.packet_header(core.ColHeader.MEASUREMENT_ID, packet.buf)
timestamps = packet_format.packet_header(core.ColHeader.TIMESTAMP, packet.buf)
ranges = packet_format.packet_field(core.ChanField.RANGE, packet.buf)
print(f' encoder counts = {measurement_ids.shape}')
print(f' timestamps = {timestamps.shape}')
print(f' ranges = {ranges.shape}')
And IMU packets can be read as follows:
elif isinstance(packet, core.ImuPacket):
# and access ImuPacket content
ax = packet_format.imu_la_x(packet.buf)
ay = packet_format.imu_la_y(packet.buf)
az = packet_format.imu_la_z(packet.buf)
wx = packet_format.imu_av_x(packet.buf)
wy = packet_format.imu_av_y(packet.buf)
wz = packet_format.imu_av_z(packet.buf)
print(f' acceleration = {ax}, {ay}, {az}')
print(f' angular_velocity = {wx}, {wy}, {wz}')
You can try the above code with the pcap_read_packets():
$ python3 -m ouster.sdk.examples.pcap $SAMPLE_DATA_PCAP_PATH read-packets
PS > py -3 -m ouster.sdk.examples.pcap $SAMPLE_DATA_PCAP_PATH read-packets