C++

Building the example code requires a compiler supporting C++14 and CMake 3.10 or newer and the Eigen3 and tins libraries with headers installed on the system. The sample visualizer also requires the GLFW3 library.

The C++ example code is available on the Ouster Github . Follow the instructions for cloning the project.

Building on Linux / macOS

Installation with apt or brew

To install build dependencies on Ubuntu:20.04+, run:

$ sudo apt install build-essential cmake libeigen3-dev libcurl4-openssl-dev \
                   libtins-dev libpcap-dev libglfw3-dev libpng-dev \
                   libflatbuffers-dev libceres-dev libtbb-dev libssl-dev \
                   libzip-dev libzstd-dev \
                   zlib1g-dev

You may also install curl with a different ssl backend, for example libcurl4-gnutls-dev or libcurl4-nss-dev.

On macOS, install XCode and homebrew and run:

$ brew install cmake pkg-config eigen curl libtins glfw libpng flatbuffers libomp ceres-solver openssl@3 tbb zstd libzip zlib

To build on macOS and Ubuntu:20.04+ run the following commands:

$ mkdir build
$ cd build
$ cmake  <path to ouster-sdk/CMakeLists.txt> -DCMAKE_BUILD_TYPE=Release -DBUILD_EXAMPLES=ON
$ cmake --build . -- -j$(nproc)

where <path to ouster-sdk> is the location of the ouster-sdk source directory. The CMake build script supports several optional flags. Add any of the following to override the defaults:

-DBUILD_VIZ=OFF                    # Do not build the sample visualizer
-DBUILD_PCAP=OFF                   # Do not build pcap tools
-DBUILD_OSF=OFF                    # Do not build OSF lib
-DBUILD_EXAMPLES=ON                # Build C++ examples
-DBUILD_TESTING=ON                 # Build tests
-DBUILD_SHARED_LIBRARY=ON          # Build the shared library and binary artifacts

Building on Windows

The example code can be built on Windows 10 with Visual Studio 2019 using CMake support and vcpkg for dependencies. Follow the official documentation to set up your build environment:

Since, VCPKG_MANIFEST_MODE is set to ON, the dependencies will be installed the build if the CMAKE_TOOLCHAIN_FILE is set correctly.

PS > $env:CMAKE_TOOLCHAIN_FILE="<PATH TO VCPKG REPO>\scripts\buildsystems\vcpkg.cmake"

Remember to run,

PS > .\vcpkg.exe integrate install

Note: The commit sha in vcpkg.json ensures that the correct version of vcpkg and dependencies are installed. Currently, we are using the release commit on 2025.02.14.

Don’t forget to integrate vcpkg with Visual Studio after bootstrapping:

PS > .\vcpkg.exe integrate install

After these steps are complete, you should be able to open, build and run the ouster-sdk project using Visual Studio:

  1. Start Visual Studio.

  2. When the prompt opens asking you what type of project to open click Open a local folder and navigate to the ouster-sdk source directory.

  3. After opening the project for the first time, wait for CMake configuration to complete.

  4. Make sure the Desktop development with C++ is installed. If not, install it using the Search bar on the top of the screen.

  5. Make sure Visual Studio is building in release mode . You may experience performance issues and missing data in the visualizer otherwise.

  6. In the menu bar at the top of the screen, select Build > Build All.

  7. To use the resulting binaries, go to View > Terminal and run, for example:

.\out\build\x64-Release\examples\client_example.exe

Running the Sample Client

Make sure the sensor is connected to the network. See “Connecting to the Sensor” in the Software User Manual for instructions and different options for network configuration.

Navigate to examples under the build directory, which should contain an executable named client_example. This program will attempt to connect to the sensor, capture lidar data, and write point clouds out to CSV files:

$ ./client_example <sensor hostname> <udp data destination>

where <sensor hostname> can be the hostname (os-99xxxxxxxxxx) or IP of the sensor and <udp data destination> is the hostname or IP to which the sensor should send lidar data. You can also supply "", an empty string, to utilize automatic detection.

On Windows, you may need to allow the client/visualizer through the Windows firewall to receive sensor data.

Building Against The Library

Navigate to examples under the ouster-sdk source directory, which should contain several linux example folders building against the sdk library. To run each use the example.bash script.

  1. compiled_in_linking_example - Compile ouster_sdk as a sub-project under a larger codebase.

  2. static_linking_example - Use installed static libs of ouster_sdk under a larger codebase.

  3. shared_linking_example - Use installed shared libs of ouster_sdk under a larger codebase.

Troubleshooting

You may encounter errors if vcpkg on your system is using an outdated version while building in manifest mode. A common error in this case is Baseline not found.

To resolve this, update vcpkg to the latest commit on the master branch.