Python¶
Building the Python SDK from source requires several dependencies:
a C++14-capable compiler
cmake >= 3.16
eigen >= 3.3
curl >= 7.58
libtins >= 3.4
libpng >= 1.6
flatbuffers == 24.3.25
libglfw3 >= 3.2
ceres == 2.0.0
python >= 3.8; <= 3.13 (with headers and development libraries)
nanobind == 2.9.2
The Python SDK source is available on the Ouster Github . You should clone the whole project.
Linux and macOS¶
It is now recommended to use vcpkg to install dependencies across all platforms.
The list of required dependencies is defined in the vcpkg.json file located at the root of the repository.
vcpkg manifest mode is used to manage ouster-sdk dependencies in a consistent and reproducible way.
To install vcpkg, please follow the instructions in the vcpkg documentation .
The setup.py sets the following environment variables to point to the vcpkg installation,
please make sure to update them if want to update location of vcpkg.json file:
$ export VCPKG_MANIFEST_DIR=<PATH TO OUSTER_SDK REPO>
$ export VCPKG_MANIFEST_MODE=ON
As an alternative, you can install the dependencies manually using following instructions:
On supported Debian-based Linux systems,
$ sudo apt install build-essential cmake libeigen3-dev libcurl4-openssl-dev \
libtins-dev libpcap-dev libglfw3-dev libpng-dev \
libflatbuffers-dev libceres-dev libtbb-dev libssl-dev \
libzip-dev libzstd-dev \
zlib1g-dev
On macOS >= 14, using Homebrew, you should be able to run:
$ brew install cmake pkg-config eigen curl libtins glfw libpng flatbuffers libomp ceres-solver openssl@3 tbb zstd libzip zlib
You can build the SDK with:
# first, specify the path to the ouster-sdk repository
$ export OUSTER_SDK_PATH=<PATH TO OUSTER_SDK REPO>
# make sure you have an up-to-date version of pip and setuptools installed
$ python3 -m pip install --user --upgrade pip setuptools
# install nanobind
$ python3 -m pip install nanobind
# then, build an installable "wheel" package
$ python3 -m pip wheel --no-deps $OUSTER_SDK_PATH/python
# or just install directly (virtualenv recommended)
$ python3 -m pip install $OUSTER_SDK_PATH/python
Note
We recommend to always use Virtual Environment for python development.
Windows 10¶
As mentioned, vcpkg is the recommended package manager for `ouster-sdk.
Please follow the instructions in the vcpkg documentation powershell to install vcpkg.
Additionally, ensure that the following are installed on your system:
Visual Studio 2017 Build Tools
Python
After that, using a developer powershell prompt:
# first, specify the path to the ouster-sdk repository
PS > $env:OUSTER_SDK_PATH="<PATH TO OUSTER_SDK>"
# point cmake to the location of vcpkg (make sure to use an absolute path)
PS > $env:CMAKE_TOOLCHAIN_FILE="<PATH TO VCPKG REPO>\scripts\buildsystems\vcpkg.cmake"
# set the correct vcpkg triplet
PS > $env:VCPKG_TARGET_TRIPLET="x64-windows"
# set build options related to the compiler
PS > $env:CMAKE_GENERATOR_PLATFORM="x64"
PS > $env:CMAKE_GENERATOR="Visual Studio 15 2017"
# install nanobind
PS > py -m pip install nanobind ninja
Optionally, if you want to update the default settings of directory for the manifest file or disable manifest mode, update the environment variables below:
PS > $env:VCPKG_MANIFEST_DIR=<PATH TO OUSTER_SDK REPO>
PS > $env:VCPKG_MANIFEST_MODE=ON
Then, you can build the SDK with:
# then, build an installable "wheel" package
PS > py -m pip wheel --no-deps "$env:OUSTER_SDK_PATH\python"
# or just install directly (virtualenv recommended)
PS > py -m pip install "$env:OUSTER_SDK_PATH\python"
See the top-level README in the Ouster SDK repository for more details on setting up a development environment on Windows.
Developing¶
Install in editable mode with pip using pip install -e. For a faster development cycle, you can
rebuild using python3 setup.py build_ext -i instead of reinstalling the package after every
change. For a local debug build, you can also add the -g flag.
The Ouster SDK package includes configuration for flake8 and mypy. To run:
# install nanobind
$ python3 -m pip install nanobind
# install and run flake8 linter
$ python3 -m pip install flake8
$ cd ${OUSTER_SDK_PATH}/python
$ python3 -m flake8
# install and run mypy in an environment with
$ python3 -m pip install mypy
$ python3 -m mypy src/
Running Tests¶
To run tests while developing, install the pytest package and run it from the root of the Python
SDK package:
$ cd ${OUSTER_SDK_PATH}/python
$ python3 -m pytest
To run interactive viz.PointViz tests, use --interactive argument:
$ cd ${OUSTER_SDK_PATH}/python
$ python3 -m pytest --interactive
To run tests against multiple Python versions simultaneously, use the tox package:
$ cd ${OUSTER_SDK_PATH}/python
$ python3 -m tox
This will take longer, since it will build the package from a source distribution for each supported Python version available.