Skip to navigation

Get the system network configuration

Get the system network configuration

Response

System network configuration
carrierbooleanOptional

State of Ethernet link, true when physical layer is connected

duplexenumOptional

Duplex mode of Ethernet link, half or full

Allowed values:
ethaddrstringOptionalformat: "macAddress"

Ethernet hardware (MAC) address.

hostnamestringOptional
Hostname of the sensor, also used when requesting DHCP address and registering mDNS hostname
ipv4objectOptional
ipv6objectOptional
speeddoubleOptional
Ethernet physical layer speed in Mbps, should be 1000 Mbps
mtuintegerOptional
Current ethernet MTU in bytes.
mtu_overrideinteger or nullOptional

Persisted ethernet MTU override in bytes. null when unset.