Get specific Multipurpose IO (MIO) channel state
Get specific Multipurpose IO (MIO) channel state
Get the current state of a specific Multipurpose IO (MIO) hardware channel by its index. Each channel has aliases and will be configured as input or disabled.
Operations to configure and query Multipurpose IO (MIO) hardware channels. MIO provides configurable input/output functionality for external hardware integration, supporting both individual channel configuration and bulk operations using bitmasks.
Path parameters
channel_id
Channel index (0 or 1)
Response
Multipurpose IO hardware state for specific channel
aliases
Alternative names for the channel
input
Current input state of the channel (read-only).
enable
Whether the channel is enabled for MIO operation.
config
Current channel configuration mode. 'OTHER' indicates the channel is not available for MIO operation. If enable is not set and config is OTHER, the channel is used by another service.
Allowed values:
Errors
404
Not Found Error
500
Internal Server Error