Get custom profile configuration
Returns the udp_profile_lidar_custom configuration as a CustomProfile
object from the requested config source. Defaults to staged. Returns
null when no custom profile is configured.
Query parameters
source
Config source to read from.
Allowed values:
Response
Custom profile configuration, or null when none
n_words
Number of 32-bit output words in the custom profile.
fields
Placed fields within the custom profile word layout.
Errors
400
Bad Request Error
500
Internal Server Error