Get factory profile layout template
Returns the factory pixel assembler field layout for a built-in UDP lidar
profile via keeper command get_active_asm_config {profile}. Use this as a
starting template when authoring a custom profile. CUSTOM is not a valid
template. Returns a CustomProfile object or null when unavailable.
In mock/recovery mode returns null.
Path parameters
udp_profile_lidar
Built-in UDP lidar profile name (alphanumeric and underscore only), e.g. RNG15_RFL8_NIR8.
Response
Factory layout template for the requested profile, or null when unavailable
n_words
Number of 32-bit output words in the custom profile.
fields
Placed fields within the custom profile word layout.
Errors
400
Bad Request Error
500
Internal Server Error