ouster.sdk.util.pose_util module¶
- no_scipy()[source]¶
Checks the scipy availability with a warning message. :rtype:
bool- Return type:
bool
- exp_rot_vec(vec)[source]¶
Converts so3 vector to a rotation matrix.
- Parameters:
vec (
ndarray) – so3 rotation vector [3] or vectors [N, 3] to rotation matrix [3, 3] or matrices [N, 3, 3]- Return type:
ndarray- Returns:
rotation matrix or matrices
- log_rot_mat(rm)[source]¶
Convert rotation matrix to so3 coordinates (i.e. log() operator)
- Parameters:
rm (
ndarray) – rotation matrix [3, 3] or matrices [N, 3, 3]- Return type:
ndarray- Returns:
so3 coordinate rotation vector [3] or [N, 3]
- exp_pose6(pose6)[source]¶
Convert exponential poses to homogeneous matrix poses.
- Parameters:
pose6 (
ndarray) – vector [6] or matrix [N, 6] of exponential poses- Return type:
ndarray- Returns:
Homogeneous matrix poses of size [4, 4] or [N, 4, 4].
- log_pose(pose)[source]¶
Convert homogeneous matrix(s) to exp pose coordinates.
- Parameters:
pose (
ndarray) – homogeneous pose [4, 4] or poses [N, 4, 4]- Return type:
ndarray- Returns:
exp pose coordinates [6] or [N, 6]
- pose_interp(p1, p2, t, *, delta_pose6=None)[source]¶
Pose interpolation between pose1 and pose2 at time t as ratio.
- Parameters:
p1 (
ndarray) – starting posep2 (
ndarray) – ending poset (
float) – ratio between pose p1 and p2 at what point to interpolate, not restricted between [0, 1] and can be extended for out of boundsdelta_pose6 (
Optional[ndarray]) – pre-calculated difference inv(p1) @ p2, saves computation if it’s available already
- Return type:
ndarray- Returns:
pose of the point at time t on the line defined by p1 and p2 on SE3 manifold
- traj_interp(traj_poses, ts)[source]¶
Trajectory interpolation for points in between.
TODO[pb]: Extend with time_bounds args for traj evaluator when needed :rtype:
ndarray- Parameters:
traj_poses (Sequence[Tuple[int | float | number, ndarray]])
ts (Sequence[int | float | number] | ndarray)
- Return type:
ndarray
- class TrajectoryEvaluator(poses, *, time_bounds=0)[source]¶
Bases:
PoserInterpolates trajectory for a set of timestamps from knot poses.
TODO[pb]: Add function to add/remove knot poses from traj eval.
- TODO: Optionally, we may want to implement these calculations in C++ and
use bindings to make it faster.
- Parameters:
poses (
Sequence[Tuple[Union[int,float,number],ndarray]]) – List of knot poses with timestamps. Every list item is a tuple (ts, pose).time_bounds (
Optional[float]) –whether to restrict the pose interpolation to the timestamp range within the poses list: None - no restriction at all on the timestamps that can
be used to get pose from the trajectory
- 0 - strict bounds on the timestamp range in the
poses list
- >0 - ratio that is allowed to go over the timestamp
bounds. ratio value is applied as the ratio of pose[1].ts - pose[0].ts for the left bound, and pose[N].ts - pose[N-1].ts for the right bound.
- pose_frames(source, *, poses=None)[source]¶
Add poses to LidarFrames stream.
- Parameters:
source – one of: - Sequence[core.LidarFrame] - single frame sources - Sequence[core.FrameSet] - multi frame set sources
poses (Poser | None)
- load_kitti_poses(file)[source]¶
Loads the Kitti poses from the file.
- Return type:
ndarray- Returns:
[N, 4, 4] array of homogeneous poses
- Parameters:
file (str)
- make_kiss_traj_poses(poses)[source]¶
Makes a traj poses from kiss poses.
- Parameters:
poses (
Union[Sequence[ndarray],ndarray]) – pose for every frame in the sequence as returned by KissICP- Returns:
0.5 For example frame indexes 0, 1, 2 produce timestamps 0.5, 1.5, 2.5
- Return type:
trajectory poses timestamped by the frame index mid point
- pose_frames_from_kitti(source, kitti_poses)[source]¶
Add poses to LidarFrames stream using the previously saved per frame poses.
Every pose is considered to be in the middle of the frame. We assume that very first frame starts at t = 0 and ends at t = 1, thus the first pose is timestamped as 0.5, second pose is timestamped at 1.5 (middle of the second frame), and so on … to the very last pose N which timestamped at N + 0.5 for the last N frame.
- Parameters:
source – one of: - Sequence[core.LidarFrame] - single frame sources - Sequence[core.FrameSet] - multi frame set sources
kitti_poses (
str) – path to the file with in kitti poses format, i.e. every line contains 12 floats of 4x4 homogeneous transformation matrix ([:3, :]in numpy notation, row-major serialized)