Source code for ouster.sdk.util.pose_util

from typing import (Union, Tuple, List, Optional, Sequence, Protocol)

import numpy as np

import bisect

from ouster.sdk import core

import logging

try:
    from scipy.spatial.transform import Rotation as R
    _no_scipy = False
except ImportError:
    _no_scipy = True

# show "No scipy ..."" message only once on the first encounter
_no_scipy_warned = False


[docs] def no_scipy() -> bool: """Checks the scipy availability with a warning message.""" global _no_scipy_warned if _no_scipy: if _no_scipy_warned: logger = logging.getLogger("ouster-sdk-pose-util") logger.warning("No scipy module is found. Please install scipy for " "faster poses calculations: pip3 install scipy.") _no_scipy_warned = True return True else: return False
# takes in a pose vector and returns a unit vector pointing in the same direction
[docs] def normalize_vector(v: np.ndarray) -> np.ndarray: norm = np.linalg.norm(v) if norm == 0: return v return v / norm
Numeric = Union[int, float, np.number] # 3D pose (rotation + translation) represented by 6 elements # of se3 Lie algebra (i.e. exponential coordinates): # [wx, wy, wz, x, y, z] Pose6 = np.ndarray # 3D pose (rotation + translation) represented by 4x4 matrix # of SE3 manifold (i.e. homogeneous matrix): # 4x4 matrix: [R | T] # [0 | 1] # where: R is 3x3 rotation matrix SO3 # T is 3x1 translation vector PoseH = np.ndarray Pose = Union[Pose6, PoseH] TrajPoses = Sequence[Tuple[Numeric, Pose]] # List of pairs (ts, Pose6), where 6 element pose in exponential coordinates. # pose : [wx, wy, wz, x, y, z] PosesList = List[Tuple[int, Pose6]] # ========================================================================== # ======== Temp stub functions for no scipy environments =================== def _no_scipy_exp_rot_vec(vec: np.ndarray) -> np.ndarray: """Converts so3 vector(s) to a rotation matrix(s). (no scipy version, not optimised) Dimensions: [3] -> [3, 3] or [N, 3] -> [N, 3, 3] """ ret_first = False if vec.ndim == 1: vec = vec[np.newaxis, ...] ret_first = True res = np.zeros((vec.shape[0], 3, 3)) for i in range(vec.shape[0]): theta = np.linalg.norm(vec[i]) if abs(theta) < 1e-9: res[i] = np.eye(3) continue rot_axis = vec[i] / theta w = np.array([[0, -rot_axis[2], rot_axis[1]], [rot_axis[2], 0, -rot_axis[0]], [-rot_axis[1], rot_axis[0], 0]]) res[i] = np.eye(3) + np.sin(theta) * w \ + (1 - np.cos(theta)) * np.dot(w, w) return res[0] if ret_first else res # Lynch and Park: 3.2.3.3, Page 87, Algorithm def _no_scipy_log_rot_mat(rm) -> np.ndarray: """Convert rotation matrix(s) to so3 vector coordinates (log() operator) (no scipy version, not optimised) Dimensions: [3, 3] -> [3] or [N, 3, 3] -> [N, 3] """ ret_first = False if rm.ndim == 2: rm = rm[np.newaxis, ...] ret_first = True res = np.zeros((rm.shape[0], 3)) for i in range(rm.shape[0]): acos = 0.5 * (np.trace(rm[i]) - 1) if acos >= 1: res[i] = np.zeros(3) continue if acos <= -1: if abs(1 + rm[i, 2, 2]) > 1e-9: res[i] = np.pi * ( 1.0 / np.sqrt(2 + 2 * rm[i, 2, 2])) * np.array( [rm[i, 0, 2], rm[i, 1, 2], 1 + rm[i, 2, 2]]) continue if abs(1 + rm[i, 1, 1]) > 1e-9: res[i] = np.pi * (1.0 / np.sqrt(2 + 2 * rm[i, 1, 1])) * np.array( [rm[i, 0, 1], 1 + rm[i, 1, 1], rm[i, 2, 1]]) continue res[i] = np.pi * (1.0 / np.sqrt(2 + 2 * rm[i, 0, 0])) * np.array( [1 + rm[i, 0, 0], rm[i, 1, 0], rm[i, 2, 0]]) continue theta = np.arccos(acos) w = (0.5 / np.sin(theta)) * (rm[i] - rm[i].transpose()) res[i] = theta * np.array([w[2, 1], w[0, 2], w[1, 0]]) return res[0] if ret_first else res def _no_scipy_exp_pose6(vec: np.ndarray) -> np.ndarray: """Convert exponential pose6 vector(s) to homogeneous matrix(s). (no scipy version, not optimised) Dimensions: [6] -> [4, 4] or [N, 6] -> [N, 4, 4] """ ret_first = False if vec.ndim == 1: vec = vec[np.newaxis, ...] ret_first = True res = np.zeros((vec.shape[0], 4, 4)) for i in range(vec.shape[0]): # standard implementation theta = np.linalg.norm(vec[i, :3]) if abs(theta) < 1e-9: res[i] = np.r_[np.c_[np.eye(3), vec[i, 3:]], [[0, 0, 0, 1]]] continue rot_axis = vec[i, :3] / theta w = np.array([[0, -rot_axis[2], rot_axis[1]], [rot_axis[2], 0, -rot_axis[0]], [-rot_axis[1], rot_axis[0], 0]]) hom = np.eye(4) hom[:3, :3] = _no_scipy_exp_rot_vec(vec[i, :3]) hom[:3, 3] = np.dot( np.eye(3) * theta + (1 - np.cos(theta)) * w + (theta - np.sin(theta)) * np.dot(w, w), vec[i, 3:]) / theta res[i] = hom return res[0] if ret_first else res def _no_scipy_log_pose(hmat: np.ndarray) -> np.ndarray: """Convert homogeneous matrix(s) to exp pose6 vector(s) coordinate. (no scipy version, not optimised) Dimensions: [4, 4] -> [6] or [N, 4, 4] -> [N, 6] """ # standard implementation ret_first = False if hmat.ndim == 2: hmat = hmat[np.newaxis, ...] ret_first = True res = np.zeros((hmat.shape[0], 6)) for i in range(hmat.shape[0]): sov3 = _no_scipy_log_rot_mat(hmat[i, :3, :3]) if np.array_equal(sov3, np.zeros(3)): res[i] = np.r_[np.zeros(3), hmat[i, :3, 3]] continue theta = np.linalg.norm(sov3) rot_axis = sov3 / theta w = np.array([[0, -rot_axis[2], rot_axis[1]], [rot_axis[2], 0, -rot_axis[0]], [-rot_axis[1], rot_axis[0], 0]]) t = np.dot( np.eye(3) / theta - 0.5 * w + (1 / theta - 0.5 / np.tan(theta / 2)) * np.dot(w, w), hmat[i, :3, 3]) res[i] = np.r_[sov3, theta * t] return res[0] if ret_first else res # ========================================================================== # ==========================================================================
[docs] def exp_rot_vec(vec: np.ndarray) -> np.ndarray: """Converts so3 vector to a rotation matrix. Args: vec: so3 rotation vector [3] or vectors [N, 3] to rotation matrix [3, 3] or matrices [N, 3, 3] Return: rotation matrix or matrices """ if no_scipy(): return _no_scipy_exp_rot_vec(vec) return R.from_rotvec(vec).as_matrix()
[docs] def log_rot_mat(rm: np.ndarray) -> np.ndarray: """Convert rotation matrix to so3 coordinates (i.e. log() operator) Args: rm: rotation matrix [3, 3] or matrices [N, 3, 3] Return: so3 coordinate rotation vector [3] or [N, 3] """ if no_scipy(): return _no_scipy_log_rot_mat(rm) return R.from_matrix(rm).as_rotvec()
# Lynch and Park: 3.3.3.2, Page 106, Algorithm
[docs] def exp_pose6(pose6: Pose6) -> np.ndarray: """Convert exponential poses to homogeneous matrix poses. Args: pose6: vector [6] or matrix [N, 6] of exponential poses Return: Homogeneous matrix poses of size [4, 4] or [N, 4, 4]. """ if no_scipy(): return _no_scipy_exp_pose6(pose6) single_pose = False if pose6.ndim > 2: raise ValueError(f"ERROR: Expected 1-,2-dim inputs to exp_pose6. But" f" {pose6.ndim} dimensions provided.") elif pose6.ndim == 1: single_pose = True pose6 = pose6[np.newaxis, :] theta = np.linalg.norm(pose6[:, :3], axis=1) flag = np.abs(theta) < 1e-9 if np.all(flag): hom = np.tile(np.eye(4), (pose6.shape[0], 1, 1)) hom[:, :3, 3] += pose6[:, 3:] return hom[0] if single_pose else hom # overwrite close to zero values theta[flag] = 1 rot_axis = pose6[:, :3] / theta[:, np.newaxis] w = np.empty((pose6.shape[0], 3, 3), np.float64) w[:, 0, 0] = 0 w[:, 0, 1] = -rot_axis[:, 2] w[:, 0, 2] = rot_axis[:, 1] w[:, 1, 0] = rot_axis[:, 2] w[:, 1, 1] = 0 w[:, 1, 2] = -rot_axis[:, 0] w[:, 2, 0] = -rot_axis[:, 1] w[:, 2, 1] = rot_axis[:, 0] w[:, 2, 2] = 0 hom = np.tile(np.eye(4), (pose6.shape[0], 1, 1)) hom[:, :3, :3] = R.from_rotvec(pose6[:, :3]).as_matrix() temp = \ np.eye(3)[np.newaxis, :, :] * theta[:, np.newaxis, np.newaxis] + \ (1 - np.cos(theta))[:, np.newaxis, np.newaxis] * w + \ ((theta - np.sin(theta))[:, np.newaxis, np.newaxis] * np.einsum('ijk,ikl->ijl', w, w)) hom[:, :3, -1] = np.einsum('ijk,ik,i->ij', temp, pose6[:, 3:], 1 / theta, optimize=['einsum_path', (0, 1), (0, 1)]) # Overwrite bad transforms hom[flag] = np.eye(4)[np.newaxis, ...] hom[flag, :3, 3] += pose6[flag, 3:] return hom[0] if single_pose else hom
[docs] def log_pose(pose: PoseH) -> np.ndarray: """Convert homogeneous matrix(s) to exp pose coordinates. Args: pose: homogeneous pose [4, 4] or poses [N, 4, 4] Return: exp pose coordinates [6] or [N, 6] """ if no_scipy(): return _no_scipy_log_pose(pose) if pose.ndim not in [2, 3]: raise ValueError(f"ERROR: Expected 2-,3-dim inputs to log_pose. But" f" {pose.ndim} dimensions provided.") single_pose = False if pose.ndim == 2: single_pose = True pose = pose[np.newaxis, :] sov3 = R.from_matrix(pose[:, :3, :3]).as_rotvec() theta = np.linalg.norm(sov3, axis=1) flag_def = theta < 1e-9 # overwrite close to zero values theta[flag_def] = 1 if np.all(flag_def): if single_pose: return np.concatenate([np.zeros(3), pose[0, :3, 3].ravel()]) else: return np.c_[np.zeros((pose.shape[0], 3)), pose[:, :3, 3]] rot_axis = sov3 / theta[:, np.newaxis] w = np.empty((rot_axis.shape[0], 3, 3), np.float64) w[:, 0, 0] = 0 w[:, 0, 1] = -rot_axis[:, 2] w[:, 0, 2] = rot_axis[:, 1] w[:, 1, 0] = rot_axis[:, 2] w[:, 1, 1] = 0 w[:, 1, 2] = -rot_axis[:, 0] w[:, 2, 0] = -rot_axis[:, 1] w[:, 2, 1] = rot_axis[:, 0] w[:, 2, 2] = 0 t = np.einsum( "i,ijk,ik->ij", theta, np.eye(3)[np.newaxis, :, :] / theta[:, np.newaxis, np.newaxis] - 0.5 * w + (1 / theta - 0.5 / np.tan(theta / 2))[:, np.newaxis, np.newaxis] * np.einsum('ijk,ikl->ijl', w, w), pose[:, :3, 3]) res = np.c_[sov3, t] # overwrite the zero rotation (i.e. identity) since it # was left with ones stub to avoid div zero res[flag_def] = np.c_[np.zeros((np.count_nonzero(flag_def), 3)), pose[flag_def, :3, 3]] return res[0] if single_pose else res
[docs] def pose_interp(p1: Pose, p2: Pose, t: float, *, delta_pose6: Optional[Pose6] = None) -> np.ndarray: """Pose interpolation between pose1 and pose2 at time t as ratio. Args: p1: starting pose p2: ending pose t: ratio between pose p1 and p2 at what point to interpolate, not restricted between [0, 1] and can be extended for out of bounds delta_pose6: pre-calculated difference `inv(p1) @ p2`, saves computation if it's available already Return: pose of the point at time `t` on the line defined by p1 and p2 on SE3 manifold """ pose1 = np.array(p1) if pose1.ndim == 1: pose1 = exp_pose6(pose1) pose2 = np.array(p2) if pose2.ndim == 1: pose2 = exp_pose6(pose2) if delta_pose6 is None: pose_d = np.dot(np.linalg.inv(pose1), pose2) log_pose_d = log_pose(pose_d) else: log_pose_d = delta_pose6 pose_d_dt = exp_pose6(log_pose_d * t) pose_interp = np.dot(pose1, pose_d_dt) return pose_interp
[docs] def traj_interp(traj_poses: TrajPoses, ts: Union[Sequence[Numeric], np.ndarray]) -> np.ndarray: """Trajectory interpolation for points in between. TODO[pb]: Extend with `time_bounds` args for traj evaluator when needed """ return TrajectoryEvaluator(traj_poses).poses_at(ts)
[docs] class Poser(Protocol): """Actor that adds poses to LidarFrames""" def __call__(self, frame: core.LidarFrame, *, col_ts: Optional[np.ndarray] = None) -> core.LidarFrame: """Add poses to the frame, modifying in-place.""" ...
[docs] class TrajectoryEvaluator(Poser): """Interpolates trajectory for a set of timestamps from knot poses. TODO[pb]: Add function to add/remove knot poses from traj eval. TODO: Optionally, we may want to implement these calculations in C++ and use bindings to make it faster. """ def __init__(self, poses: TrajPoses, *, time_bounds: Optional[float] = 0): """ Args: poses: List of knot poses with timestamps. Every list item is a tuple (ts, pose). time_bounds: whether to restrict the pose interpolation to the timestamp range within the poses list: None - no restriction at all on the timestamps that can be used to get pose from the trajectory 0 - strict bounds on the timestamp range in the poses list >0 - ratio that is allowed to go over the timestamp bounds. ratio value is applied as the ratio of pose[1].ts - pose[0].ts for the left bound, and pose[N].ts - pose[N-1].ts for the right bound. """ if len(poses) < 2: raise ValueError("TrajectoryEvaluator expects at least 2 poses.") is_pose_hom = True if poses[0][1].size == 16 else False if not is_pose_hom: assert poses[0][1].size == 6, "Expect all poses either [6] or [4, 4] size" # check time non-decreasing order for i, (ts, p) in enumerate(poses[1:], start=1): assert ts > poses[i - 1][0], f"Expected increasing trajectories" \ f" timestamps but found {ts} <= {poses[i - 1][0]}" assert poses[i][1].size == 16 if is_pose_hom else poses[i][1].size == 6, \ "Expected all poses in a trajectory to be of the same type:" \ "[6] or [4, 4]" self._poses = poses self._time_bounds = time_bounds if len(self._poses) > 0: # pre-calculating intermediaries: poses matrix and poses deltas # converting all pose knots to homogeneous form poses_arr = np.array([p[1] for p in self._poses]) self._poses_mat = poses_arr if is_pose_hom else exp_pose6( poses_arr) # precalculating deltas between adjacent poses deltas_mat = np.matmul(np.linalg.inv(self._poses_mat[:-1]), self._poses_mat[1:]) # we only need vec6 form for deltas to do interpolations self._deltas = np.r_[np.zeros((1, 6)), log_pose(deltas_mat)] # store keys separately for bisect function self._ts_keys: List[Numeric] = [x[0] for x in self._poses] def _check_ts_and_bounds(self, ts: Union[Sequence[Numeric], np.ndarray]): """Checks whether `ts` in the trajectory poses timestamps with bounds""" # check time non-decreasing order if len(ts) > 1: for t1, t2 in zip(ts[:-1], ts[1:]): assert t1 <= t2, f"Expected non-decreasing timestamps " \ f"but found {t1} > {t2}" # no check for bounds is needed if self._time_bounds is None: return # get left/right bounds distance left_bound = (self._poses[0][0] - ts[0]) / (self._poses[1][0] - self._poses[0][0]) right_bound = (ts[-1] - self._poses[-1][0]) / (self._poses[-1][0] - self._poses[-2][0]) if left_bound > self._time_bounds or right_bound > self._time_bounds: raise ValueError( f"Timestamps should be in the poses timestamp range: " f"from {self._ts_keys[0]} to {self._ts_keys[-1]}, with " f"{self._time_bounds} bounds. But got from {ts[0]} to " f"{ts[-1]}") # time bounds on the edges are fine return
[docs] def pose_at(self, ts: Numeric) -> PoseH: """Calculates a single pose (4x4 matrix) at a given `ts` timestamp.""" self._check_ts_and_bounds([ts]) if ts < self._poses[0][0]: # out on the left dt = (ts - self._ts_keys[0]) / (self._ts_keys[1] - self._ts_keys[0]) pose_d_dt = exp_pose6(self._deltas[1] * dt) pose_base = self._poses_mat[0] elif ts >= self._poses[-1][0]: # out on the right dt = (ts - self._ts_keys[-2]) / (self._ts_keys[-1] - self._ts_keys[-2]) pose_d_dt = exp_pose6(self._deltas[-1] * dt) pose_base = self._poses_mat[-2] else: # within traj poses timestamps curr_idx = bisect.bisect_right(self._ts_keys, ts) dt = (ts - self._ts_keys[curr_idx - 1]) / ( self._ts_keys[curr_idx] - self._ts_keys[curr_idx - 1]) pose_d_dt = exp_pose6(self._deltas[curr_idx] * dt) pose_base = self._poses_mat[curr_idx - 1] return np.dot(pose_base, pose_d_dt)
[docs] def poses_at(self, ts: Union[Sequence[Numeric], np.ndarray]) -> np.ndarray: """Calculates multiple poses (4x4 matrices) at a given `ts` timestamps.""" if len(ts) == 0: return np.array([]) self._check_ts_and_bounds(ts) ts_size = len(ts) pose_d_dts = np.zeros((ts_size, 6)) dts = np.zeros(ts_size) curr_idx_1_poses = np.tile(np.eye(4), (ts_size, 1, 1)) curr_idx = 0 for i in range(ts_size): if ts[i] < self._poses[0][0]: # out on the left dts[i] = (ts[i] - self._ts_keys[0]) / (self._ts_keys[1] - self._ts_keys[0]) pose_d_dts[i] = self._deltas[1] curr_idx_1_poses[i] = self._poses_mat[0] elif ts[i] >= self._poses[-1][0]: # out on the right dts[i] = (ts[i] - self._ts_keys[-2]) / (self._ts_keys[-1] - self._ts_keys[-2]) pose_d_dts[i] = self._deltas[-1] curr_idx_1_poses[i] = self._poses_mat[-2] else: if curr_idx == 0: # reach the data range by the curr_idx first curr_idx = bisect.bisect_right(self._ts_keys, ts[i]) elif ts[i] > self._ts_keys[curr_idx]: # current pose knot (to the right) is already behind, need # to advance to the next pose knot if curr_idx + 1 >= len(self._poses): # no more poses break # trying to get just next pose curr_idx += 1 if ts[i] > self._ts_keys[curr_idx]: # do bisect again, because it's a discontinuity here # i.e. the current ts[i] is too far from the # previous one [i-1] curr_idx = bisect.bisect_right(self._ts_keys, ts[i]) dts[i] = (ts[i] - self._ts_keys[curr_idx - 1]) / ( self._ts_keys[curr_idx] - self._ts_keys[curr_idx - 1]) pose_d_dts[i] = self._deltas[curr_idx] curr_idx_1_poses[i] = self._poses_mat[curr_idx - 1] pose_d_dts = np.einsum("i,ij->ij", dts, pose_d_dts) pose_d_dts_mat = exp_pose6(pose_d_dts) return np.matmul(curr_idx_1_poses, pose_d_dts_mat)
def __bool__(self) -> bool: return bool(self._poses) def __call__(self, frame: core.LidarFrame, *, col_ts: Optional[np.ndarray] = None) -> core.LidarFrame: """Add poses to the frame. Use `col_ts` if the column timestamps need to be remapped to a different time scale. Args: col_ts: optional array of [frame.W] remapped timestamps to use instead of frame.timestamp for pose calculations. """ valid_cols = (np.bitwise_and(frame.status, 1) == 1) if col_ts is not None and col_ts.ndim == 1 and col_ts.size == frame.w: ts = col_ts[valid_cols] else: ts = frame.timestamp[valid_cols] if ts.size == 0: return frame frame.body_to_world[valid_cols] = self.poses_at(ts) return frame def __len__(self) -> int: return len(self._poses) def __getitem__(self, idx): return self._poses[idx]
[docs] def pose_frames( source, *, poses: Optional[Poser] = None ): """Add poses to LidarFrames stream. Args: source: one of: - Sequence[core.LidarFrame] - single frame sources - Sequence[core.FrameSet] - multi frame set sources """ for obj in source: if isinstance(obj, core.LidarFrame): # Iterator[core.LidarFrame] yield poses(obj) if poses is not None else obj elif isinstance(obj, core.FrameSet): # collated frame sets: List[FrameSet] if poses is not None: yield [ poses(frame) if frame is not None else None for frame in obj ] else: yield obj else: raise ValueError( "Expected one of types: LidarFrame, Tuple[Optional[LidarFrame]]" "elements. But got:", type(obj))
[docs] def load_kitti_poses(file: str) -> np.ndarray: """Loads the Kitti poses from the file. Returns: [N, 4, 4] array of homogeneous poses """ kitti_poses = np.loadtxt(file, delimiter=" ") poses_num = kitti_poses.shape[0] poses = np.concatenate( (kitti_poses, np.tile(np.array([0, 0, 0, 1]), (poses_num, 1))), axis=1) poses = poses.reshape((-1, 4, 4)) return poses
[docs] def make_kiss_traj_poses(poses: Union[Sequence[Pose], np.ndarray]) -> TrajPoses: """Makes a traj poses from kiss poses. Args: poses: pose for every frame in the sequence as returned by KissICP Returns: trajectory poses timestamped by the frame index mid point: 0.5 For example frame indexes 0, 1, 2 produce timestamps 0.5, 1.5, 2.5 """ traj_poses = list([(0.5 + i, p) for i, p in enumerate(poses)]) return traj_poses
[docs] def pose_frames_from_kitti( source, kitti_poses: str ): """Add poses to LidarFrames stream using the previously saved per frame poses. Every pose is considered to be in the middle of the frame. We assume that very first frame starts at t = 0 and ends at t = 1, thus the first pose is timestamped as 0.5, second pose is timestamped at 1.5 (middle of the second frame), and so on ... to the very last pose N which timestamped at N + 0.5 for the last N frame. Args: source: one of: - Sequence[core.LidarFrame] - single frame sources - Sequence[core.FrameSet] - multi frame set sources kitti_poses: path to the file with in kitti poses format, i.e. every line contains 12 floats of 4x4 homogeneous transformation matrix (``[:3, :]`` in numpy notation, row-major serialized) """ # load one pose per frame poses = load_kitti_poses(kitti_poses) # make time indexed poses starting from 0.5 traj_poses = make_kiss_traj_poses(poses) traj_eval = TrajectoryEvaluator(traj_poses, time_bounds=1.5) norm_col_ts: Optional[np.ndarray] norm_col_ts = None frame_idx = -1 start_frame_id = -1 start_frame_ts = -1 for obj, in source: if isinstance(obj, core.LidarFrame): # Iterator[core.LidarFrame] frame = obj # checking for the source looping (if frame_id and frame_ts was seen) try: first_valid_col_ts = frame.timestamp[frame.get_first_valid_column()] except RuntimeError: continue if start_frame_id < 0: start_frame_id = frame.frame_id start_frame_ts = first_valid_col_ts elif (start_frame_id == frame.frame_id and start_frame_ts == first_valid_col_ts): # loop detected, reset frame_idx frame_idx = -1 frame_idx += 1 if norm_col_ts is None: norm_col_ts = np.linspace(0, 1.0, frame.w, endpoint=False) idx_ts = frame_idx + norm_col_ts traj_eval(frame, col_ts=idx_ts) yield frame elif isinstance(obj, core.FrameSet): # collated frame sets: core.FrameSet # TODO[pb]: Make it for multi frame set sources when we have stable # multi source interfaces raise ValueError("Multi frame set sources not yet implemented. Got: ", type(obj)) else: raise ValueError( "Expected one of types: LidarFrame, Tuple[Optional[LidarFrame]]" "elements. But got:", type(obj))