ouster.sdk.core.core module

Copyright (c) 2021, Ouster, Inc. All rights reserved.

This module contains wrappers for packet sources, frame borders, and pose validation. Defines how to read packets, manage frames, and check pose validity.

class Packets(it, metadata)[source]

Bases: PacketSource

Create a PacketSource from an existing iterator.

Parameters:
property sensor_info: List[SensorInfo]

Retrieve sensor information for all sensors in the packet source.

Returns:

A list of SensorInfo objects, each containing metadata about a sensor, such as serial number, firmware version, and calibration details.

close()[source]
Return type:

None

property is_live: bool

Check if the packet source is live.

class FrameBorder(meta, pred=<function FrameBorder.<lambda>>)[source]

Bases: object

Create callable helper that indicates the cross frames packets.

Parameters:
first_valid_column_pose(frame)[source]

Return first valid column pose of a LidarFrame :rtype: ndarray

Parameters:

frame (LidarFrame)

Return type:

ndarray

last_valid_column_pose(frame)[source]

Return last valid column pose of a LidarFrame :rtype: ndarray

Parameters:

frame (LidarFrame)

Return type:

ndarray