Source code for ouster.sdk.core.core
"""
Copyright (c) 2021, Ouster, Inc.
All rights reserved.
This module contains wrappers for packet sources, frame borders, and pose validation.
Defines how to read packets, manage frames, and check pose validity.
"""
from typing import (Iterable, Iterator, List, Callable, Tuple, Union)
import logging
import numpy as np
from ouster.sdk._bindings.client import (SensorInfo, PacketFormat, LidarFrame,
LidarPacket, ImuPacket, ZonePacket, Packet, PacketSource)
logger = logging.getLogger("ouster.sdk.core.core")
[docs]
class Packets(PacketSource):
"""Create a :class:`PacketSource` from an existing iterator."""
_it: Iterable[Union[LidarPacket, ImuPacket, ZonePacket]]
_metadata: List[SensorInfo]
def __init__(self, it: Iterable[Union[LidarPacket, ImuPacket, ZonePacket]], metadata: SensorInfo):
"""
Args:
it: A stream of packets
metadata: Metadata for the packet stream
"""
PacketSource.__init__(self)
self._it = it
self._metadata = [metadata]
@property
def sensor_info(self) -> List[SensorInfo]:
return self._metadata
def __iter__(self) -> Iterator[Tuple[int, Union[LidarPacket, ImuPacket, ZonePacket]]]:
"""Return the underlying iterator."""
for packet in self._it:
yield (0, packet)
[docs]
def close(self) -> None:
pass
@property
def is_live(self) -> bool:
return False
[docs]
class FrameBorder:
"""Create callable helper that indicates the cross frames packets."""
def __init__(self, meta: SensorInfo, pred: Callable[[Packet], bool] = lambda _: True):
self._last_f_id = -1
self._last_packet_ts = None
self._last_packet_res = False
self._pred = pred
self._pf = PacketFormat(meta)
def __call__(self, packet: Packet) -> bool:
if isinstance(packet, LidarPacket):
# don't examine packets again
if (self._last_packet_ts and (packet.host_timestamp != 0) and
self._last_packet_ts == packet.host_timestamp):
return self._last_packet_res
f_id = self._pf.frame_id(packet.buf)
changed = (self._last_f_id != -1 and f_id != self._last_f_id)
self._last_packet_res = changed and self._pred(packet)
self._last_f_id = f_id
return self._last_packet_res
return False
[docs]
def first_valid_column_pose(frame: LidarFrame) -> np.ndarray:
"""Return first valid column pose of a LidarFrame"""
try:
return frame.body_to_world[frame.get_first_valid_column()]
except RuntimeError:
return np.identity(4, dtype=np.float64)
[docs]
def last_valid_column_pose(frame: LidarFrame) -> np.ndarray:
"""Return last valid column pose of a LidarFrame"""
try:
return frame.body_to_world[frame.get_last_valid_column()]
except RuntimeError:
return np.identity(4, dtype=np.float64)