Source code for ouster.sdk.viz.tracks_accumulator

"""
Copyright (c) 2023, Ouster, Inc.
All rights reserved.
"""

import numpy as np
from typing import Optional
from ouster.sdk._bindings.viz import Cloud, PointViz
from ouster.sdk.viz.model import LidarFrameVizModel
from ouster.sdk.viz.accum_base import AccumulatorBase
from ouster.sdk.viz.track import Track


[docs] class TracksAccumulator(AccumulatorBase): """Encapsulates render state for tracks (frame positions) and key frames (which are "interesting" frame positions according to the LidarFrameVizAccumulatorsConfig.) Cloud objects (from the ouster_viz library) are used to render the tracks.""" DEFAULT_PT_SIZE = 5 DEFAULT_KF_PT_SIZE = 10 # TODO[tws] support MultiTrack? def __init__(self, model: LidarFrameVizModel, point_viz: PointViz, track: Track): super().__init__(model, point_viz, track) self._accum_mode_track = True pnum = self._track._xyz.shape[0] self._cloud_track: Cloud = Cloud(pnum) self._cloud_track.set_point_size(self.DEFAULT_PT_SIZE) self._cloud_kf_track: Cloud = Cloud(track._kf_max_num + 1) self._cloud_kf_track.set_point_size(self.DEFAULT_KF_PT_SIZE) self._cloud_kf_track.set_xyz(track._kf_xyz) self._cloud_kf_track.set_key(track._kf_key[np.newaxis, ...]) self._viz.add(self._cloud_track) self._viz.add(self._cloud_kf_track) self._ensure_cloud_track() @property def track_visible(self) -> bool: """Returns true if the track is visible.""" return self._accum_mode_track
[docs] def toggle_visibility(self, state: Optional[bool] = None): """Toggle track visibility by adding or removing the Clouds used to render it to / from the viz.""" new_state = (not self._accum_mode_track if state is None else state) if self._accum_mode_track and not new_state: self._viz.remove(self._cloud_track) self._viz.remove(self._cloud_kf_track) elif (not self._accum_mode_track and new_state): self._viz.add(self._cloud_track) self._viz.add(self._cloud_kf_track) self._accum_mode_track = new_state
def _ensure_cloud_track(self) -> None: """Create/re-create the Clouds used to render the track in the viz.""" pnum = self._track._xyz.shape[0] if self._cloud_track.size != pnum: self._viz.remove(self._cloud_track) self._viz.remove(self._cloud_kf_track) self._cloud_track = Cloud(pnum) self._cloud_track.set_point_size(self.DEFAULT_PT_SIZE) self._cloud_track.set_xyz(self._track._xyz) self._cloud_track.set_key(self._track._key[np.newaxis, ...]) if self.track_visible: self._viz.add(self._cloud_track) self._viz.add(self._cloud_kf_track) # TODO[tws] generalize draw method interface def _draw_track(self) -> None: """Updates the values in the Clouds used to render the track.""" self._ensure_cloud_track() self._cloud_track.set_xyz(self._track._xyz) self._cloud_track.set_key(self._track._key[np.newaxis, ...]) self._cloud_kf_track.set_xyz(self._track._kf_xyz) self._cloud_kf_track.set_key(self._track._kf_key[np.newaxis, ...])