Source code for ouster.sdk.viz.map_accumulator

import numpy as np
from typing import Dict, Optional, List, Union, cast
from ouster.sdk.core import ChanField, FrameSet
from ouster.sdk.core import dewarp
from ouster.sdk._bindings.viz import Cloud, PointViz
from ouster.sdk.viz.accum_base import AccumulatorBase
from ouster.sdk.viz.model import LidarFrameVizModel
from ouster.sdk.viz.track import Track, TRACK_MAP_GROWTH_RATE
from ouster.sdk.viz.view_mode import CloudPaletteItem
from ouster.sdk.viz.accumulators_config import LidarFrameVizAccumulatorsConfig

MAP_INIT_POINTS_NUM: int = 10000


[docs] class MapAccumulator(AccumulatorBase): """Used by LidarFrameVizAccumulators to display a point cloud that is produced by all frames in the source data.""" def __init__(self, model: LidarFrameVizModel, point_viz: PointViz, track: Track, config: LidarFrameVizAccumulatorsConfig): super().__init__(model, point_viz, track) # TODO[tws] consider refactoring or removing _map_enabled, either by making it an attribute of base or by # using optional instances of MapAccumulator and FramesAccumulator to indicate # enabled status self._map_enabled = config._map_enabled self._accum_mode_map = self._map_enabled # TODO[tws] kind of redundant self._map_select_ratio = config._map_select_ratio self._map_max_points = config._map_max_points self._map_overflow_start = config._map_overflow_from_start # initialize MAP structs map_init_points_num = MAP_INIT_POINTS_NUM if self._map_enabled else 0 map_init_points_num = min(self._map_max_points, map_init_points_num) self._map_xyz = np.zeros((map_init_points_num, 3), dtype=np.float32) # calculated color keys for every map point, indexed by cloud mode name self._map_keys: Dict[str, np.ndarray] = {} self._map_idx = 0 self._map_overflow = False # viz.Cloud for map points self._cloud_map: Optional[Cloud] = None self._ensure_cloud_map()
[docs] def toggle_visibility(self, state: Optional[bool] = None): new_state = (not self._accum_mode_map if state is None else state) if self._accum_mode_map and not new_state: assert self._cloud_map self._viz.remove(self._cloud_map) elif not self._accum_mode_map and new_state: assert self._cloud_map self._viz.add(self._cloud_map) self._accum_mode_map = new_state
def _ensure_cloud_map(self) -> None: """Create/re-create the cloud MAP object""" def make_cloud_map(n: int): self._cloud_map = Cloud(n) self._cloud_map.set_point_size(self._cloud_pt_size) current_palette = self._get_palette_from_active_mode_name(self.active_cloud_mode) if current_palette: self._cloud_map.set_palette(current_palette.palette) if self.map_visible: self._viz.add(self._cloud_map) pnum = self._map_xyz.shape[0] if not self._cloud_map: make_cloud_map(pnum) elif self._cloud_map.size < pnum: self._viz.remove(self._cloud_map) make_cloud_map(pnum) def _ensure_structs_map(self, xyz_size: int = 1) -> None: """Check map idx and array sizes and increase if needed""" if (not self._map_overflow and self._map_idx + xyz_size > self._map_xyz.shape[0]): new_size = min( self._map_max_points, int((self._map_xyz.shape[0] + xyz_size) * TRACK_MAP_GROWTH_RATE)) map_xyz = np.zeros((new_size, 3), dtype=np.float32) map_xyz[:self._map_xyz.shape[0]] = self._map_xyz self._map_xyz = map_xyz for map_key_name, map_key in self._map_keys.items(): new_map_key = np.zeros( (new_size, *map_key.shape[1:]), dtype=map_key.dtype) new_map_key[:map_key.shape[0]] = map_key self._map_keys[map_key_name] = new_map_key del map_key self._map_overflow = (self._map_idx + xyz_size > new_size) # reset map_idx from the beginning if there is no space for all # incoming points and map_overflow_start is enabled if (self._map_overflow_start and self._map_idx + xyz_size > self._map_xyz.shape[0]): self._map_idx = 0 @property def map_visible(self) -> bool: """Whether overall map (MAP) is visible""" return self._accum_mode_map def _update_map(self) -> None: """Update the map (MAP) data. Extract the select ratio of random points from the current frame. The map size if bounded by ``map_max_points``, selected random points defined by ratio ``map_select_ratio``, flag that triggers the map overwrite from the beginning rather than randomly is ``map_overflow_from_start``. """ assert len(self._frame) == len(self._model._sensors) for sensor, frame in zip(self._model._sensors, self._frame): if frame is None: return # get random xyz points using map select ratio range_field = frame.field(ChanField.RANGE) sel_flag = range_field != 0 nzi, nzj = np.nonzero(sel_flag) nzc = np.random.choice(len(nzi), min(int(self._map_select_ratio * len(nzi)), self._map_max_points), replace=False) row_sel, col_sel = nzi[nzc], nzj[nzc] xyz = sensor._xyzlut(range_field) xyz = cast(np.ndarray, dewarp(xyz, frame.body_to_world))[row_sel, col_sel] xyz_num = xyz.shape[0] # TODO[tws] previously protected by "with self._lock" - do we still need this? self._ensure_structs_map(xyz_num) idxs: Union[List[int], np.ndarray] if not self._map_overflow or self._map_overflow_start: idxs = list(range(self._map_idx, self._map_idx + xyz_num)) # type: ignore else: idxs = np.random.choice(self._map_xyz.shape[0], xyz_num, replace=False) # type: ignore self._map_xyz[idxs] = xyz for mode in sensor._cloud_modes.values(): field_colors = mode._prepare_data(frame, return_num=0) if field_colors is not None: key = field_colors[row_sel, col_sel] if mode.name not in self._map_keys: self._map_keys[mode.name] = np.zeros( (self._map_xyz.shape[0], *key.shape[1:]), dtype=key.dtype) self._map_keys[mode.name][idxs] = key self._map_idx += xyz_num
[docs] def update(self, frame: FrameSet, frame_num: Optional[int] = None) -> None: super().update(frame, frame_num) self._update_map()
def _update_cloud_mode(self): self._draw_map() def _get_palette_from_active_mode_name(self, mode_name: str) -> CloudPaletteItem: if mode_name == ChanField.REFLECTIVITY or \ mode_name == ChanField.REFLECTIVITY2: current_palette = self._model._palettes._refl_cloud_palettes[self._cloud_palette_ind] else: current_palette = self._model._palettes._cloud_palettes[self._cloud_palette_ind] return current_palette def _update_cloud_palette(self) -> None: # FIXME[tws] the CloudMode only applies to the sensor that was used to it # which probably means we need to use separate clouds per sensor anyway # This is wrong because # 1. the sensor may not have the mode # 2. the is_norm_reflectivity_mode may be inconsistent across sensors for the REFLECTIVITY mode # So for now we're just assuming that all sensors have valid calibrated reflectivity. current_palette = self._get_palette_from_active_mode_name(self.active_cloud_mode) if not current_palette: return self._cloud_palette_prev: Optional[CloudPaletteItem] if self._cloud_palette_prev is None or self._cloud_palette_prev.name != current_palette.name: self._cloud_palette_prev = current_palette if self._cloud_map: self._cloud_map.set_palette(current_palette.palette)
[docs] def update_point_size(self, point_size: float): self._cloud_pt_size = point_size if self._cloud_map: self._cloud_map.set_point_size(self._cloud_pt_size)
def _draw_map(self) -> None: """Update the map cloud""" self._ensure_cloud_map() if self._cloud_map is None: return self._cloud_map.set_xyz(self._map_xyz) if self.active_cloud_mode in self._map_keys: self._cloud_map.set_key( self._map_keys[self.active_cloud_mode][np.newaxis, ...]) self._update_cloud_palette()