Source code for ouster.sdk.core.masked_frame_set_source
from typing import List, Optional, Iterator
import numpy as np
from ouster.sdk._bindings.client import FrameSetSource
from ouster.sdk.core import SensorInfo, LidarFrame, FrameSet
from .frame_ops import mask
from ouster.sdk.core import destagger
[docs]
class MaskedFrameSetSource(FrameSetSource):
def __init__(self, frame_set_source: FrameSetSource, fields: List[str],
masks: List[Optional[np.ndarray]]) -> None:
FrameSetSource.__init__(self)
# Make sure current requirements are met
if len(frame_set_source.sensor_info) != len(masks):
raise ValueError("the number of masks should match the count of sensors")
self._frame_set_source = frame_set_source
self._fields = fields
self._masks = [destagger(si, mask, inverse=True) if mask is not None else None
for si, mask in zip(frame_set_source.sensor_info, masks)]
@property
def sensor_info(self) -> List[SensorInfo]:
return self._frame_set_source.sensor_info
@property
def is_live(self) -> bool:
return self._frame_set_source.is_live
@property
def is_indexed(self) -> bool:
return self._frame_set_source.is_indexed
@property
def frames_num(self) -> List[int]:
return self._frame_set_source.frames_num
def __len__(self) -> int:
return len(self._frame_set_source)
def __length_hint__(self) -> int:
return self._frame_set_source.__length_hint__()
def __iter__(self) -> Iterator[FrameSet]:
for frames in self._frame_set_source.__iter__():
result: List[Optional[LidarFrame]] = []
for idx, frame in enumerate(frames):
if frame:
cpy = LidarFrame(frame)
if self._masks[idx] is not None:
mask(cpy, self._fields, self._masks[idx]) # type: ignore
result.append(cpy)
else:
result.append(None)
yield FrameSet(result)
[docs]
def close(self) -> None:
pass
def __del__(self) -> None:
self.close()
def _mask_fn(self: FrameSetSource, fields: List[str], masks: List[Optional[np.ndarray]]):
return MaskedFrameSetSource(self, fields, masks)
FrameSetSource.mask = _mask_fn # type: ignore