Set a single configuration parameter
Any configuration parameter can be set by using this command.
Note: After PUT /api/v1/sensor/config/{param} request is received successfully, the sensor will reinitialize automatically to make the new configuration active, and the config settings are persisted across power cycles.
Path parameters
param
Query parameters
target
Specifies which configuration target to set:
staged: Updates the configuration for incremental validation without committing the changes to hardware. The staged configuration will be committed when theactiveorpersistedtarget is specified
Note: Parameters will be range checked, but will not be validated for mutual compatibility until the configuration is made active
active: Commits the staged configuration to hardwarepersisted: Equivalent toactivebut saves the configuration to non-volatile memory if it passes validation
Allowed values:
Request
A JSON object containing the details of a single config item
Response
Command succeeded
Errors
400
Bad Request Error