Reset OSSD output
Manually clear latched OSSD trips and faults by cycling the OSSD generator
enable. The request must echo the current reset_id from the OSSD status
endpoint; Keeper rotates the token on success so the request cannot be
replayed. Returns the post-reset status, including the new reset_id.
A trip source that is still asserted, or a persistent hardware fault,
re-latches immediately.
Request
The current reset_id from the OSSD status endpoint. Rejected if it
does not match the live token.
Response
True when OSSD dual-channel output is configured on the MIO pins
Live OSSD generator status.
DISABLED- OSSD generator is not running.ENABLED- OSSD generator is enabled.ACTIVE- OSSD outputs are asserted and diagnostics are clean.TRIPPED- outputs are deasserted because the trip source asserted (for example a Zone Monitor infringement). Not a hardware failure.FAULT- OSSD diagnostics detected a defect such as a short, open load, or failed startup qualification.
Human-readable latched OSSD trip and fault messages
Single-use token that must be echoed by a reset request. Rotated on each successful reset so a stale or replayed request cannot re-clear a latched fault.