Skip to navigation
Overview

API Reference Overview

HTTP API for querying and configuring Ouster sensors

Ouster sensors expose an HTTP API at /api/v1 served directly from the sensor. Use it to query sensor metadata, configure the sensor, manage firmware, and retrieve diagnostics. The OpenAPI description can be read from /api/v1/openapi.yaml.

All configuration parameter names are case-sensitive. Refer to the API reference pages for exact spelling. Examples throughout this documentation are tested on Linux. macOS and Windows users should adapt the command syntax accordingly.

Base URL

Requests use the sensor’s hostname or IP address as the base:

http://<sensor-hostname-or-ip>/api/v1/

For example, a sensor with hostname os-992244000006.local:

curl --request GET http://os-992244000006.local/api/v1/sensor/metadata/sensor_info

Supported clients

The API accepts standard HTTP requests. Any of the following work:

ClientNotes
curlUsed in all examples throughout this documentation
HTTPieHuman-friendly CLI alternative to curl
BrowserGET endpoints are accessible directly in a web browser
REST clientsAdvanced REST Client, Postman, Insomnia, etc.
Custom codeAny HTTP library (Python requests, Go net/http, etc.)

API surface

The HTTP API is organized into five resource groups:

Sensor metadata

Read-only endpoints that return fixed sensor properties — serial number, firmware version, calibration data, beam geometry, and data format descriptors.

EndpointDescription
GET /api/v1/sensor/metadata/sensor_infoSerial number, firmware revision, product line, and status
GET /api/v1/sensor/metadata/lidar_data_formatLidar packet structure and channel configuration
GET /api/v1/sensor/metadata/imu_data_formatIMU packet structure
GET /api/v1/sensor/metadata/beam_intrinsicsPer-beam azimuth and altitude angles
GET /api/v1/sensor/metadata/lidar_intrinsicsLidar-to-sensor coordinate transform
GET /api/v1/sensor/metadata/imu_intrinsicsIMU-to-sensor coordinate transform
GET /api/v1/sensor/metadata/calibration_statusCalibration validity flags
GET /api/v1/sensor/metadataAll metadata fields in a single response
GET /api/v1/sensor/mioMultipurpose I/O channel state (all channels)
GET /api/v1/sensor/mio/{channel}Multipurpose I/O channel state (single channel)

Sensor configuration

Read and modify sensor operating parameters. A POST to /api/v1/sensor/config applies one or more parameters simultaneously and triggers reinitialization. Individual parameters can also be targeted with GET, PUT, or DELETE on their specific path.

EndpointDescription
GET /api/v1/sensor/configActive configuration
POST /api/v1/sensor/configApply one or more configuration parameters
GET /api/v1/sensor/config/{param}Read a single configuration parameter
PUT /api/v1/sensor/config/{param}Set a single configuration parameter
DELETE /api/v1/sensor/configReset configuration to factory defaults
GET /api/v1/sensor/config/operating_modeCurrent operating mode (NORMAL or STANDBY)
PUT /api/v1/sensor/config/operating_modeSwitch operating mode

System

Restart the sensor, update firmware, and manage network settings.

EndpointDescription
POST /api/v1/system/restartRestart or reinitialize the sensor
GET /api/v1/system/firmwareInstalled firmware version
POST /api/v1/system/firmwareUpload and apply a new firmware image
GET /api/v1/system/networkFull network configuration
GET /api/v1/system/network/ipv4IPv4 address and DHCP status
PUT /api/v1/system/network/ipv4/overrideSet a static IPv4 address
DELETE /api/v1/system/network/ipv4/overrideRemove the static IP and revert to DHCP
PUT /api/v1/system/network/speed_overrideOverride link speed
DELETE /api/v1/system/network/speed_overrideRemove link speed override

Time

Query PTP and system time synchronization state.

EndpointDescription
GET /api/v1/timeCombined sensor and system time info
GET /api/v1/time/sensorSensor timestamp and sync mode
GET /api/v1/time/systemHost system clock info
GET /api/v1/time/ptpPTP synchronization status
GET /api/v1/time/ptp/profileActive PTP profile
PUT /api/v1/time/ptp/profileSet PTP profile

Alerts and diagnostics

Retrieve active and historical alerts, download a full diagnostics bundle, and read live telemetry.

EndpointDescription
GET /api/v1/sensor/alertsFull alert log
GET /api/v1/sensor/alerts?cursor=<n>Alert log starting from cursor position
GET /api/v1/sensor/alerts?mode=summaryActive alerts only
GET /api/v1/diagnostics/dumpComplete diagnostics archive (attach to support requests)
GET /api/v1/sensor/telemetryLive telemetry snapshot

Quick example

Retrieve sensor info and apply a configuration change in two commands:

# Read sensor info
curl http://os-992244000006.local/api/v1/sensor/metadata/sensor_info
# Set lidar mode to 1024x10 and point UDP output at a host
curl --request POST \
--url http://os-992244000006.local/api/v1/sensor/config \
--header "Content-Type: application/json" \
--data '{"lidar_mode": "1024x10", "udp_dest": "192.0.2.1"}'

User-editable data

Firmware v3.1 added a user-editable data store (/api/v1/user/data) for embedding arbitrary metadata on the sensor — calibration notes, site tags, asset IDs, or any other ASCII/Unicode string up to 128 KB. This data persists across reboots and is independent of sensor configuration.

TCP API (deprecated)

The TCP API was deprecated in firmware v3.1. All supported functionality is available through the HTTP API. Contact Ouster Support if you need guidance migrating from the TCP API.