ouster.sdk.pcap.pcap module¶
Copyright (c) 2021, Ouster, Inc. All rights reserved.
- record(packets, pcap_path, *, src_ip='127.0.0.1', dst_ip='127.0.0.1', lidar_port=7502, imu_port=7503, zm_port=7504, use_sll_encapsulation=False)[source]¶
Record a sequence of sensor packets to a pcap file.
- Parameters:
packets (
Iterable[Packet]) – A (finite!) sequence of packetspcap_path (
str) – Path of the output pcap filesrc_ip (
str) – Source IP to use for all packetsdst_ip (
str) – Destination IP to use for all packetslidar_port (
int) – Src/dst port to use for lidar packetsimu_port (
int) – Src/dst port to use for imu packetsuse_sll_encapsulation (
bool) – Use sll encapsulationzm_port (int)
- Return type:
int- Returns:
Number of packets captured