ouster.sdk.examples.colormaps module¶
Copyright (c) 2021, Ouster, Inc. All rights reserved.
Ouster spezia colormap
- colorize(image)[source]¶
Use Ouster spezia colormap to get from gray to color space.
- Parameters:
image (
ndarray) – 2D array of values in the range [0, 1]- Returns:
Array of RGB values of the same dimension selected from the color map
- normalize(data, percentile=0.05)[source]¶
Normalize and clamp data for better color mapping.
This is a utility function used ONLY for the purpose of 2D image visualization. The resulting values are not fully reversible because the final clipping step discards values outside of [0, 1].
- Parameters:
data (
ndarray) – array of data to be transformed for visualizationpercentile (
float) – values in the bottom/top percentile are clamped to 0 and 1
- Returns:
An array of doubles with the same shape as
imagewith values normalized to the range [0, 1].