ouster.sdk.core.data module¶
Copyright (c) 2021, Ouster, Inc. All rights reserved.
- BufferT¶
Types that support the buffer protocol.
alias of
bytes|bytearray|memoryview|ndarray
- class ChanField[source]¶
Bases:
object- RANGE = 'RANGE'¶
- RANGE2 = 'RANGE2'¶
- SIGNAL = 'SIGNAL'¶
- SIGNAL2 = 'SIGNAL2'¶
- R = 'R'¶
- G = 'G'¶
- B = 'B'¶
- RGB = 'RGB'¶
- REFLECTIVITY = 'REFLECTIVITY'¶
- REFLECTIVITY2 = 'REFLECTIVITY2'¶
- NEAR_IR = 'NEAR_IR'¶
- FLAGS = 'FLAGS'¶
- FLAGS2 = 'FLAGS2'¶
- WINDOW = 'WINDOW'¶
- ZONE = 'ZONE'¶
- RAW_HEADERS = 'RAW_HEADERS'¶
- RAW32_WORD1 = 'RAW32_WORD1'¶
- RAW32_WORD2 = 'RAW32_WORD2'¶
- RAW32_WORD3 = 'RAW32_WORD3'¶
- RAW32_WORD4 = 'RAW32_WORD4'¶
- RAW32_WORD5 = 'RAW32_WORD5'¶
- RAW32_WORD6 = 'RAW32_WORD6'¶
- RAW32_WORD7 = 'RAW32_WORD7'¶
- RAW32_WORD8 = 'RAW32_WORD8'¶
- RAW32_WORD9 = 'RAW32_WORD9'¶
- NORMALS = 'NORMALS'¶
- NORMALS2 = 'NORMALS2'¶
- GROUND = 'GROUND'¶
- GROUND2 = 'GROUND2'¶
- IMU_ACC = 'IMU_ACC'¶
- IMU_GYRO = 'IMU_GYRO'¶
- IMU_TIMESTAMP = 'IMU_TIMESTAMP'¶
- IMU_MEASUREMENT_ID = 'IMU_MEASUREMENT_ID'¶
- IMU_STATUS = 'IMU_STATUS'¶
- IMU_PACKET_TIMESTAMP = 'IMU_PACKET_TIMESTAMP'¶
- IMU_ALERT_FLAGS = 'IMU_ALERT_FLAGS'¶
- POSITION_STRING = 'POSITION_STRING'¶
- POSITION_LAT_LONG = 'POSITION_LAT_LONG'¶
- POSITION_TIMESTAMP = 'POSITION_TIMESTAMP'¶
- LIVE_ZONESET_HASH = 'LIVE_ZONESET_HASH'¶
- ZONE_TIMESTAMP = 'ZONE_TIMESTAMP'¶
- ZONE_PACKET_TIMESTAMP = 'ZONE_PACKET_TIMESTAMP'¶
- ZONE_STATES = 'ZONE_STATES'¶
- ZONE_ALERT_FLAGS = 'ZONE_ALERT_FLAGS'¶
- class ColHeader(value, names=<not given>, *values, module=None, qualname=None, type=None, start=1, boundary=None)[source]¶
Bases:
EnumColumn headers available in lidar data.
This definition is deprecated.
- TIMESTAMP = 0¶
- ENCODER_COUNT = 1¶
- MEASUREMENT_ID = 2¶
- STATUS = 3¶
- FRAME_ID = 4¶
- stagger(info, fields)[source]¶
Return a staggered copy of the provided fields.
In the default staggered representation, each column corresponds to a single timestamp. A destaggered representation compensates for the azimuth offset of each beam, returning columns that correspond to a single azimuth angle.
- Parameters:
info (
SensorInfo) – Sensor metadata associated with the provided datafields (
ndarray) – A numpy array of shape H X W or H X W X N
- Return type:
ndarray- Returns:
A staggered numpy array of the same shape