from typing import Any, Tuple, Union
import numpy as np
from ouster.sdk.viz import PointViz, Image, Label, Mesh, Cloud
[docs]
class Toggle:
def __init__(self, viz: PointViz, item: Any, initially_visible: bool = False):
self._viz = viz
self._item = item
self._visible = False
self.visible = initially_visible
[docs]
def hide(self):
self.visible = False
[docs]
def show(self):
self.visible = True
[docs]
def toggle(self):
self.visible = not self.visible
@property
def visible(self) -> bool:
return self._visible
@visible.setter
def visible(self, visible: bool):
"""Depending on the visible parameter,
add or remove the image from the PointViz
depending on whether it's already added or removed."""
if visible and not self._visible:
self._viz.add(self._item)
if not visible and self._visible:
self._viz.remove(self._item)
self._visible = visible
[docs]
class ToggleImage(Toggle):
"""
This class encapsulates properties of an image, such as whether it is visible in the supplied PointViz instance.
This makes up for a deficiency in PointViz which requires that API users remember whether
a widget has been added or not.
"""
def __init__(self, viz: PointViz, initially_visible: bool = False):
self._image = Image()
super().__init__(viz, self._image, initially_visible)
self._hshift = 0.0
self._position = (0.0, 0.0, 0.0, 0.0)
[docs]
def set_image(self, image: np.ndarray):
self._image.set_image(image)
@property
def hshift(self):
return self._hshift
@hshift.setter
def hshift(self, hshift: float):
self._hshift = hshift
self._image.set_hshift(hshift)
@property
def position(self):
return self._position
@position.setter
def position(self, position: Tuple[float, float, float, float]):
self._position = position
self._image.set_position(*self._position)
[docs]
class ToggleLabel(Toggle):
"""
This class encapsulates properties of a label, such as whether it is visible in the supplied PointViz instance.
This makes up for a deficiency in PointViz which requires that API users remember whether
a widget has been added or not.
"""
def __init__(
self, viz: PointViz,
initial_text: str,
initial_position: Union[Tuple[float, float], Tuple[float, float, float]],
initially_visible: bool = False,
align_right: bool = False,
align_top: bool = False,
):
self._position = initial_position
self._scale = 1.0
self._text = initial_text
self._rgba = (1, 1, 1, 1)
if len(initial_position) == 2:
self._label = Label(initial_text, initial_position[0], initial_position[1], align_right, align_top)
elif len(initial_position) == 3:
self._label = Label(initial_text, *initial_position)
super().__init__(viz, self._label, initially_visible)
@property
def text(self):
return self._text
@text.setter
def text(self, text: str):
self._label.set_text(text)
@property
def scale(self):
return self._scale
@scale.setter
def scale(self, scale: float):
self._scale = scale
self._label.set_scale(scale)
@property
def position(self):
return self._position
@position.setter
def position(self, position: Union[Tuple[float, float], Tuple[float, float, float]]):
self._position = position
self._label.set_position(*self._position)
@property
def text_height(self):
return self._label.text_height
@property
def rgba(self):
return self._rgba
@rgba.setter
def rgba(self, rgba: Tuple[float, float, float, float]):
self._label.set_rgba(rgba)
[docs]
class ToggleMesh(Toggle):
def __init__(self, viz: PointViz, mesh: Mesh, initially_visible: bool = False):
super().__init__(viz, mesh, initially_visible)
[docs]
class ToggleCloud(Toggle):
def __init__(self, viz: PointViz, cloud: Cloud, initially_visible: bool = False):
super().__init__(viz, cloud, initially_visible)