Source code for ouster.sdk.viz.view_mode

from typing import (List, Optional, Union, Protocol, runtime_checkable, Tuple)

from dataclasses import dataclass
import numpy as np
from ouster.sdk import core
from ouster.sdk.core import (Version, AutoExposure, BeamUniformityCorrector,
                             LocalToneMapper)

from ouster.sdk._bindings.viz import Cloud, Image


[docs] @runtime_checkable class FieldViewMode(Protocol): """LidarFrame field processor View modes define the process of getting the key data for the frame and return number as well as checks the possibility of showing data in that mode, see `enabled()`. """ _info: Optional[core.SensorInfo] @property def name(self) -> str: """Name of the view mode""" ... @property def names(self) -> List[str]: """Name of the view mode per return number""" ... def _prepare_data(self, ls: core.LidarFrame, return_num: int = 0) -> Optional[np.ndarray]: """Prepares data for visualization given the frame and return number""" ...
[docs] def enabled(self, ls: core.LidarFrame, return_num: int = 0) -> bool: """Checks the view mode availability for a frame and return number""" ...
[docs] @runtime_checkable class ImageMode(FieldViewMode, Protocol): """Applies the view mode key to the viz.Image"""
[docs] def set_image(self, img: Image, ls: core.LidarFrame, return_num: int = 0) -> None: """Prepares the key data and sets the image key to it.""" ...
[docs] @runtime_checkable class CloudMode(FieldViewMode, Protocol): """Applies the view mode key to the viz.Cloud"""
[docs] def set_cloud_color(self, cloud: Cloud, ls: core.LidarFrame, *, return_num: int = 0) -> None: """Prepares the key data and sets the cloud key to it.""" ...
[docs] class ImageCloudMode(ImageMode, CloudMode, Protocol): """Applies the view mode to viz.Cloud and viz.Image""" pass
def _second_chan_field(field: str) -> Optional[str]: """Get the second return field name.""" # yapf: disable second_fields = dict({ core.ChanField.RANGE: core.ChanField.RANGE2, core.ChanField.SIGNAL: core.ChanField.SIGNAL2, core.ChanField.REFLECTIVITY: core.ChanField.REFLECTIVITY2, core.ChanField.FLAGS: core.ChanField.FLAGS2, core.ChanField.NORMALS: core.ChanField.NORMALS2, core.ChanField.GROUND: core.ChanField.GROUND2 }) # yapf: enable return second_fields.get(field, None)
[docs] class RingMode(CloudMode): """View mode to show laser ring.""" def __init__(self, info: core.SensorInfo) -> None: """ Args: info: sensor metadata """ self._info = info self._key_data: Optional[np.ndarray] = None @property def name(self) -> str: return "RING" @property def names(self) -> List[str]: return ["RING"] def _prepare_data(self, ls: core.LidarFrame, return_num: int = 0) -> Optional[np.ndarray]: if self._key_data is None: key_data = np.empty((self._info.h, self._info.w), dtype=np.uint8) for i in range(0, self._info.h): key_data[i, :] = int((i / self._info.h) * 255.0) self._key_data = key_data return self._key_data
[docs] def set_cloud_color(self, cloud: Cloud, ls: core.LidarFrame, return_num: int = 0) -> None: self._prepare_data(ls, return_num) assert self._key_data is not None cloud.set_key(self._key_data)
[docs] def enabled(self, ls: core.LidarFrame, return_num: int = 0): return True
[docs] class SensorMode(CloudMode): """View mode to show sensor index.""" def __init__(self, info: core.SensorInfo, color: Tuple[int, int, int]) -> None: """ Args: info: sensor metadata """ self._info = info self._color = color self._key_data: Optional[np.ndarray] = None @property def name(self) -> str: return "SENSOR" @property def names(self) -> List[str]: return ["SENSOR"] def _prepare_data(self, ls: core.LidarFrame, return_num: int = 0) -> Optional[np.ndarray]: if self._key_data is None: self._key_data = np.empty((self._info.h, self._info.w, 3), dtype=np.uint8) self._key_data[:] = self._color return self._key_data
[docs] def set_cloud_color(self, cloud: Cloud, ls: core.LidarFrame, return_num: int = 0) -> None: self._prepare_data(ls, return_num) assert self._key_data is not None cloud.set_key(self._key_data)
[docs] def enabled(self, ls: core.LidarFrame, return_num: int = 0): return True
[docs] class TimestampMode(CloudMode): """View mode to show column timestamp.""" def __init__(self, info: core.SensorInfo) -> None: """ Args: info: sensor metadata """ self._info = info @property def name(self) -> str: return "TIMESTAMP" @property def names(self) -> List[str]: return ["TIMESTAMP"] def _prepare_data(self, ls: core.LidarFrame, return_num: int = 0) -> Optional[np.ndarray]: nonzero = np.nonzero(ls.status) min = np.min(ls.timestamp[nonzero]) timestamps = (ls.timestamp - min).astype(np.float32, copy=True) delta = np.max(ls.timestamp) - min # handle case when all points have same value to avoid divide by zero if delta <= 0: delta = 1.0 timestamps /= delta key_data = np.tile(timestamps, (ls.h, 1)) return key_data
[docs] def set_cloud_color(self, cloud: Cloud, ls: core.LidarFrame, return_num: int = 0) -> None: key_data = self._prepare_data(ls, return_num) if key_data is not None: cloud.set_key(key_data)
[docs] def enabled(self, ls: core.LidarFrame, return_num: int = 0): return True
[docs] class SimpleMode(ImageCloudMode): """Basic view mode with AutoExposure and BeamUniformityCorrector Handles single and dual returns frames. When AutoExposure is enabled its state updates only for return_num=0 but applies for both returns. """ def __init__(self, field: str, *, info: Optional[core.SensorInfo] = None, prefix: Optional[str] = "", suffix: Optional[str] = "", use_ae: bool = True, use_buc: bool = False, scale: Optional[float] = None, zero_invalid: bool = False) -> None: """ Args: info: sensor metadata used mainly for destaggering here field: name of field to process, second return is handled automatically prefix: name prefix suffix: name suffix use_ae: if True, use AutoExposure for the field use_buc: if True, use BeamUniformityCorrector for the field scale: if use_ae is false and this is set, use this to scale the values for display zero_invalid: if true, only allow 0 to map to zero """ self._info = info self._fields = [field] field2 = _second_chan_field(field) if field2: self._fields.append(field2) self._ae = AutoExposure() if use_ae else None self._buc = BeamUniformityCorrector() if use_buc else None self._prefix = f"{prefix}: " if prefix else "" self._suffix = f" ({suffix})" if suffix else "" self._wrap_name = lambda n: f"{self._prefix}{n}{self._suffix}" self._scale = scale self._zero_invalid = zero_invalid @property def name(self) -> str: return self._wrap_name(str(self._fields[0])) @property def names(self) -> List[str]: return [self._wrap_name(str(f)) for f in self._fields] def _prepare_data(self, ls: core.LidarFrame, return_num: int = 0) -> Optional[np.ndarray]: if not self.enabled(ls, return_num): return None f = self._fields[return_num] field = ls.field(f) key_data = field.astype(np.float32, copy=True) if self._buc: self._buc.update(key_data) if self._ae: self._ae.update(key_data, update_state=(return_num == 0)) elif self._scale is not None: key_data *= self._scale else: key_max = np.max(key_data) if key_max: key_data = key_data / key_max if self._zero_invalid: key_data = np.maximum(key_data, 1.01 / 255) key_data[field == 0] = 0 return key_data
[docs] def set_image(self, img: Image, ls: core.LidarFrame, return_num: int = 0) -> None: if self._info is None: raise ValueError( f"VizMode[{self.name}] requires metadata to make a 2D image") key_data = self._prepare_data(ls, return_num) if key_data is not None: img.set_image(core.destagger(self._info, key_data))
[docs] def set_cloud_color(self, cloud: Cloud, ls: core.LidarFrame, return_num: int = 0) -> None: key_data = self._prepare_data(ls, return_num) if key_data is not None: cloud.set_key(key_data)
[docs] def enabled(self, ls: core.LidarFrame, return_num: int = 0): return (self._fields[return_num] in ls.fields if return_num < len(self._fields) else False)
[docs] class RGBMode(ImageCloudMode): """RGB view mode""" def __init__(self, field: str, *, info: Optional[core.SensorInfo] = None) -> None: """ Args: info: sensor metadata used mainly for destaggering here field: channel field to process """ self._info = info self._field = field @property def name(self) -> str: return self._field @property def names(self) -> List[str]: return [self._field] def _prepare_data(self, ls: core.LidarFrame, return_num: int = 0) -> Optional[np.ndarray]: field = ls.field(self._field) if np.ndim(field) != 3 and field.shape != 3: raise TypeError(f"Unsupport field shape: {field.shape}") if field.dtype == np.uint8: return field elif field.dtype == np.uint16: return (field >> 8).astype(np.uint8) elif field.dtype == np.float32: key_data = field elif field.dtype == np.float64: key_data = field.astype(np.float32, copy=True) else: raise TypeError(f"Unsupport field type {field.dtype}") return key_data.clip(0, 1.0)
[docs] def set_image(self, img: Image, ls: core.LidarFrame, return_num: int = 0) -> None: if self._info is None: raise ValueError( f"VizMode[{self.name}] requires metadata to make a 2D image") key_data = self._prepare_data(ls) if key_data is not None: img.set_image(core.destagger(self._info, key_data))
[docs] def set_cloud_color(self, cloud: Cloud, ls: core.LidarFrame, return_num: int = 0) -> None: key_data = self._prepare_data(ls) if key_data is not None: cloud.set_key(key_data)
[docs] def enabled(self, ls: core.LidarFrame, return_num: int = 0): field = ls.field(self._field) return np.ndim(field) == 3
[docs] class HDRRGBMode(ImageCloudMode): """RGB view mode using LocalToneMapper.""" def __init__(self, field: str, info: core.SensorInfo) -> None: self._info = info self._field = field self._tonemapper = LocalToneMapper() self._last_frame: Optional[core.LidarFrame] = None self._last_data: Optional[np.ndarray] = None @property def name(self) -> str: return self._field @property def names(self) -> List[str]: return [self._field] def _prepare_data(self, ls: core.LidarFrame, return_num: int = 0) -> Optional[np.ndarray]: if not self.enabled(ls, return_num): return None if ls is self._last_frame: return self._last_data self._last_frame = ls field = ls.field(self._field) if field.dtype != np.float16: raise TypeError(f"Unsupported field type: {field.dtype}") f16_destag = core.destagger(self._info, field) sdr_destag = self._tonemapper.update(f16_destag) sdr_data = core.stagger(self._info, sdr_destag) self._last_data = sdr_data self._last_destag_data = sdr_destag return sdr_data
[docs] def set_image(self, img: Image, ls: core.LidarFrame, return_num: int = 0) -> None: if self._info is None: raise ValueError( f"VizMode[{self.name}] requires metadata to make a 2D image") key_data = self._prepare_data(ls, return_num) if key_data is not None: img.set_image(self._last_destag_data)
[docs] def set_cloud_color(self, cloud: Cloud, ls: core.LidarFrame, return_num: int = 0) -> None: key_data = self._prepare_data(ls, return_num) if key_data is not None: cloud.set_key(key_data)
[docs] def enabled(self, ls: core.LidarFrame, return_num: int = 0) -> bool: field = ls.field(self._field) return np.ndim(field) == 3 and field.shape[2] == 3
[docs] class NormalsMode(ImageCloudMode): """Normals value remap [-1, 1] -> [0, 1]""" def __init__(self, field: str, *, info: Optional[core.SensorInfo] = None) -> None: self._info = info self._fields = [field] field2 = _second_chan_field(field) if field2: self._fields.append(field2) @property def name(self) -> str: return str(self._fields[0]) @property def names(self) -> List[str]: return [str(field) for field in self._fields] def _prepare_data(self, ls: core.LidarFrame, return_num: int = 0) -> Optional[np.ndarray]: if not self.enabled(ls, return_num): return None field = self._fields[return_num] data = ls.field(field) if np.ndim(data) != 3 or data.shape[-1] != 3: raise TypeError(f"Unsupported normal field shape: {data.shape}") key_data = np.asarray(data, dtype=np.float32) zero_mask = np.all(key_data == 0.0, axis=-1) np.clip(key_data, -1.0, 1.0, out=key_data) key_data = 0.5 * (key_data + 1.0) if np.any(zero_mask): key_data[zero_mask] = 0.0 return key_data
[docs] def set_image(self, img: Image, ls: core.LidarFrame, return_num: int = 0) -> None: if self._info is None: raise ValueError( f"VizMode[{self.name}] requires metadata to make a 2D image") key_data = self._prepare_data(ls, return_num) if key_data is not None: img.set_image(core.destagger(self._info, key_data))
[docs] def set_cloud_color(self, cloud: Cloud, ls: core.LidarFrame, return_num: int = 0) -> None: key_data = self._prepare_data(ls, return_num) if key_data is not None: cloud.set_key(key_data)
[docs] def enabled(self, ls: core.LidarFrame, return_num: int = 0): if return_num >= len(self._fields): return False field = self._fields[return_num] if field not in ls.fields: return False data = ls.field(field) return np.ndim(data) == 3 and data.shape[-1] == 3
[docs] class ReflMode(SimpleMode, ImageCloudMode): """Prepares image/cloud data for REFLECTIVITY channel""" def __init__(self, *, info: Optional[core.SensorInfo] = None) -> None: super().__init__(core.ChanField.REFLECTIVITY, info=info, use_ae=True) # used only for uncalibrated reflectivity in FW prior v2.1.0 # TODO: should we check for calibrated reflectivity status from # metadata too? if self._info is not None: self._normalized_refl = (self._info.get_version() >= Version.from_string("v2.1.0")) else: # NOTE/TODO[pb]: ReflMode added through viz extra mode mechanism # may not have a correct normalized_refl set ... need a refactor. self._normalized_refl = True def _prepare_data(self, ls: core.LidarFrame, return_num: int = 0) -> Optional[np.ndarray]: if not self.enabled(ls, return_num): return None f = self._fields[return_num] refl_data = ls.field(f).astype(np.float32, copy=True) if self._normalized_refl: refl_data /= 255.0 else: # mypy doesn't recognize that we always should have _ae here # so we have explicit check if self._ae: self._ae.update(refl_data, update_state=(return_num == 0)) return refl_data
[docs] def is_norm_reflectivity_mode(mode: FieldViewMode) -> bool: """Checks whether the image/cloud mode is a normalized REFLECTIVITY mode """ # NOTE[pb]: This is highly implementation specific and doesn't look nicely, # i.e. it's more like duck/duct plumbing .... but suits the need. return (isinstance(mode, ReflMode) and mode._normalized_refl)
LidarFrameVizMode = Union[ImageCloudMode, ImageMode, CloudMode] """Field view mode types"""
[docs] @dataclass class CloudPaletteItem: """Palette with a name""" name: str palette: np.ndarray