Source code for ouster.sdk.viz.model

"""
Copyright (c) 2021, Ouster, Inc.
All rights reserved.

Types for managing visualization state.
"""

import copy
import threading
import weakref
from queue import LifoQueue
from dataclasses import dataclass
from functools import partial
import numpy as np
from typing import Any, Callable, Dict, List, Optional, Set, Tuple

from .view_mode import (ImageMode, CloudMode, LidarFrameVizMode,
                        SimpleMode, ReflMode, RGBMode,
                        HDRRGBMode,
                        NormalsMode, RingMode, TimestampMode,
                        is_norm_reflectivity_mode, CloudPaletteItem, SensorMode)
from ouster.sdk._bindings.viz import (Cloud, Image, Label, PointViz, Mesh, Cuboid,
                   ObjectOverlay,
                   calref_palette, spezia_palette, spezia_cal_ref_palette, grey_palette,
                   grey_cal_ref_palette, viridis_palette, viridis_cal_ref_palette,
                   magma_palette, magma_cal_ref_palette, MouseButton, MouseButtonEvent,
                   EventModifierKeys, WindowCtx)
import ouster.sdk.core as core
from ouster.sdk.core import (ChanField, FrameSet)
from ouster.sdk.util import img_aspect_ratio
from .widgets import ToggleImage, ToggleLabel, ToggleMesh
from ouster.sdk.core import ZONE_OCCUPANCY_FIELDNAME, ZONE_STATES_FIELDNAME, \
    CoordinateFrame, ClassMapSet, first_valid_column_pose
from ouster.sdk.viz.mesh import clouds_from_zrb, voxel_style_mesh_from_zrb
from ouster.sdk._bindings.viz import precompute_voxel_vertices
from ouster.sdk._deprecation import deprecated_alias
from enum import Enum


[docs] class ZoneSelectionMode(Enum): NONE = 0 LIVE = 1 ALL = 2
[docs] class ZoneRenderMode(Enum): STL = 0 CLOUDS = 1 STL_AND_CLOUDS = 2 VOXEL_MESH = 3
[docs] class ObjectColorMode(Enum): OBJECT_ID = 0 OBJECT_CLASS = 1
[docs] class ObjectViewMode(Enum): OVERLAY_AND_MAIN_VIEW = 0 OVERLAY_ONLY = 1 MAIN_VIEW_ONLY = 2 NONE = 3
def _flatten(xss: List[List[Any]]) -> List[Any]: """Flattens a list of lists.""" return [x for xs in xss for x in xs] def _sync_object_pose_from_frame(obj: core.Object, frame: core.LidarFrame) -> None: """Update an object's body-to-world pose from the frame at its timestamp.""" if obj.timestamp == 0: return try: obj.body_to_world = core.pose_at_timestamp(frame, obj.timestamp) except ValueError: pass def _object_for_overlay_cuboid(obj: core.Object, frame: core.LidarFrame) -> core.Object: """Return an object whose pose is dewarped for the 2D panorama overlay.""" if obj.timestamp == 0: return obj pose_ref = core.Pose(first_valid_column_pose(frame)) overlay_obj = copy.copy(obj) overlay_obj.body_to_world = pose_ref return overlay_obj
[docs] @dataclass class ImgModeItem: """Image mode for specific return with explicit name.""" mode: ImageMode name: str return_num: int = 0
[docs] @dataclass class VizExtraMode: """Image/Cloud mode factory func Used to embed viz modes from external plugins. """ func: Callable[[], LidarFrameVizMode]
[docs] def create(self, info: Optional[core.SensorInfo] = None) -> LidarFrameVizMode: extra_mode = self.func() if info and hasattr(extra_mode, "_info") and extra_mode._info is None: extra_mode._info = info return extra_mode
# Viz modes added externally _viz_extra_modes: List[VizExtraMode] _viz_extra_modes = [] # Viz palettes added externally _viz_extra_palettes: List[CloudPaletteItem] _viz_extra_palettes = [] def _hsv_to_rgb(H, S, V): ''' Converts an integer HSV tuple (value range from 0 to 255) to an RGB tuple ''' # Check if the color is Grayscale if S == 0: return (V, V, V) # Make hue 0-5 region = H // 43 # Find remainder part, make it from 0-255 remainder = (H - (region * 43)) * 6 # Calculate temp vars, doing integer multiplication P = (V * (255 - S)) >> 8 Q = (V * (255 - ((S * remainder) >> 8))) >> 8 T = (V * (255 - ((S * (255 - remainder)) >> 8))) >> 8 # Assign temp vars based on color cone region if region == 0: return (V, T, P) elif region == 1: return (Q, V, P) elif region == 2: return (P, V, T) elif region == 3: return (P, Q, V) elif region == 4: return (T, P, V) else: return (V, P, Q) # Generate a rainbow palette rainbow_palette = np.zeros((256, 3), np.float32) for i in range(0, 256): res = _hsv_to_rgb(int(i * 230 / 255), 255, 255) rainbow_palette[i, 0] = res[0] / 255 rainbow_palette[i, 1] = res[1] / 255 rainbow_palette[i, 2] = res[2] / 255 discrete_rainbow_palette = rainbow_palette[::len(rainbow_palette) // 36] # Generate a B/W palette for images with a special case for 0 image_bw_palette = np.zeros((256, 3), np.float32) for i in range(1, 256): image_bw_palette[i, :] = 0.1 + 0.9 * (i - 1) / 254
[docs] class Palettes: """Represents the color palettes used within an instance of LidarFrameViz. Also keeps track of the palette currently in use.""" def __init__(self, _ext_palettes: List[CloudPaletteItem]): """Initialize a Palettes object, which populates two lists of palettes - one for normal view modes and one for ReflMode.""" # Note these 2 palette arrays must always be the same length self._cloud_palettes: List[CloudPaletteItem] self._cloud_palettes = [ CloudPaletteItem("Cal. Ref", calref_palette), CloudPaletteItem("Ouster Colors", spezia_palette), CloudPaletteItem("Greyscale", grey_palette), CloudPaletteItem("Viridis", viridis_palette), CloudPaletteItem("Magma", magma_palette), CloudPaletteItem("Rainbow", rainbow_palette) ] self._refl_cloud_palettes: List[CloudPaletteItem] self._refl_cloud_palettes = [ CloudPaletteItem("Cal. Ref", calref_palette), CloudPaletteItem("Cal. Ref. Ouster Colors", spezia_cal_ref_palette), CloudPaletteItem("Cal. Ref. Greyscale", grey_cal_ref_palette), CloudPaletteItem("Cal. Ref. Viridis", viridis_cal_ref_palette), CloudPaletteItem("Cal. Ref. Magma", magma_cal_ref_palette), CloudPaletteItem("Rainbow", rainbow_palette) ] # Add extra color palettes, usually inserted through plugins self._cloud_palettes.extend(_viz_extra_palettes) self._refl_cloud_palettes.extend(_viz_extra_palettes) self._cloud_palettes.extend(_ext_palettes or []) self._refl_cloud_palettes.extend(_ext_palettes or []) # the index of the current palette used for the clouds self._cloud_palette_ind = 0 assert len(self._cloud_palettes) == len(self._refl_cloud_palettes)
[docs] def set_palette(self, index: int) -> None: """Set the current palette index.""" assert len(self._cloud_palettes) == len(self._refl_cloud_palettes) assert self._cloud_palette_ind >= 0 and self._cloud_palette_ind < len(self._cloud_palettes) self._cloud_palette_ind = index
[docs] def cycle_cloud_palette(self, direction: int) -> None: """Updates the current palette to use.""" assert len(self._cloud_palettes) == len(self._refl_cloud_palettes) self.set_palette((self._cloud_palette_ind + direction) % len(self._cloud_palettes))
[docs] def get_palette(self, cloud_mode: CloudMode) -> CloudPaletteItem: """Gets the current color palette depending on the view mode.""" assert len(self._cloud_palettes) == len(self._refl_cloud_palettes) refl_mode = is_norm_reflectivity_mode(cloud_mode) if refl_mode: return self._refl_cloud_palettes[self._cloud_palette_ind] else: return self._cloud_palettes[self._cloud_palette_ind]
[docs] def get_palette_by_name(self, name: str) -> CloudPaletteItem: for palette in self._cloud_palettes: if palette.name == name: return palette raise KeyError(name)
[docs] def get_current_palette(self) -> CloudPaletteItem: """Gets the name of the current palette.""" return self._cloud_palettes[self._cloud_palette_ind]
[docs] def triggered_live_zone_color(palette, zone_id): return (*palette[(int(zone_id) * 20) % palette.shape[0]], 1)
[docs] class Selection2d: def __init__(self, p1: Tuple[int, int], p2: Tuple[int, int], sensor_index: int, sensor: 'SensorModel', image_index: int, image: Image): self._p1 = p1 self._p2 = p2 self._sensor_index = sensor_index self._sensor = sensor self._image_index = image_index self._image = image self._update_mask() self._finalized = False @property def sensor(self): return self._sensor @property def finalized(self): return self._finalized
[docs] def finalize(self): self._finalized = True
def __str__(self): return f'2d selection {self._p1} - {self._p2}' @property def p1(self): return self._p1 @p1.setter def p1(self, p1): self._p1 = p1 self._update_mask() @property def p2(self): return self._p2 @p2.setter def p2(self, p2): self._p2 = p2 self._update_mask() def _update_mask(self): min_x = min(self.p1[0], self.p2[0]) max_x = max(self.p1[0], self.p2[0]) min_y = min(self.p1[1], self.p2[1]) max_y = max(self.p1[1], self.p2[1]) self._aoi_mask = np.zeros((self._sensor._meta.h, self._sensor._meta.w), np.float32) self._aoi_mask[min_x:max_x, min_y:max_y] = 1 @property def area(self) -> int: """ Calculates and returns the area of the rectangular selection. The area is calculated as the absolute difference between the x and y coordinates, ensuring a positive result regardless of the points' order. """ x1, y1 = self._p1 x2, y2 = self._p2 width = abs(x2 - x1) height = abs(y2 - y1) return width * height
_colors = [] _colors.append((255, 0, 0)) _colors.append((255, 255, 0)) _colors.append((255, 0, 255)) _colors.append((0, 255, 255)) _colors.append((0, 0, 255)) _colors.append((0, 255, 0)) _colors.append((255, 255, 255)) _colors.append((255, 191, 0)) _colors.append((0, 120, 0)) _zero_invalid_fields = ["NEAR_IR", "SIGNAL", "REFLECTIVITY", "RANGE", "WINDOW"]
[docs] class SensorModel: """ A model object representing viz state for a single sensor. """ def __init__(self, viz: PointViz, meta, *, _img_aspect_ratio: float = 0, palettes: Palettes = Palettes([]), index: Optional[int] = None): self._viz = viz self._enabled = True self._meta = meta self._xyzlut = core.XYZLut(meta, use_extrinsics=True) self._palettes = palettes self._zone_palette = palettes.get_palette_by_name('Rainbow').palette self._num_clouds = 2 self._clouds: List[Cloud] = [] self._cloud_masks: List[np.ndarray] = [] for i in range(self._num_clouds): self._clouds.append(Cloud(self._xyzlut)) mask = np.zeros((meta.h, meta.w, 4), dtype=np.uint8) mask[:, :, 1] = 255 self._cloud_masks.append(mask) self._cloud_modes: Dict[str, CloudMode] = {} self._selected_pts: Dict[int, np.ndarray] = {} self._selecting_pts: Dict[int, np.ndarray] = {} for idx, cloud in enumerate(self._clouds): def cb(ret_idx, selected_pts, pts): # update our list of selected points # note, be careful to not capture the viz (even indirectly) here # or it creates a weird reference leak selected_pts[ret_idx] = pts cloud.set_on_select(partial(cb, idx, self._selecting_pts)) self._palette_dirty = [True] * len(self._clouds) self._num_images = 2 self._images: List[Image] = [] self._image_modes: Dict[str, ImgModeItem] = {} for i in range(self._num_images): self._images.append(Image()) self._object_overlay = ObjectOverlay() self._object_overlay.set_sensor_info(self._meta) if _img_aspect_ratio: self._img_aspect_ratio = _img_aspect_ratio else: self._img_aspect_ratio = img_aspect_ratio(meta) self._modes: List[LidarFrameVizMode] = [] # Add extra viz mode, usually inserted through plugins self._modes.extend([vm.create(meta) for vm in _viz_extra_modes]) self._modes.append(RingMode(meta)) self._modes.append(TimestampMode(meta)) if index is not None: self._color = _colors[index % len(_colors)] self._modes.append(SensorMode(meta, self._color)) # TODO[tws] decide whether it's necessary to provide extra modes via the constructor # self._modes.extend(_ext_modes or []) self._black_palette = np.zeros((256, 3), dtype=np.float32) self._populate_image_cloud_modes() self._image_calref_palette = copy.deepcopy(calref_palette) self._image_calref_palette[0] = [0.1, 0.1, 0.1] self._show_sky = False self._has_imu_data = False self._imu_plot = ToggleImage(viz, initially_visible=True) self._sensor_label = ToggleLabel(viz, "", (0, 1), initially_visible=True) # for the OSD self._stl_meshes = {} self._stl_mesh_labels = {} self._zrb_clouds = {} self._zrb_meshes: Dict[int, Optional[ToggleMesh]] = {} self._zone_states: Optional[np.ndarray] = None if meta.format.zone_monitoring_enabled and meta.zone_set is not None: zone_set = meta.zone_set self._voxel_vertices = precompute_voxel_vertices(self._meta) for zone_id, zone in zone_set.zones.items(): # TODO[tws] C++ if zone.stl is not None: simple_mesh = zone.stl.to_mesh() if len(simple_mesh.triangles) < 1: print(f"Warning: mesh for zone {zone_id} is invalid.") continue mesh = Mesh.from_simple_mesh(simple_mesh) sensor_to_body_transform = zone_set.sensor_to_body_transform \ if zone.stl.coordinate_frame == CoordinateFrame.BODY else np.eye(4) zone_transform = meta.sensor_to_body @ np.linalg.inv(sensor_to_body_transform) mesh.set_transform(zone_transform) mesh_widget = ToggleMesh(viz, mesh, initially_visible=True) self._stl_meshes[zone_id] = mesh_widget # TODO[tws] bind a method for viz::Mesh to return points, or perhaps the centroid mesh_label_pos = ( # TODO[tws] dedupe simple_mesh.triangles[0].coords[0][0], simple_mesh.triangles[0].coords[0][1], simple_mesh.triangles[0].coords[0][2], 1 ) mesh_label_pos = zone_transform.dot(mesh_label_pos) mesh_label = ToggleLabel(viz, '', mesh_label_pos[0:3], initially_visible=False) mesh_label.scale = 0.20 self._stl_mesh_labels[zone_id] = mesh_label if zone.zrb is not None: self._zrb_clouds[zone_id] = clouds_from_zrb(viz, zone.zrb, self._xyzlut) self._zrb_meshes[zone_id] = None # created on demand def _clear_aois(self) -> None: self._selected_pts.clear() def _populate_image_cloud_modes(self) -> None: # TODO[tws] de-duplicate with logic in _amend_view_modes self._image_modes = {name: ImgModeItem(mode, name, num) for mode in self._modes if isinstance(mode, ImageMode) for num, name in enumerate(mode.names) } self._cloud_modes = {m.name: m for m in self._modes if isinstance(m, CloudMode)} @staticmethod def _get_field_class_for_field_name(field_name, frame) -> Optional[core.FieldType]: for field_type in frame.field_types: if field_type.name == field_name: return field_type.field_class return None def _create_view_mode_for_field(self, field_name, frame) -> Optional[LidarFrameVizMode]: """Create the appropriate view mode depending on a field's name and dimensions.""" mode: Optional[LidarFrameVizMode] = None if field_name in [ChanField.FLAGS2, ChanField.RANGE2, ChanField.REFLECTIVITY2, ChanField.SIGNAL2, ChanField.GROUND2]: return None if field_name in frame.fields: if SensorModel._get_field_class_for_field_name(field_name, frame) != core.FieldClass.PIXEL_FIELD: return None field = frame.field(field_name) f_shape = field.shape if len(f_shape) == 3 and f_shape[2] == 3: # 3D field upper_name = field_name.upper() if upper_name.startswith("NORMALS"): mode = NormalsMode(field_name, info=self._meta) elif ("RGB" in upper_name) and field.dtype == np.float16: mode = HDRRGBMode(field_name, info=self._meta) else: mode = RGBMode(field_name, info=self._meta) elif len(f_shape) == 2: zero_invalid = field_name in _zero_invalid_fields if field_name == ChanField.REFLECTIVITY: mode = ReflMode(info=self._meta) elif field_name == ChanField.NEAR_IR: mode = SimpleMode(field_name, info=self._meta, use_ae=True, use_buc=True, zero_invalid=zero_invalid) elif field_name == ChanField.WINDOW: mode = SimpleMode(field_name, info=self._meta, scale=1.0 / 255.0, use_ae=False, use_buc=False, zero_invalid=zero_invalid) else: mode = SimpleMode(field_name, info=self._meta, use_ae=True, use_buc=False, zero_invalid=zero_invalid) return mode # TODO[tws] rename def _amend_view_modes(self, frame): """ Update the available fields for this model given a frame. """ if not self._has_imu_data: # TODO[tws] set based on imu visualization config maybe? if frame.has_field('IMU_GYRO') or frame.has_field('IMU_ACC'): self._has_imu_data = True for field_name in frame.fields: # skip if view mode already exists if field_name in self._image_modes or \ field_name == ChanField.FLAGS or \ field_name == ChanField.FLAGS2: continue mode = self._create_view_mode_for_field(field_name, frame) if isinstance(mode, ImageMode): for num, name in enumerate(mode.names): self._image_modes[name] = ImgModeItem(mode, name, num) if isinstance(mode, CloudMode): self._cloud_modes[field_name] = mode
[docs] def update_cloud_palettes(self, cloud_mode_name) -> None: """Sets each cloud palette given the cloud mode name. Has no effect if the cloud mode is not available for this sensor.""" cloud_mode = self._cloud_modes.get(cloud_mode_name) if cloud_mode: palette = self._palettes.get_palette(cloud_mode) for cloud in self._clouds: cloud.set_palette(palette.palette) else: # flag to set this later if we failed self._palette_dirty = [True] * len(self._clouds)
_max_range: int = 100000
[docs] def update_cloud(self, cloud, cloud_mode, range_field: str, return_num: int, frame: Optional[core.LidarFrame]) -> None: """Updates the given Cloud with the given CloudMode.""" if frame is None: # make the frame invisible if it isnt present cloud.set_range(np.zeros((cloud.cols, cloud.size // cloud.cols), dtype=np.uint32)) return if range_field in frame.fields: range_data = frame.field(range_field) else: range_data = np.zeros((frame.h, frame.w), dtype=np.uint32) cloud.set_column_poses(frame.body_to_world.astype(np.float32)) if return_num == 0 and self._show_sky: self._max_range = max(self._max_range, np.max(range_data) + 10000) copy = np.copy(range_data) copy[range_data == 0] = self._max_range cloud.set_range(copy) else: cloud.set_range(range_data) # display the cloud as black if we are missing this chanfield if not cloud_mode: cloud.set_palette(self._black_palette) return # set palette if dirty and we have the mode if self._palette_dirty[return_num]: palette = self._palettes.get_palette(cloud_mode) cloud.set_palette(palette.palette) self._palette_dirty[return_num] = False if cloud_mode.enabled(frame, return_num): cloud_mode.set_cloud_color(cloud, frame, return_num=return_num) else: cloud_mode.set_cloud_color(cloud, frame, return_num=0)
[docs] def update_clouds(self, cloud_mode_name: str, frame: Optional[core.LidarFrame]) -> None: """Update range and mode for each cloud given a mode name and a frame.""" cloud_mode = self._cloud_modes.get(cloud_mode_name, None) for return_num, range_field in ((0, ChanField.RANGE), (1, ChanField.RANGE2)): if return_num < len(self._clouds): self.update_cloud(self._clouds[return_num], cloud_mode, range_field, return_num, frame)
[docs] def update_image(self, image, image_mode_item: ImgModeItem, frame: Optional[core.LidarFrame]) -> None: """Update the view mode of the given image.""" # TODO[tws] optimize, move to image model(?) if not frame: image.set_image(np.zeros((self._meta.h, self._meta.w), dtype=np.float32)) return refl_mode = False mode = image_mode_item.mode if mode: refl_mode = is_norm_reflectivity_mode(mode) if refl_mode: image.set_palette(self._image_calref_palette) elif mode.name in _zero_invalid_fields: # use a pallete with a special case for 0 = invalid image.set_palette(image_bw_palette) else: image.clear_palette() else: image.clear_palette() if mode is not None and mode.enabled(frame, image_mode_item.return_num): mode.set_image(image, frame, image_mode_item.return_num) else: # TODO[tws]: deduplicate, e.g. by making this a method in an image model class image.set_image(np.zeros((self._meta.h, self._meta.w), dtype=np.float32))
[docs] def update_images(self, image_mode_names: List[str], frame: Optional[core.LidarFrame]) -> None: """Update image values and mode given mode names and a frame.""" assert len(image_mode_names) == len(self._images) for i in range(len(self._images)): image_mode_item = self._image_modes.get(image_mode_names[i]) if image_mode_item: self.update_image(self._images[i], image_mode_item, frame) else: # TODO[tws]: deduplicate, e.g. by making this a method in an image model class self._images[i].set_image(np.zeros((self._meta.h, self._meta.w), dtype=np.float32))
[docs] def update_zones(self, frame: Optional[core.LidarFrame] = None) -> None: if self._meta.zone_set is None: return # TODO[tws] use >= max zone id constant here live_zone_ids: Set[int] = set() if self._zone_states is not None: live_zone_ids = {zone_state.id for zone_state in self._zone_states if zone_state.id < 255} zrb_pose: Optional[np.ndarray] = None stl_pose: Optional[np.ndarray] = None if frame is not None: try: pose = frame.body_to_world[frame.get_last_valid_column()] except RuntimeError: pose = None if pose is not None: zrb_pose = pose zrb_mesh_pose = (pose @ self._meta.sensor_to_body) stl_pose = ((pose @ self._meta.sensor_to_body) @ np.linalg.inv(self._meta.zone_set.sensor_to_body_transform)) # set mesh visibility and color for zone_id in self._stl_meshes.keys(): stl_mesh = self._stl_meshes.get(zone_id) if stl_mesh: visible = False if self._zone_render_mode in (ZoneRenderMode.STL_AND_CLOUDS, ZoneRenderMode.STL) and self._enabled: if self._zone_selection_mode == ZoneSelectionMode.ALL: visible = True elif self._zone_selection_mode == ZoneSelectionMode.LIVE and zone_id in live_zone_ids: visible = True stl_mesh.visible = visible stl_mesh_label = self._stl_mesh_labels[zone_id] stl_mesh_label.hide() if zone_id not in live_zone_ids: stl_mesh._item.set_edge_rgba((0.5, 0.5, 0.5, 0.5)) else: stl_mesh._item.set_edge_rgba((0.8, 0.8, 0.8, 0.8)) if stl_pose is not None: zone = self._meta.zone_set.zones[zone_id] if zone.stl.coordinate_frame == CoordinateFrame.BODY: stl_mesh._item.set_transform(stl_pose) else: stl_mesh._item.set_transform(zrb_mesh_pose) # set voxel mesh visibility for zone_id, zrb_mesh in self._zrb_meshes.items(): visible = False if self._zone_render_mode == ZoneRenderMode.VOXEL_MESH and self._enabled: if self._zone_selection_mode == ZoneSelectionMode.ALL: visible = True elif self._zone_selection_mode == ZoneSelectionMode.LIVE and zone_id in live_zone_ids: visible = True zone = self._meta.zone_set.zones[zone_id] if zrb_mesh is None and zone.zrb is not None: zrb_mesh = ToggleMesh( self._viz, voxel_style_mesh_from_zrb( zone.zrb, self._meta, self._voxel_vertices, False, True ) ) zrb_mesh._item.set_transform(self._meta.sensor_to_body) self._zrb_meshes[zone_id] = zrb_mesh if zrb_mesh is not None: zrb_mesh.visible = visible if zrb_pose is not None: zrb_mesh._item.set_transform(zrb_mesh_pose) # set zone clouds visibility for zone_id, (near_cloud, far_cloud) in self._zrb_clouds.items(): visible = False if self._zone_render_mode in (ZoneRenderMode.STL_AND_CLOUDS, ZoneRenderMode.CLOUDS) and self._enabled: if self._zone_selection_mode == ZoneSelectionMode.ALL: visible = True elif self._zone_selection_mode == ZoneSelectionMode.LIVE and zone_id in live_zone_ids: visible = True # TODO[tws] set cloud color near_cloud.visible = visible far_cloud.visible = visible if zrb_pose is not None: near_cloud._item.set_pose(zrb_pose) far_cloud._item.set_pose(zrb_pose) # set mesh label visibility for zone_id, stl_mesh_label in self._stl_mesh_labels.items(): visible = False if self._zone_selection_mode != ZoneSelectionMode.NONE and zone_id in live_zone_ids and self._enabled: visible = True stl_mesh_label.visible = visible # set triggered mesh color and label if self._zone_states is not None: for zone_state in self._zone_states: zone_id = zone_state.id live = bool(zone_state.live) trigger_status = zone_state.trigger_status stl_mesh = self._stl_meshes.get(zone_id) # TODO[tws] configurable colors live_color = triggered_live_zone_color(self._zone_palette, zone_id) if stl_mesh: stl_mesh_label = self._stl_mesh_labels[zone_id] if live: stl_mesh_label.text = str(zone_state.count) stl_mesh_label.rgba = live_color if trigger_status: stl_mesh._item.set_edge_rgba(live_color) else: stl_mesh_label.text = ""
[docs] def update_zone_occupancy_cloud_and_image_masks(self, frame: Optional[core.LidarFrame], palettes: Palettes): if not frame: # TODO[tws] deactivate zones / clear masks return destaggered_mask = mask = np.zeros((self._meta.h, self._meta.w, 4), dtype=np.uint8) if frame.has_field(ZONE_OCCUPANCY_FIELDNAME): occupancy = frame.field(ZONE_OCCUPANCY_FIELDNAME) # TODO[tws] consider flags mode. # TODO[tws] color mask depending on zone color? if frame.has_field(ZONE_STATES_FIELDNAME): zone_states = frame.field(ZONE_STATES_FIELDNAME) for z_idx in range(16): # TODO[tws] max live zones constant zone_state = zone_states[z_idx] zone_id = zone_state.id # TODO[tws] use >= max zone id constant here if zone_id == 255: continue bit = 0x1 << z_idx color = triggered_live_zone_color(self._zone_palette, zone_id) mask[(occupancy & bit) > 0] = np.array(color) * 255 else: for z_idx in range(16): # TODO[tws] max live zones constant bit = 0x1 << z_idx color = triggered_live_zone_color(self._zone_palette, z_idx) mask[(occupancy & bit) > 0] = np.array(color) * 255 destaggered_mask = core.destagger(self._meta, mask) self._cloud_masks[0] = mask for image in self._images: image.set_mask(destaggered_mask)
[docs] def update_object_id_cloud_and_image_masks(self, frame: Optional[core.LidarFrame], mask_palette): if not frame: return for field_name in frame.fields: if field_name.endswith("INSTANCE_ID"): mask = np.zeros((self._meta.h, self._meta.w, 4), dtype=np.uint8) oid = frame.field(field_name) has_object = oid != -1 mask[has_object] = np.dstack( ( mask_palette[oid % len(mask_palette)] * 255.0, np.ones((frame.h, frame.w)) * 255.0 ) )[has_object] destaggered_mask = core.destagger(self._meta, mask) self._cloud_masks[0] = mask for image in self._images: image.set_mask(destaggered_mask)
[docs] def hide_all_zone_geometry(self): for near_cloud, far_cloud in self._zrb_clouds.values(): near_cloud.visible = False far_cloud.visible = False for stl_mesh in self._stl_meshes.values(): stl_mesh.visible = False for stl_mesh_label in self._stl_mesh_labels.values(): stl_mesh_label.hide() for zrb_mesh in self._zrb_meshes.values(): if zrb_mesh is not None: zrb_mesh.visible = False
[docs] def set_zone_selection_and_render_mode(self, selection_mode: ZoneSelectionMode, render_mode: ZoneRenderMode): self.hide_all_zone_geometry() self._zone_selection_mode = selection_mode self._zone_render_mode = render_mode self.update_zones()
[docs] class LidarFrameVizModel: def __init__(self, viz: PointViz, metas: List[core.SensorInfo], *, _img_aspect_ratio: float): self._viz = viz self._cloud_pt_size: float = 2.0 self._metas = metas assert len(metas) > 0, "ERROR: Expecting at least one sensor" _ext_palettes: List[CloudPaletteItem] = [] # TODO[tws] implement self._palettes: Palettes = Palettes(_ext_palettes) self._sensors: List[SensorModel] = [] for idx, meta in enumerate(self._metas): # only set index (which enables sensor based coloring) if we have > 1 sensor model = SensorModel(viz, meta, _img_aspect_ratio=_img_aspect_ratio, palettes=self._palettes, index=None if len(self._metas) == 1 else idx) self._sensors.append(model) self._max_clouds = max(sensor._num_clouds for sensor in self._sensors) self._max_images = max(sensor._num_images for sensor in self._sensors) self._cloud_mode_ind: int = 0 self._cloud_mode_name: str = '' self._cloud_enabled = [True] self._image_mode_ind = [0] * self._max_images self._image_mode_names = [''] * self._max_images self._set_cloud_pt_size(self._cloud_pt_size) self._known_fields: Set[str] = set() # set of known fields self._cloud_palette_name = '' self._flags_palette = discrete_rainbow_palette self._object_color_mode = ObjectColorMode.OBJECT_ID self._object_view_mode = ObjectViewMode.OVERLAY_AND_MAIN_VIEW self._frame_set: FrameSet = FrameSet([None] * len(metas)) # Object-related self._objects: Dict[core.Object, Cuboid] = {} self._object_labels: Dict[core.Object, ToggleLabel] = {} self._class_maps: ClassMapSet = ClassMapSet({}) self._class_map_name: str = '' # AOI-related self._mouse_down_image: Optional[int] = None self._current_selection: List[Selection2d] = [] self._aoi_labels = [Label("", 0, 0) for _ in range(self._max_images)] self._3d_aoi_label = Label("", 0, 0) self._preexisting_selection: bool = False # regrettable, since images aren't always aware of the context they're rendered in self._ctx: Optional[WindowCtx] = None self._img_size_fraction = 4 self._flip_images = False self._show_one_image = False self._objects_selected = False self._move_queue: LifoQueue[Optional[Tuple]] = LifoQueue() self._queue_idx = 0 # create thread to handle selection requests in parallel self._aoi_lock = threading.RLock() def worker(mq, this): last_index = -1 while True: item = mq.get() if item is None: break self = this() idx, sx, sy, ex, ey, update = item # ignore old requests, we only want the most recent if idx < last_index: continue last_index = idx self.clear_masks() self._viz.pick(sx, sy, ex, ey) if self._objects_selected: self._viz.update() self._objects_selected = False # swap in the new selections and then update the AoIs with self._aoi_lock: for sensor in self._sensors: sensor._selected_pts.clear() for one, two in sensor._selecting_pts.items(): sensor._selected_pts[one] = two sensor._selecting_pts.clear() self.update_aoi() self._pick_thread = threading.Thread(target=worker, daemon=True, args=(self._move_queue, weakref.ref(self))) self._pick_thread.start() def __del__(self): self.finish()
[docs] def finish(self): """Stop any background processing""" self._move_queue.put(None)
def _set_cloud_pt_size(self, point_size): for sensor in self._sensors: for cloud in sensor._clouds: cloud.set_point_size(point_size) # TODO[tws] likely remove @property def metadata(self) -> List[core.SensorInfo]: """Metadatas for the displayed sensors.""" return self._metas
[docs] def set_class_maps(self, class_maps: core.ClassMapSet) -> None: """Set the class maps for the visualizer.""" self._class_maps = class_maps self._class_map_name = sorted(class_maps.keys())[0] if class_maps else ''
def _amend_view_modes_all(self, frames: FrameSet) -> None: """Add new image and cloud view modes to each sensor for each any new fields in the received frames.""" assert len(frames) == len(self._sensors) for frame, sensor in zip(frames, self._sensors): if not frame: continue # TODO[tws] optimize; _known_fields is only used to check for # whether preferred fields are available for default view modes self._known_fields.update(frame.fields) sensor._amend_view_modes(frame) # if no view modes are set yet, set them! self._use_default_view_modes()
[docs] def update_cloud_palette_name(self): """Gets the name of the palette used for the point clouds.""" # the cloud palette name *technically* may not be the same across all sensors # we'll find the palette name of the first sensor if len(self._sensors) > 0: cloud_mode = self._sensors[0]._cloud_modes.get(self._cloud_mode_name, None) palette = self._palettes.get_palette(cloud_mode) self._cloud_palette_name = palette.name
[docs] def update_cloud_palettes(self): """Updates the point clouds to use the currently-selected palette.""" self.update_cloud_palette_name() for sensor in self._sensors: sensor.update_cloud_palettes(self._cloud_mode_name)
[docs] def sorted_cloud_mode_names(self): """Returns all the cloud mode names.""" return sorted( list( set( _flatten([sensor._cloud_modes.keys() for sensor in self._sensors]) ) ), key = lambda key: key.lower() )
[docs] def sorted_image_mode_names(self): """Returns the image mode names, limited to those for fields we've seen in at least one LidarFrame.""" return sorted( list( set( _flatten([sensor._image_modes.keys() for sensor in self._sensors]) ) & self._known_fields # limit to fields seen in LidarFrames ), key = lambda key: key.lower() )
[docs] def select_cloud_mode(self, name: str) -> bool: """Updates the currently selected cloud mode from the list of all available cloud modes. Returns false if the requested mode is not available. """ all_cloud_mode_names = self.sorted_cloud_mode_names() if name not in all_cloud_mode_names: return False self._cloud_mode_ind = all_cloud_mode_names.index(name) self._cloud_mode_name = name self.update_cloud_palettes() return True
[docs] def cycle_cloud_mode(self, direction: int): """Updates the currently selected cloud mode from the list of all available cloud modes.""" all_cloud_mode_names = self.sorted_cloud_mode_names() self._cloud_mode_ind = (self._cloud_mode_ind + direction) % len(all_cloud_mode_names) self._cloud_mode_name = all_cloud_mode_names[self._cloud_mode_ind] self.update_cloud_palettes()
[docs] def select_image_mode(self, i: int, name: str) -> bool: """Updates the currently selected image mode from the list of all available cloud modes. Returns false if the requested mode is not available. """ all_image_mode_names = self.sorted_image_mode_names() if name not in all_image_mode_names: return False self._image_mode_ind[i] = all_image_mode_names.index(name) self._image_mode_names[i] = name return True
[docs] def cycle_image_mode(self, i: int, direction: int): """Updates the currently selected image mode from the list of all available cloud modes.""" all_image_mode_names = self.sorted_image_mode_names() if len(all_image_mode_names) == 0: return self._image_mode_ind[i] = (self._image_mode_ind[i] + direction) % len(all_image_mode_names) self._image_mode_names[i] = all_image_mode_names[self._image_mode_ind[i]]
# TODO[tws] optimize update image palettes def _use_default_view_modes(self): """Try to set the image and cloud view modes to sensible defaults, depending on what fields have been discovered via _amend_view_modes_all. If no sensible default can be found, the method will pick the view modes associated with the first fields. """ if self._cloud_mode_name and self._image_mode_names: # exit early if the view modes are already set return sorted_cloud_mode_names = self.sorted_cloud_mode_names() sorted_image_mode_names = self.sorted_image_mode_names() if not sorted_image_mode_names or not sorted_cloud_mode_names: return # Set the modes for image 1 and cloud if "RGB" in sorted_image_mode_names: # Always show RGB if present in image 1 and cloud self._image_mode_ind[1] = sorted_image_mode_names.index("RGB") self._cloud_mode_ind = sorted_cloud_mode_names.index("RGB") else: # Otherwise prefer REFLECTIVITY2 or NEAR_IR for image 1 # For cloud prefer REFLECTIVITY preferred_field = ChanField.REFLECTIVITY2 if ChanField.REFLECTIVITY2 not in self._known_fields: preferred_field = ChanField.NEAR_IR try: self._image_mode_ind[1] = sorted_image_mode_names.index(preferred_field) self._cloud_mode_ind = sorted_cloud_mode_names.index(ChanField.REFLECTIVITY) except ValueError: self._image_mode_ind[1] = 0 self._cloud_mode_ind = 0 # Finally set the mode for image 0, which should be reflectivity try: self._image_mode_ind[0] = sorted_image_mode_names.index(ChanField.REFLECTIVITY) except ValueError: self._image_mode_ind[0] = 0 self._cloud_mode_name = sorted_cloud_mode_names[self._cloud_mode_ind] for i in range(2): self._image_mode_names[i] = sorted_image_mode_names[self._image_mode_ind[i]] self.update_cloud_palettes()
[docs] def update_objects_for_list(self, key: str, object_list): def cuboid_select_cb(lsv_weakref, viz_weakref, cuboid_weakref, selected_color, obj, lsvm_weakref, _) -> None: # ignored param is a list of ids lsv = lsv_weakref() viz = viz_weakref() lsvm = lsvm_weakref() cuboid = cuboid_weakref() if not lsv or not viz or not cuboid or not lsvm: return if obj.id in lsv._object_labels: return cuboid.set_rgba(selected_color) pos = (obj.body_to_world * obj.object_to_body).position vel_norm = np.linalg.norm(obj.velocity) class_map = lsv._class_maps.get(lsv._class_map_name, None) class_name = class_map.get(obj.class_id, 'UNKNOWN') if class_map else 'UNKNOWN' # type: ignore text = f"{class_name} {obj.id}\nvelocity: {vel_norm:.1f} m/s" label = ToggleLabel(viz, text, pos, initially_visible=True) label.scale = 1.25 lsv._object_labels[obj.id] = label lsvm._objects_selected = True for obj in object_list: color_attr = obj.id if self._object_color_mode == ObjectColorMode.OBJECT_ID else obj.class_id color = self._flags_palette[color_attr % len(self._flags_palette)] color = (*self._flags_palette[color_attr % len(self._flags_palette)], 0.3) cuboid = Cuboid.from_object(obj, color) lsv_weakref = weakref.ref(self) viz_weakref = weakref.ref(self._viz) cuboid_weakref = weakref.ref(cuboid) selected_color = (*color[0:3], 0.9) cb = partial( cuboid_select_cb, lsv_weakref, viz_weakref, cuboid_weakref, selected_color, obj, weakref.ref(self) ) cuboid.set_on_select(cb) if self._object_view_mode in (ObjectViewMode.OVERLAY_AND_MAIN_VIEW, ObjectViewMode.MAIN_VIEW_ONLY): self._viz.add(cuboid) self._objects[obj] = cuboid if obj.id in self._object_labels: label = self._object_labels[obj.id] label.visible = self._object_view_mode in ( ObjectViewMode.OVERLAY_AND_MAIN_VIEW, ObjectViewMode.MAIN_VIEW_ONLY ) label.position = (obj.body_to_world * obj.object_to_body).position vel_norm = np.linalg.norm(obj.velocity) class_map = self._class_maps.get(self._class_map_name, None) class_name = class_map.get(obj.class_id, 'UNKNOWN') if class_map else 'UNKNOWN' # type: ignore text = f"{class_name} {obj.id}\nvelocity: {vel_norm:.1f} m/s" label.text = text label.scale = 1.25 color = (*self._flags_palette[color_attr % len(self._flags_palette)], 0.9) cuboid.set_rgba(color)
[docs] def update_object_cuboids(self) -> None: """Add or remove cuboids from the viz based on the current object view mode.""" if self._object_view_mode in (ObjectViewMode.OVERLAY_AND_MAIN_VIEW, ObjectViewMode.OVERLAY_ONLY): for sensor_idx, sensor in enumerate(self._sensors): frame = self._frame_set[sensor_idx] overlay_cuboids = [] if frame is not None: for obj, _cuboid in self._objects.items(): color_attr = obj.id if self._object_color_mode == ObjectColorMode.OBJECT_ID else obj.class_id color = self._flags_palette[color_attr % len(self._flags_palette)] rgba = (*color, 0.9) if obj.id in self._object_labels else (*color, 0.3) overlay_cuboid = Cuboid.from_object( _object_for_overlay_cuboid(obj, frame), rgba) overlay_cuboids.append(overlay_cuboid) sensor._object_overlay.set_cuboids(overlay_cuboids) else: for sensor in self._sensors: sensor._object_overlay.set_cuboids([])
[docs] def update_objects(self, frames: FrameSet) -> None: """Update the objects in the viz from the given FrameSet.""" self._frame_set = frames # remove all objects for cuboid in self._objects.values(): self._viz.remove(cuboid) self._objects.clear() if isinstance(frames, FrameSet): for key, object_list in frames.objects.items(): self.update_objects_for_list(key, object_list) for frame in frames: if frame is None: continue for key, object_list in frame.objects.items(): self.update_objects_for_list(key, object_list) self.update_object_cuboids()
[docs] def update(self, frames: FrameSet, new_frames: bool = True) -> None: """Update the LidarFrameViz state with the provided frames.""" assert len(frames) == len(self._sensors) self._frame_set = frames self._amend_view_modes_all(frames) # if we have a 3d selection, update it on new frames if new_frames: for sensor in self._sensors: if len(sensor._selected_pts): self.update_3d_aoi(True) break self.update_objects(frames) for frame, sensor in zip(frames, self._sensors): sensor.update_clouds(self._cloud_mode_name, frame) sensor.update_images(self._image_mode_names, frame) if frame: # TODO [tws] use midpoint pose? view_mat = np.linalg.inv(frame.body_to_world[0] @ sensor._meta.sensor_to_body) sensor._object_overlay.set_view_matrix(view_mat) if frame.has_field(ZONE_STATES_FIELDNAME): # a zero timestamp indicates we didnt get a packet if frame.has_field(ChanField.ZONE_PACKET_TIMESTAMP) and \ frame.field(ChanField.ZONE_PACKET_TIMESTAMP)[0] == 0: sensor._zone_states = None else: sensor._zone_states = frame.field(ZONE_STATES_FIELDNAME) sensor.update_zones(frame) # check if we should enable dual return mode if len(self._cloud_enabled) == 1: if frame.has_field('RANGE2'): self._cloud_enabled.append(True)
[docs] def clear_masks(self): for sensor_index, sensor in enumerate(self._sensors): meta = sensor._meta mask = np.zeros((meta.h, meta.w, 4), dtype=np.uint8) for image in sensor._images: image.set_mask(mask) for cloud in sensor._clouds: cloud.set_mask(mask)
[docs] def clear_aoi(self): self._current_selection = [] [aoi_label.set_text("") for aoi_label in self._aoi_labels] self.clear_masks() self._3d_aoi_label.set_text("") with self._aoi_lock: for sensor_index, sensor in enumerate(self._sensors): sensor._selected_pts.clear()
[docs] def clear_object_selection(self): for label in self._object_labels.values(): label.hide() self._object_labels.clear()
[docs] def image_and_pixel_for_viewport_coordinate(self, ctx, x, y): pixel = None for sensor_index, sensor in enumerate(self._sensors): if not sensor._enabled: continue for image_idx, image in enumerate(sensor._images): try: pixel = image.viewport_coordinates_to_image_pixel(ctx, x, y) # TODO[tws] add accessors for image width, height to PointViz if pixel[0] >= 0 and pixel[0] < sensor._meta.h and pixel[1] >= 0 and pixel[1] < sensor._meta.w: return sensor_index, image_idx, image, pixel except RuntimeError: # TWS 20251119: this can happen when the image has zero data or width/height # in such cases we can't compute a valid relative pixel coordinate continue return None, None, None, None
_pick_start = None
[docs] def mouse_button_handler(self, ctx: WindowCtx, button: MouseButton, event: MouseButtonEvent, mods: EventModifierKeys) -> bool: ret = True if button == MouseButton.MOUSE_BUTTON_RIGHT and event == MouseButtonEvent.MOUSE_BUTTON_PRESSED: image = None if self._img_size_fraction > 0: sensor_index, image_idx, image, pixel = self.image_and_pixel_for_viewport_coordinate( ctx, ctx.mouse_x, ctx.mouse_y ) if image: self.clear_aoi() sensor = self._sensors[sensor_index] self._mouse_down_image = image_idx self._current_selection = [ Selection2d(pixel, (pixel[0] + 1, pixel[1] + 1), sensor_index, sensor, image_idx, image) for image_idx, image in enumerate(sensor._images) ] ret = False else: self.clear_aoi() if mods & EventModifierKeys.MOD_SHIFT == 0: self.clear_object_selection() self.update_overlay_colors(self._flags_palette) self._pick_start = (int(ctx.mouse_x), int(ctx.mouse_y)) ret = False self.update_aoi(ctx) if self._current_selection and \ button == MouseButton.MOUSE_BUTTON_RIGHT and \ event == MouseButtonEvent.MOUSE_BUTTON_RELEASED: # clear selections if there was a preexisting selection and the new selection is a # single pixel (mouse click and release), or if there is a selection of area == 0 area = self._current_selection[0].area if area <= 1 and self._preexisting_selection or area == 0: self.clear_aoi() self._preexisting_selection = False else: [selection.finalize() for selection in self._current_selection] self._preexisting_selection = True ret = False self.update_aoi(ctx) if button == MouseButton.MOUSE_BUTTON_RIGHT and \ event == MouseButtonEvent.MOUSE_BUTTON_RELEASED: if self._pick_start is not None: x = int(ctx.mouse_x) y = int(ctx.mouse_y) x2, y2 = self._pick_start # enqueue the final pick request self._move_queue.put((self._queue_idx, x, y, x2, y2, True), block=False) self._queue_idx += 1 self._pick_start = None return ret
_last_selection_origin = None
[docs] def update_3d_aoi(self, force_origin=False): with self._aoi_lock: # fill out the mask for sensor_idx, model in enumerate(self._sensors): for ret_idx, selection in model._selected_pts.items(): mask = np.zeros((model._meta.h, model._meta.w, 4), dtype=np.uint8) mask1d = mask.reshape([-1, 4]) mask1d[selection] = (255, 0, 0, 153) # update masks for relevant returns for idx, img in enumerate(model._images): img_mode = self._image_mode_names[idx] if img_mode in [ ChanField.FLAGS2, ChanField.RANGE2, ChanField.REFLECTIVITY2, ChanField.SIGNAL2 ]: if ret_idx == 1: img.set_mask(core.destagger(model._meta, mask)) elif img_mode in [ ChanField.FLAGS, ChanField.RANGE, ChanField.REFLECTIVITY, ChanField.SIGNAL ]: if ret_idx == 0: img.set_mask(core.destagger(model._meta, mask)) else: # show selections in either return if len(model._selected_pts) > 1: img_mask = np.copy(mask) img_mask1d = img_mask.reshape([-1, 4]) for _, mask_pts in model._selected_pts.items(): img_mask1d[mask_pts] = (255, 0, 0, 153) else: img_mask = mask img.set_mask(core.destagger(model._meta, img_mask)) model._clouds[ret_idx].set_mask(mask) num_pts = 0 data = None position = None # check if our origin is still good so we can keep it stable if self._last_selection_origin: last_sensor, last_frame, last_pt = self._last_selection_origin selection = self._sensors[last_sensor]._selected_pts.get(last_frame) if (selection is None or last_pt not in selection) or force_origin: self._last_selection_origin = None # accumulate data points in the selection for statistics # also find a 3D point to place the label point = None for sensor_idx, model in enumerate(self._sensors): for idx, selection in model._selected_pts.items(): frame = self._frame_set[sensor_idx] if frame is None: continue if len(selection) == 0: continue num_pts += len(selection) first_index = int(selection[0]) frame_w = int(frame.w) col = int(first_index % frame_w) row = int(first_index // frame_w) point = (sensor_idx, row, col) # if we need a new origin, pick one if self._last_selection_origin is None: if idx == 0: rng = frame.field("RANGE").reshape((-1,))[first_index] else: rng = frame.field("RANGE2").reshape((-1,))[first_index] position = copy.copy(model._xyzlut.offset[first_index]) position += model._xyzlut.direction[first_index] * rng position = frame.body_to_world[col] @ (position[0], position[1], position[2], 1.0) self._3d_aoi_label.set_position(position[0], position[1], position[2]) self._last_selection_origin = (sensor_idx, idx, first_index) # accumulate data points for statistics if self._cloud_mode_name == "RING": frame_data = selection // frame.w elif self._cloud_mode_name == "TIMESTAMP": frame_data = np.tile(frame.timestamp, (frame.h, 1)).reshape((-1,))[selection] elif self._cloud_mode_name == "SENSOR": frame_data = np.tile(sensor_idx, (frame.h * frame.w))[selection] elif not frame.has_field(self._cloud_mode_name): continue else: field = frame.field(self._cloud_mode_name) if field.ndim > 2: frame_data = field.reshape((-1, field.shape[-1]))[selection, :] else: frame_data = field.reshape((-1,))[selection] if data is None: data = frame_data else: data = np.concatenate((data, frame_data), axis = 0) if num_pts > 0: self._viz.add(self._3d_aoi_label) label_text = f"{self._cloud_mode_name}\n" if data is None: label_text += ( "min/max: ? ?\n" "mean/std: ? ?\n" ) else: if data.ndim > 1: def format(values: np.ndarray) -> str: return "[" + ", ".join(f"{v:6.3f}" for v in values) + "]" else: def format(values: np.ndarray) -> str: return f"{values:8.1f}" # Use float32 accumulators for fp16 RGB stats; summing/squaring AOI # pixels in float16 can overflow even when the source values are valid. stats_dtype = (np.float32 if np.issubdtype(data.dtype, np.floating) and data.dtype.itemsize < np.dtype(np.float32).itemsize else None) min = np.min(data, axis=0) max = np.max(data, axis=0) mean = np.mean(data, axis=0, dtype=stats_dtype) std = np.std(data, axis=0, dtype=stats_dtype) label_text += ( f"min/max: {format(min)} {format(max)}\n" f"mean/std:{format(mean)} {format(std)}\n" ) label_text += f"{num_pts} pts" if num_pts == 1: label_text += f"\nsensor: {point[0]}\n" col = point[2] row = point[1] sensor_info = self._sensors[point[0]]._meta shift = int(sensor_info.format.pixel_shift_by_row[row]) w = int(sensor_info.w) destaggered_col = col + shift if destaggered_col >= w: destaggered_col = destaggered_col - w elif destaggered_col < 0: destaggered_col = destaggered_col + w label_text += f"[{col} {row}] (staggered)\n" label_text += f"[{destaggered_col} {row}] (destaggered)" self._3d_aoi_label.set_text(label_text) else: self._3d_aoi_label.set_position(-10, -10, False, False) self._last_selection_origin = None self._viz.update()
[docs] def update_aoi(self, ctx: Optional[WindowCtx] = None): with self._aoi_lock: found = False for sensor_idx, model in enumerate(self._sensors): for idx, selected in model._selected_pts.items(): if len(selected) > 0: found = True if found: # update 3D AOI self.update_3d_aoi() return # try and update masks from sensors for sensor in self._sensors: sensor._clear_aois() self._3d_aoi_label.set_position(-10, -10, False, True) if not self._current_selection: return if ctx: self._ctx = ctx # clear the masks - important because the image mode may have changed self.clear_masks() for selection in self._current_selection: image_idx = selection._image_index sensor = selection._sensor image = sensor._images[image_idx] meta = sensor._meta p1 = selection.p1 p2 = selection.p2 # compute the image mask given the selection area mask = np.zeros((meta.h, meta.w, 4), dtype=np.uint8) min_x = min(p1[0], p2[0]) max_x = max(p1[0], p2[0]) min_y = min(p1[1], p2[1]) max_y = max(p1[1], p2[1]) mask[min_x:max_x, min_y:max_y, :] = (255, 0, 0, 153) image.set_mask(mask) # compute the cloud mask cloud_mask = np.zeros((meta.h, meta.w, 4), dtype=np.uint8) cloud_mask[min_x:max_x, min_y:max_y, :] = (255, 0, 0, 204) cloud_mask = core.destagger(meta, cloud_mask, inverse=True) # mask the first return cloud unless the AOI is on a 2nd return field key = self._image_mode_names[selection._image_index] cloud_index = 1 if key in [ ChanField.FLAGS2, ChanField.RANGE2, ChanField.REFLECTIVITY2, ChanField.SIGNAL2 ] else 0 sensor._clouds[cloud_index].set_mask(cloud_mask) # set the location of the text assert self._ctx mask_upper_right_viewport_coordinates = image.image_pixel_to_viewport_coordinates( self._ctx, (max_x, max_y) ) aoi_label_x = (mask_upper_right_viewport_coordinates[0] + 12) / self._ctx.viewport_width aoi_label_y = mask_upper_right_viewport_coordinates[1] / self._ctx.viewport_height if self._img_size_fraction == 0: # move offscreen (yes, it'd be better to hide it but we don't have an API method for that) self._aoi_labels[image_idx].set_position(-10, -10, False, True) else: self._aoi_labels[image_idx].set_position(aoi_label_x, aoi_label_y, False, True)
[docs] def mouse_pos_handler(self, ctx: WindowCtx, x: float, y: float) -> bool: if self._mouse_down_image is not None and self._current_selection: selection = self._current_selection[self._mouse_down_image] if selection.finalized: return True # TODO[tws] add accessors for image width, height to PointViz image_width = selection._sensor._meta.w image_height = selection._sensor._meta.h pixel = selection._image.viewport_coordinates_to_image_pixel(ctx, x, y) # clamp pixel to a valid location in the image pixel = ( max(0, min(pixel[0], image_height)), max(0, min(pixel[1], image_width)) ) # update top and bottom image selections regardless of which one we're drawing the AOI for selection in self._current_selection: # make sure p1 and p2 are not the same point on each axis first_same = selection.p1[0] == pixel[0] second_same = selection.p1[1] == pixel[1] if first_same: pixel = (selection.p1[0] + 1, pixel[1]) if second_same: pixel = (pixel[0], selection.p1[1] + 1) selection.p2 = pixel # providing the window context here is a necessary evil to compute window coordinates # of the image self.update_aoi(ctx) return False if self._pick_start is not None: # update the mask x2 = int(ctx.mouse_x) y2 = int(ctx.mouse_y) x, y = self._pick_start # enqueue another pick request self._move_queue.put((self._queue_idx, x, y, x2, y2, False), block=False) self._queue_idx += 1 return True return True
[docs] def update_aoi_label(self, frames: FrameSet): self._frame_set = frames if not self._current_selection: [label.set_text("") for label in self._aoi_labels] # type: ignore return for selection_idx, selection in enumerate(self._current_selection): sensor_idx = selection._sensor_index frame = frames[sensor_idx] if not frame: return # get filters for valid returns (range) that are within the AOI meta = selection._sensor._meta valid_aoi = core.destagger( meta, (selection._aoi_mask > 0).astype(dtype=np.uint8), inverse=True ) valid = valid_aoi > 0 # image_index = self._current_selection._image_index # FIXME support both indices? key = self._image_mode_names[selection._image_index] # consider only valid values to avoid corrupting the statistical calculations # with invalid 0 values if key in [ChanField.RANGE, ChanField.RANGE2, ChanField.REFLECTIVITY, ChanField.REFLECTIVITY2, ChanField.SIGNAL, ChanField.SIGNAL2, ChanField.NEAR_IR, ChanField.WINDOW]: valid_field = frame.field(key) > 0 valid &= valid_field if not frame.has_field(key): continue field_data = frame.field(key) data = field_data[valid] label_str = f"{str(key).replace('_', '-')}\n" p1 = selection.p1 p2 = selection.p2 # subtract one from the max values # so that we show the inclusive range rather than the slice into the numpy array min_x = min(p1[0], p2[0]) max_x = max(p1[0], p2[0]) - 1 min_y = min(p1[1], p2[1]) max_y = max(p1[1], p2[1]) - 1 field_shape = field_data.shape channel_dimension = field_shape[2] if len(field_shape) == 3 else 1 data = data.reshape(-1, channel_dimension) if data.size == 0: data = np.zeros((1, channel_dimension), dtype=np.float32) # Use float32 accumulators for fp16 RGB stats; summing/squaring AOI # pixels in float16 can overflow even when the source values are valid. stats_dtype = (np.float32 if np.issubdtype(data.dtype, np.floating) and data.dtype.itemsize < np.dtype(np.float32).itemsize else None) comp_min = np.min(data, axis=0) comp_max = np.max(data, axis=0) comp_mean = np.mean(data, axis=0, dtype=stats_dtype) comp_std = np.std(data, axis=0, dtype=stats_dtype) is_vector = channel_dimension == 3 if is_vector: def format_values(values: np.ndarray) -> str: return "[" + ", ".join(f"{v:6.3f}" for v in values) + "]" stats_lines = [ ("min/max:", format_values(comp_min), format_values(comp_max)), ("mean:", format_values(comp_mean)), ("std:", format_values(comp_std)), ] else: def format_values(values: np.ndarray) -> str: return f"{values[0]:8.1f}" stats_lines = [ ("min/max:", format_values(comp_min), format_values(comp_max)), ("mean/std:", format_values(comp_mean), format_values(comp_std)), ] for prefix, *values in stats_lines: value_str = " ".join(values).rstrip() label_str += f"{prefix:<9}{value_str}\n" label_str += f"[{min_y}:{max_y} {min_x}:{max_x}]\n" self._aoi_labels[selection._image_index].set_text(label_str)
[docs] def flip_images(self, flip: bool) -> None: self._flip_images = flip self.update_image_size(0)
[docs] def toggle_flip_images(self) -> None: self.flip_images(not self._flip_images)
[docs] def show_one_image(self, do: bool) -> None: self._show_one_image = do self.update_image_size(0)
[docs] def update_image_size(self, amount: int) -> None: """Change the size of the 2D image and position image labels.""" size_fraction_max = 20 self._img_size_fraction = (self._img_size_fraction + amount + (size_fraction_max + 1)) % ( size_fraction_max + 1) enabled_sensors = [sensor for sensor in self._sensors if sensor._enabled] image_h = self._img_size_fraction / size_fraction_max # compute the total width total_image_w = 0.0 for sensor in enabled_sensors: image_w = image_h / sensor._img_aspect_ratio total_image_w += image_w # set image positions center_x = -total_image_w / 2 last_image_right = 0.0 for sensor in enabled_sensors: image_w = image_h / sensor._img_aspect_ratio image_left = last_image_right image_right = last_image_right + image_w last_image_right = image_right if self._flip_images: image_right, image_left = image_left, image_right for image_idx, image in enumerate(sensor._images): image_top = 1.0 - image_h * image_idx image_bottom = 1.0 - image_h * (image_idx + 1) if self._flip_images: image_top, image_bottom = image_bottom, image_top if self._show_one_image and image_idx > 0: image.set_position(1000, 0, 0, 0) else: image.set_position(image_left + center_x, image_right + center_x, image_bottom, image_top) if image_idx == 0: sensor._object_overlay.set_position( image_left + center_x, image_right + center_x, image_bottom, image_top ) self.update_aoi()
[docs] def update_overlay_colors(self, palette): # TODO[tws] deduplicate logic with that found in update_objects self._flags_palette = palette for obj, cuboid in self._objects.items(): color_attr = obj.id if self._object_color_mode == ObjectColorMode.OBJECT_ID else obj.class_id color = self._flags_palette[color_attr % len(palette)] selected_color = (*color[0:3], 0.9) if obj.id in self._object_labels: cuboid.set_rgba(selected_color) else: cuboid.set_rgba((*color, 0.3)) # necessary to update the cuboids in the overlay, # which at present do not share a reference with the cuboids in the main viz self.update_object_cuboids()
# ``LidarScanVizModel`` was renamed to ``LidarFrameVizModel`` in the scan -> frame # migration. Expose the old name (with a deprecation warning) so existing call # sites keep working. deprecated_alias("LidarScanVizModel", "LidarFrameVizModel", LidarFrameVizModel, globals(), "1.0")