"""
Copyright (c) 2023, Ouster, Inc.
All rights reserved.
Ouster frame accumulation for LidarFrameViz
"""
from typing import (Optional, Dict, Tuple, Callable, Any)
import threading
from functools import partial
from ouster.sdk._bindings.viz import PointViz, WindowCtx, Label
from ouster.sdk.viz.model import LidarFrameVizModel
from ouster.sdk.viz.frames_accumulator import FramesAccumulator
from ouster.sdk.viz.map_accumulator import MapAccumulator
from ouster.sdk.viz.accumulators_config import LidarFrameVizAccumulatorsConfig
from ouster.sdk.viz.track import MultiTrack
from ouster.sdk.viz.tracks_accumulator import TracksAccumulator
from ouster.sdk.core import FrameSet
from ouster.sdk._deprecation import deprecated_alias
[docs]
class LidarFrameVizAccumulators:
"""Accumulate frames, track poses and overall map view
Every new frame (``LidarFrame`` or ``FrameSet``) is passed
through ``update(frame, num)``.
Available visualization depends on whether poses are present or not
and params set on init. View modes are combination of:
* **TRACK** - frame poses (i.e. trajectories) of every frame "seen" (poses
required)
* **ACCUM** - set of accumulated frames (key frames) picked according to
params
* **MAP** - overall map with select ratio of random points from every
frame passed through ``update()``
"""
def __init__(self,
model: LidarFrameVizModel,
point_viz: PointViz,
config: LidarFrameVizAccumulatorsConfig,
lock: threading.RLock):
"""
Args:
model: a LidarFrameVizModel instance.
point_viz: the PointViz instance to use for rendering clouds.
config: a LidarFrameVizAccumulatorsConfig that accepts the following keyword args:
accum_max_num: aka, ``--accum-num``, the maximum number of accumulated
(ACCUM) frames to keep
accum_min_dist_meters: aka, ``--accum-every-m``, the minimum distance
between accumulated (ACCUM) key frames
accum_min_dist_num: aka, ``--accum-every``, the minimum distance in
frames between accumulated (ACCUM) key frames
map_enabled: enable overall map accumulation (MAP) (``--map``)
map_select_ratio: percent of points to select from the frames to the
overall map (MAP), default 0.001
map_max_points: maximum number of points to keep in overall map (MAP)
map_overflow_from_start: if True, on map overflow continue writing
points from the beginning (as in ring buffer), if False, overwrite
points randomly in the existing map
"""
self._lock = lock
self._viz = point_viz
track = MultiTrack(model, config)
self._track = track
self._config = config
self._ma = MapAccumulator(model, point_viz, track._tracks[0], config)
self._sa = FramesAccumulator(model, point_viz, track)
self._ta = TracksAccumulator(model, point_viz, track._tracks[0])
if self._ma._map_enabled:
self._ma.toggle_visibility(True)
elif config._accum_max_num > 0:
self._sa.toggle_visibility(True)
self._ta.toggle_visibility(True)
# initialize osd (on screen display text)
self._osd: Optional[Label] = None
self._osd_enabled = False
# callback for any external vizs that need to hookup into the draw update
# (currently used by LidarFrameViz to update the OSD text)
self._key_press_pre_draw: Callable[[], Any] = lambda: None
self._osd_enabled = True
self._osd = Label("", 0, 1, align_right=False)
self._viz.add(self._osd)
self._initialize_key_bindings()
self._cloud_pt_size: float = 1
@property
def track_accumulator(self) -> TracksAccumulator:
"""Get the TracksAccumulator instance."""
return self._ta
[docs]
def cycle_cloud_mode(self, direction) -> bool:
with self._lock:
self._ma.cycle_cloud_mode(direction=direction)
self._sa.cycle_cloud_mode(direction=direction)
return True
[docs]
def cycle_cloud_palette(self, direction) -> bool:
with self._lock:
self._ma.cycle_cloud_palette(direction=direction)
self._sa.cycle_cloud_palette(direction=direction)
return True
def _initialize_key_bindings(self) -> None:
"""Initialize key bindings and key definitions."""
# TODO[tws] typing
key_bindings: Dict[Tuple[int, int], Callable[[], bool]] = {
(ord('J'), 0): partial(self.update_point_size, amount=1),
(ord('J'), 1): partial(self.update_point_size, amount=-1),
(ord('K'), 0): partial(self.cycle_cloud_mode, direction=1),
(ord('K'), 1): partial(self.cycle_cloud_mode, direction=-1),
(ord('G'), 0): partial(self.cycle_cloud_palette, direction=1),
(ord('G'), 1): partial(self.cycle_cloud_palette, direction=-1),
(ord('6'), 0): partial(self.toggle_mode_accum),
(ord('7'), 0): partial(self.toggle_mode_map),
}
key_definitions: Dict[str, str] = {
'j / SHIFT+j': "Increase/decrease point size of accumulated clouds or map",
'k / SHIFT+k': "Cycle point cloud coloring mode of accumulated clouds or map",
'g / SHIFT+g': "Cycle point cloud color palette of accumulated clouds or map",
'6': "Toggle frames accumulation view mode (ACCUM)",
'7': "Toggle overall map view mode (MAP)",
}
self._key_definitions = key_definitions
def handle_keys(ctx: WindowCtx, key: int,
mods: int) -> bool:
if (key, mods) in key_bindings:
draw = key_bindings[key, mods]()
if draw:
# notify neighbor vizs that need to update on key press re-draw
if self._key_press_pre_draw is not None:
self._key_press_pre_draw()
# draw + _viz.update() inside
self.draw()
else:
self._viz.update()
return True
self._viz.push_key_handler(handle_keys)
[docs]
def update_point_size(self, amount: int) -> bool:
"""Change the point size of the MAP/ACCUM point cloud."""
# TODO[tws] generalize
with self._lock:
self._cloud_pt_size = min(10.0, max(1.0, self._cloud_pt_size + amount))
self._ma.update_point_size(self._cloud_pt_size)
self._sa.update_point_size(self._cloud_pt_size)
return True
[docs]
def toggle_sensor(self, sensor_idx, state: bool):
self._sa.toggle_sensor(sensor_idx, state)
[docs]
def toggle_mode_accum(self, state: Optional[bool] = None) -> bool:
"""Toggle ACCUM view"""
with self._lock:
self._sa.toggle_visibility(state)
return True
[docs]
def toggle_mode_map(self, state: Optional[bool] = None) -> bool:
"""Toggle MAP view"""
with self._lock:
self._ma.toggle_visibility(state)
return True
[docs]
def toggle_mode_track(self, state: Optional[bool] = None) -> bool:
with self._lock:
self._ta.toggle_visibility(state)
return True
[docs]
def toggle_osd(self, state: Optional[bool] = None) -> bool:
"""Show or hide the on-screen display."""
with self._lock:
self._osd_enabled = (not self._osd_enabled
if state is None else state)
return True
[docs]
def osd_text(self) -> str:
"""Prepare OSD text for use in draw_osd or elsewhere."""
osd_text = ""
def append_with_nl(s1: str, s2: str):
if s1 and s2:
return f"{s1}\n{s2}"
return s1 or s2
# Lines like:
# frame, map accum [6, 7]: ON, OFF
# mode [K]: REFLECTIVITY
# palette [G]: Cal Ref
accum_str = ""
accum_states = []
if self._config._accum_max_num > 0:
accum_states.append(
("frame", "6",
"ON" if self._sa.accum_visible else "OFF"))
if self._ma._map_enabled:
accum_states.append(("map", "7", "ON" if self._ma.map_visible else "OFF"))
if accum_states:
active_cloud_mode = self._ma.active_cloud_mode
active_cloud_palette = self._ma._get_palette_from_active_mode_name(active_cloud_mode)
accum_names_str = ", ".join([s[0] for s in accum_states])
accum_keys_str = ", ".join([s[1] for s in accum_states])
accum_status_str = ", ".join([s[2] for s in accum_states])
accum_str = f"{accum_names_str} accum [{accum_keys_str}]: {accum_status_str}\n"
accum_str += f" mode [K]: {active_cloud_mode}\n" # TODO[tws] generalize
accum_str += f" palette [G]: {active_cloud_palette.name}\n" # TODO[tws] generalize
accum_str += f" point size [J]: {int(self._cloud_pt_size)}"
return append_with_nl(osd_text, accum_str)
def _draw_osd(self):
"""Update on screen display label text"""
if self._osd_enabled:
self._osd.set_text(self.osd_text())
else:
self._osd.set_text("")
[docs]
def clear_track(self) -> None:
self._track.clear()
[docs]
def update(self,
frames: FrameSet,
frame_num: Optional[int] = None) -> None:
"""
Updates the accumulation state from the current frame. Locking is necessary here because the accumulation state
depends on the current view mode, which might change in a separate thread than the thread that calls update().
"""
with self._lock:
self._ma._use_default_view_modes()
self._sa._use_default_view_modes()
self._track.update(frames, frame_num)
if self._ma._map_enabled:
self._ma.update(frames, frame_num)
self._sa.update(frames, frame_num)
self._ta.update(frames, frame_num)
def _draw(self) -> None:
self._ta._draw_track()
if self._ma.map_visible:
self._ma._draw_map()
self._draw_osd()
# TODO[tws] likely remove; realistically we only need one lock and LidarFrameViz should manage it
[docs]
def draw(self, update: bool = True) -> None:
"""Process and draw the latest state to the screen."""
with self._lock:
self._draw()
if update:
self._viz.update()
# ``LidarScanVizAccumulators`` was renamed to ``LidarFrameVizAccumulators`` in
# the scan -> frame migration. Expose the old name (with a deprecation warning)
# so existing call sites keep working.
deprecated_alias("LidarScanVizAccumulators", "LidarFrameVizAccumulators",
LidarFrameVizAccumulators, globals(), "1.0")