Source code for ouster.sdk.viz.accum_base
from typing import List, Optional
from ouster.sdk.viz import Cloud, PointViz
from ouster.sdk.viz.model import LidarFrameVizModel
from ouster.sdk.viz.track import Track
import ouster.sdk.core as core
from ouster.sdk.core import ChanField, FrameSet
from ouster.sdk.viz.view_mode import (CloudMode, CloudPaletteItem, is_norm_reflectivity_mode)
[docs]
class AccumulatorBase:
"""The base of any class used in LidarFrameVizAccumulators that displays data accumulated from frames."""
def __init__(self, model: LidarFrameVizModel, point_viz: PointViz, track: Track):
self._frame_num = 1
self._viz = point_viz
self._model = model
self._track = track
self._metas = model.metadata
# init view cloud mode toggle
self._cloud_mode_ind = 0
self._cloud_mode_name: str = ''
# init cloud palette toggle
self._cloud_palette_ind = 0
self._cloud_palette_prev: Optional[CloudPaletteItem] = \
self._model._palettes._refl_cloud_palettes[self._cloud_palette_ind]
self._cloud_pt_size: float = 1.0
# frame poses track
self._cloud_track: Optional[Cloud] = None
@property
def metadata(self) -> List[core.SensorInfo]:
"""Metadatas for the displayed sensors."""
return self._metas
[docs]
def get_palette(self, cloud_mode: CloudMode) -> CloudPaletteItem:
# TODO[tws] deduplicate the palette selection code with that in Palettes
refl_mode = is_norm_reflectivity_mode(cloud_mode)
if refl_mode:
return self._model._palettes._refl_cloud_palettes[self._cloud_palette_ind]
else:
return self._model._palettes._cloud_palettes[self._cloud_palette_ind]
@property
def active_cloud_mode(self) -> str:
"""Name of current color mode of point ACCUM/MAP point clouds"""
return self._cloud_mode_name
def _update_cloud_mode(self):
pass
def _update_cloud_palette(self):
pass
[docs]
def cycle_cloud_mode(self, *, direction: int = 1):
"""Change the coloring mode of the point cloud for MAP/ACCUM clouds"""
all_cloud_mode_names = self._model.sorted_cloud_mode_names()
self._cloud_mode_ind = (self._cloud_mode_ind + direction) % len(all_cloud_mode_names)
self._cloud_mode_name = all_cloud_mode_names[self._cloud_mode_ind]
self._update_cloud_mode()
[docs]
def cycle_cloud_palette(self, *, direction: int = 1):
"""Change the color palette of the point cloud for MAP/ACCUM clouds"""
npalettes = len(self._model._palettes._cloud_palettes)
self._cloud_palette_ind = (self._cloud_palette_ind + direction +
npalettes) % npalettes
# update internal states immediately so the OSD text of frames accum
# is switched already to a good state (needed for LidarFrameViz osd
# update)
self._update_cloud_palette()
# TODO: likely refactor to de-duplicate logic (but not state) with LidarFrameVizModel
def _use_default_view_modes(self):
"""Try to set the image and cloud view modes to sensible defaults, depending on what
fields have been discovered via _amend_view_modes_all.
If no sensible default can be found, the method will
pick the view modes associated with the first fields.
"""
if self._cloud_mode_name:
# exit early if the view modes are already set
return
sorted_cloud_mode_names = self._model.sorted_cloud_mode_names()
if sorted_cloud_mode_names == ["RING", "SENSOR", "TIMESTAMP"]:
return
try:
if "RGB" in sorted_cloud_mode_names:
preferred_field = "RGB"
else:
preferred_field = ChanField.REFLECTIVITY
self._cloud_mode_ind = sorted_cloud_mode_names.index(preferred_field)
except ValueError:
# handle a situation where no desired channels are present
self._cloud_mode_ind = 0
self._cloud_mode_name = sorted_cloud_mode_names[self._cloud_mode_ind]
self._update_cloud_palette()
[docs]
def update(self,
frame: FrameSet,
frame_num: Optional[int] = None) -> None:
"""Register the new frame and update the states of TRACK, ACCUM and MAP"""
self._frame = frame
if frame_num is not None:
self._frame_num = frame_num
else:
self._frame_num += 1
[docs]
def toggle_visibility(self, state: Optional[bool] = None):
pass