Source code for ouster.sdk.util.progress_bar

from typing import Optional
import time


[docs] def progressbar(progress, total, prefix="", suffix=""): """ Displays progress in the console as a percentage. Args: progress: The current progress (number of items completed). total: The total number of items. prefix: A prefix string to display before the progress bar (optional). suffix: A suffix string to display after the progress bar (optional). """ if total == 0: raise ValueError( "Progress cannot be displayed for a total of 0 items.") progress = total if progress > total else progress percent = round(100 * progress / total, 1) filled_length = int(round(percent * 20 / 100)) bar = f'[{filled_length * "#"}{(20 - filled_length) * "-"}]' print(f'{prefix} {bar} {percent}% {suffix}', end="\r")
[docs] class ProgressBar: _last_time: Optional[float] = None _total: int def __init__(self, total, alpha = 0.05, unit=""): self._total = total self._iteration_time = 0 self._alpha = alpha self._last_progress = 0 if len(unit): self._unit = f" {unit}/sec" else: self._unit = "/sec"
[docs] def clear(self): # only do this if we printed if self._last_time is None: return # \r = Go to the start of the line # \033[2K = Clear the entire line print("\r\033[2K", end="")
[docs] def update(self, progress, prefix="", suffix=""): now = time.monotonic() if self._last_time is not None: delta = max(1, progress - self._last_progress) self._last_progress = progress dt = (now - self._last_time) / delta if self._iteration_time == 0: self._iteration_time = dt else: self._iteration_time = self._iteration_time * (1.0 - self._alpha) + dt * self._alpha # make sure we dont divide by zero or have negative if self._iteration_time <= 0: self._iteration_time = 0.00001 frame_rate = 1.0 / self._iteration_time rate = f"{frame_rate:>5.0f}" remaining = max(0, self._total - progress) if self._total == 0: eta = "" else: eta = f"{remaining / frame_rate:>4.0f} sec remaining" else: rate = "?" eta = "" self._last_time = now if self._total == 0: total = 100 progress = progress % (total) filled_length = progress // 5 bar = f'[{filled_length * "-"}#{(19 - filled_length) * "-"}]' print(f'{prefix} {bar} {suffix} {rate}{self._unit} {eta}', end="\r") else: total = self._total progress = total if progress > total else progress percent = round(100 * progress / total, 1) filled_length = int(round(percent * 20 / 100)) bar = f'[{filled_length * "#"}{(20 - filled_length) * "-"}]' print(f'{prefix} {bar} {percent:>5}% {suffix} {rate}{self._unit} {eta}', end="\r")
def __enter__(self): """Called when entering the 'with' block.""" return self def __exit__(self, exc_type, exc_value, traceback): """ Called when exiting the 'with' block. """ self.clear() return None