"""Miscellaneous utilities."""
from typing import cast
from ouster.sdk import core
import numpy as np
[docs]
def fov_vertical(info: core.SensorInfo) -> float:
altitude_zeros = np.count_nonzero(info.beam_altitude_angles == 0.0)
if altitude_zeros > 1:
altitudes = info.beam_altitude_angles[np.nonzero(
info.beam_altitude_angles)] # type: ignore
else:
altitudes = info.beam_altitude_angles
fov_vertical = np.max(altitudes) - np.min(altitudes)
if fov_vertical < 1e-9 and len(altitudes) > 1:
print("WARNING: Sensor has vertical field of view of 0. Check beam_altitude_angles values.")
fov_vertical = 1.0
return fov_vertical
[docs]
def fov_horizontal(info: core.SensorInfo) -> float:
if len(info.beam_azimuth_angles) == info.format.pixels_per_column:
fov_horizontal = 360.0
else:
azimuth_zeros = np.count_nonzero(info.beam_azimuth_angles == 0.0)
if azimuth_zeros > 1:
azimuths = info.beam_azimuth_angles[np.nonzero(
info.beam_azimuth_angles)] # type: ignore
else:
azimuths = info.beam_azimuth_angles
fov_horizontal = np.max(azimuths) - np.min(azimuths)
if fov_horizontal < 1e-9:
print("WARNING: Sensor has horizontal field of view of 0. Check beam_azimuth_angles values.")
fov_horizontal = 1.0
return fov_horizontal
[docs]
def img_aspect_ratio(info: core.SensorInfo) -> float:
"""Returns 2D image aspect ratio based on sensor FOV angles.
Uses the order:
img_aspect_ratio = FOV_vertical / FOV_horizontal
"""
return fov_vertical(info) / fov_horizontal(info)
[docs]
def quaternion_to_rotation_matrix(q: np.ndarray) -> np.ndarray:
"""Converts Quaternion [w, x, y, z] to Rotation [3x3] matrix."""
(q0, q1, q2, q3) = q / np.linalg.norm(q)
# yapf: disable
# autopep8: off
return np.array([
[2 * (q0 * q0 + q1 * q1) - 1, 2 * (q1 * q2 - q0 * q3), 2 * (q1 * q3 + q0 * q2)],
[2 * (q1 * q2 + q0 * q3), 2 * (q0 * q0 + q2 * q2) - 1, 2 * (q2 * q3 - q0 * q1)],
[2 * (q1 * q3 - q0 * q2), 2 * (q2 * q3 + q0 * q1), 2 * (q0 * q0 + q3 * q3) - 1]
])
# autopep8: on
# yapf: enable
[docs]
def rotation_matrix_to_quaternion(R: np.ndarray) -> np.ndarray:
"""Converts a Rotation [3x3] matrix to Quaternion [w, x, y, z]."""
# yapf: disable
# autopep8: off
tr = np.trace(R)
if tr > 0:
S = 0.5 / np.sqrt(tr + 1.0)
w = 0.25 / S
x = (R[2, 1] - R[1, 2]) * S
y = (R[0, 2] - R[2, 0]) * S
z = (R[1, 0] - R[0, 1]) * S
elif (R[0, 0] > R[1, 1]) and (R[0, 0] > R[2, 2]):
S = 2.0 * np.sqrt(1.0 + R[0, 0] - R[1, 1] - R[2, 2])
w = (R[2, 1] - R[1, 2]) / S
x = 0.25 * S
y = (R[0, 1] + R[1, 0]) / S
z = (R[0, 2] + R[2, 0]) / S
elif R[1, 1] > R[2, 2]:
S = 2.0 * np.sqrt(1.0 + R[1, 1] - R[0, 0] - R[2, 2])
w = (R[0, 2] - R[2, 0]) / S
x = (R[0, 1] + R[1, 0]) / S
y = 0.25 * S
z = (R[1, 2] + R[2, 1]) / S
else:
S = 2.0 * np.sqrt(1.0 + R[2, 2] - R[0, 0] - R[1, 1])
w = (R[1, 0] - R[0, 1]) / S
x = (R[0, 2] + R[2, 0]) / S
y = (R[1, 2] + R[2, 1]) / S
z = 0.25 * S
return np.array([w, x, y, z])
# autopep8: on
# yapf: enable
[docs]
def euler_to_rotation_matrix(roll, pitch, yaw):
"""
Convert Euler angles (roll, pitch, yaw) to a 3D rotation matrix.
Parameters:
roll : Rotation about the x-axis (rad)
pitch : Rotation about the y-axis (rad)
yaw : Rotation about the z-axis (rad)
Returns:
R : 3x3 rotation matrix
"""
R_x = np.array([
[1, 0, 0],
[0, np.cos(roll), -np.sin(roll)],
[0, np.sin(roll), np.cos(roll)]
])
R_y = np.array([
[np.cos(pitch), 0, np.sin(pitch)],
[0, 1, 0],
[-np.sin(pitch), 0, np.cos(pitch)]
])
R_z = np.array([
[np.cos(yaw), -np.sin(yaw), 0],
[np.sin(yaw), np.cos(yaw), 0],
[0, 0, 1]
])
return R_z @ (R_y @ R_x)
[docs]
def xyzrpy_to_matrix(px, py, pz, r, p, y):
"""
A method that takes position + euler angles (rad) and produces an equivalent 4x4 transform.
Parameters:
px, py, pz: position
r, p, y: rotation expressed in euler angles (rad)
Returns:
R : 4x4 transformation matrix
"""
out = np.eye(4)
out[:3, 3] = np.array([px, py, pz])
out[:3, :3] = euler_to_rotation_matrix(r, p, y)
return out
[docs]
def xyzq_to_matrix(px, py, pz, qx, qy, qz, qw):
"""
A method that takes position + quaternion (rad) and produces an equivalent 4x4 transform.
Parameters:
px, py, pz: position
qx, qy, qz, qw: rotation expressed in a quaternion
Returns:
R : 4x4 transformation matrix
"""
out = np.eye(4)
out[:3, 3] = np.array([px, py, pz])
out[:3, :3] = quaternion_to_rotation_matrix(np.array([qw, qx, qy, qz]))
return out
[docs]
def parse_extrinsics_from_string(extrinsics: str, degrees=True) -> np.ndarray:
"""
A utility method to parse extrinsics in multiple formats.
Parameters:
extrinsics: a string representing a file or extrinsics in a supported format
degrees: whether angles should be parsed as degress (True by default)
Acceptale extrinsics formats:
- A json with containing a per sensor extrinsics
- identity ; Use this to override any stored extrinsics with identity
- X Y Z R P Y ; 'R P Y' represent euler angles (deg)
- X Y Z QX QY QZ QW ; (QX, QY QZ, QW) represent a quaternion
- n1 n2 .. n16 ; 16 floats representing a 2D array in a row-major order
Returns:
R : 4x4 transformation matrix or a filename
"""
sep = ',' if ',' in extrinsics else ' '
elements = extrinsics.split(sep)
if len(elements) == 1:
# treat as a filename if not 'identity' keyword
return np.eye(4) if elements[0] == "identity" else cast(np.ndarray, elements[0])
try:
float_elements = [float(e) for e in elements]
except Exception:
raise ValueError(f"extrinsics values: {elements} could not parsed as numbers")
if len(float_elements) == 6:
xyz = float_elements[:3]
rpy = [np.deg2rad(e) for e in float_elements[3:7]] if degrees else float_elements[3:7]
return xyzrpy_to_matrix(*xyz, *rpy)
if len(float_elements) == 7:
return xyzq_to_matrix(*float_elements)
if len(float_elements) == 16:
return np.array([*float_elements]).reshape((4, 4))
raise ValueError("Unsupported extrinsics format, check `ouster-cli source --help`"
" for proper usage")