Source code for ouster.sdk.examples.reference

"""
Copyright (c) 2021, Ouster, Inc.
All rights reserved.

Reference implementations of common operations.
"""

from itertools import product
from math import cos, pi, sin, sqrt
from typing import List

import numpy as np

from ouster.sdk import core

# TODO: replace link when new FW 2.5/3.0 manual is up


[docs] def xyz_proj_beam_to_sensor_transform(metadata: core.SensorInfo, frame: core.LidarFrame) -> np.ndarray: """Computes a point cloud from a frame as numpy array. This is a reference implementation that follows the calculations from `Section X`_ of the Software User Manual exactly. Output is a point cloud in the *sensor frame* with points arranged in column-major order, with coordinates in meters. Args: metadata: Sensor metadata associated with the frame frame: A frame of lidar data Returns: A H x W x 3 array of point coordinates .. _Section X: https://docs.ouster.com/sensor-docs """ # use homogeneous coordinates for convenient transformation xyz = np.zeros((frame.w * frame.h, 4)) # iterate over each measurement channel/row and measurement block/column for u, v in product(range(frame.h), range(frame.w)): r = frame.field(core.ChanField.RANGE)[u, v] n = sqrt(metadata.beam_to_lidar_transform[0, 3]**2 + metadata.beam_to_lidar_transform[2, 3]**2) # frames are always a full frame, so the measurement id is also the index assert frame.measurement_id[v] == v theta_encoder = 2.0 * pi * (1.0 - v / frame.w) theta_azimuth = -2.0 * pi * (metadata.beam_azimuth_angles[u] / 360.0) phi = 2.0 * pi * (metadata.beam_altitude_angles[u] / 360.0) # zero ranges represent no return; avoid applying offsets to these if r == 0.0: continue # compute point coordinates in the lidar frame x = (r - n) * cos(theta_encoder + theta_azimuth) * cos(phi) + metadata.beam_to_lidar_transform[0, 3] * cos(theta_encoder) y = (r - n) * sin(theta_encoder + theta_azimuth) * cos(phi) + metadata.beam_to_lidar_transform[0, 3] * sin(theta_encoder) z = (r - n) * sin(phi) + metadata.beam_to_lidar_transform[2, 3] # insert into xyz; point order is row-major to match input frame xyz[u * frame.w + v] = [x, y, z, 1] # transform from lidar to sensor frame and scale to meters from millimeters xyz_sensor = xyz @ metadata.lidar_to_sensor_transform.T return xyz_sensor[:, :3].reshape(frame.h, frame.w, 3) * 0.001
[docs] def xyz_proj_origin_to_origin_mm(metadata: core.SensorInfo, frame: core.LidarFrame) -> np.ndarray: """Computes a point cloud from a frame as numpy array This is the old reference implementation that follows the calculations from `Section 3.1.2`_ of the FW 2.0 Software User Manual exactly for OS-0, OS-1, and OS-2 sensors. The output is a point cloud in the *sensor frame* with points arranged in column-major order, with coordinates in meters. Args: metadata: Sensor metadata associated with the frame frame: A frame of lidar data Returns: A H x W x 3 array of point coordinates .. _Section 3.1.2: https://data.ouster.io/downloads/software-user-manual/software-user-manual-v2p0.pdf#a """ # use homogeneous coordinates for convenient transformation xyz = np.zeros((frame.w * frame.h, 4)) # return 0s since this method is not valid for OS-DOME if "OS-DOME" in metadata.prod_line: return xyz # iterate over each measurement channel/row and measurement block/column for u, v in product(range(frame.h), range(frame.w)): r = frame.field(core.ChanField.RANGE)[u, v] n = metadata.lidar_origin_to_beam_origin_mm # frames are always a full frame, so the measurement id is also the index assert frame.measurement_id[v] == v theta_encoder = 2.0 * pi * (1.0 - v / frame.w) theta_azimuth = -2.0 * pi * (metadata.beam_azimuth_angles[u] / 360.0) phi = 2.0 * pi * (metadata.beam_altitude_angles[u] / 360.0) # zero ranges represent no return; avoid applying offsets to these if r == 0.0: continue # compute point coordinates in the lidar frame x = (r - n) * cos(theta_encoder + theta_azimuth) * cos(phi) + n * cos(theta_encoder) y = (r - n) * sin(theta_encoder + theta_azimuth) * cos(phi) + n * sin(theta_encoder) z = (r - n) * sin(phi) # insert into xyz; point order is row-major to match input frame xyz[u * frame.w + v] = [x, y, z, 1] # transform from lidar to sensor frame and scale to meters from millimeters xyz_sensor = xyz @ metadata.lidar_to_sensor_transform.T return xyz_sensor[:, :3].reshape(frame.h, frame.w, 3) * 0.001
[docs] def destagger(pixel_shift_by_row: List[int], field: np.ndarray) -> np.ndarray: """Reference implementation for destaggering a field of data. In the default staggered representation, each column corresponds to a single timestamp. In the destaggered representation, each column corresponds to a single azimuth angle, compensating for the azimuth offset of each beam. Destaggering is used for visualizing lidar data as an image or for algorithms that exploit the structure of the lidar data, such as beam_uniformity in ouster_viz, or computer vision algorithms. Args: pixel_shift_by_row: List of pixel shifts by row from sensor metadata field: Staggered data as a H x W numpy array Returns: Destaggered data as a H x W numpy array """ destaggered = np.zeros(field.shape) nrows = field.shape[0] # iterate over every row and apply pixel shift for u in range(nrows): destaggered[u, :] = np.roll(field[u, :], pixel_shift_by_row[u]) return destaggered