Source code for ouster.sdk.examples.pcap

"""
Copyright (c) 2021, Ouster, Inc.
All rights reserved.

Executable examples for using the pcap APIs.

This module has a rudimentary command line interface. For usage, run::

    $ python -m ouster.sdk.examples.pcap -h
"""
import os
import argparse
import numpy as np

from ouster.sdk import core, pcap
from ouster.sdk.examples.colormaps import normalize


[docs] def pcap_3d_one_frame(source_file: str, num: int = 0, visualize: bool = True): """Render one frame from a pcap file in the Open3D viewer. Args: source: path to pcap num: frame number in a given pcap file (satrs from *0*) visualize: when False, return xyz array without opening a window """ try: import open3d as o3d # type: ignore except ModuleNotFoundError: print( "This example requires open3d, which may not be available on all " "platforms. Try running `pip3 install open3d` first.") exit(1) # open source source = pcap.PcapFrameSetSource(source_file) metadata = source.sensor_info[0] from more_itertools import nth # get single frame by index frames = nth(source, num) if not frames: print(f"ERROR: Frame # {num} in not present in pcap file") source.close() exit(1) frame = frames[0] assert frame is not None # [doc-stag-open3d-one-frame] # compute point cloud using core.SensorInfo and core.LidarFrame xyz = core.XYZLut(metadata)(frame) # [doc-etag-open3d-one-frame] if not visualize: source.close() return xyz # [doc-stag-open3d-one-frame-pointcloud] # create point cloud and coordinate axes geometries cloud = o3d.geometry.PointCloud( o3d.utility.Vector3dVector(xyz.reshape((-1, 3)))) # type: ignore axes = o3d.geometry.TriangleMesh.create_coordinate_frame( 1.0) # type: ignore # initialize visualizer and rendering options vis = o3d.visualization.Visualizer() # type: ignore vis.create_window() vis.add_geometry(cloud) vis.add_geometry(axes) ropt = vis.get_render_option() ropt.point_size = 1.0 ropt.background_color = np.asarray([0, 0, 0]) # initialize camera settings ctr = vis.get_view_control() ctr.set_zoom(0.1) ctr.set_lookat([0, 0, 0]) ctr.set_up([1, 0, 0]) # run visualizer main loop print("Press Q or Escape to exit") vis.run() vis.destroy_window() source.close()
# [doc-etag-open3d-one-frame-pointcloud]
[docs] def pcap_display_xyz_points(source_file: str, num: int = 0, plot: bool = True): """Plot point cloud using matplotlib or return xyz/colors when plot is False.""" # open the source source = pcap.PcapFrameSetSource(source_file) metadata = source.sensor_info[0] # [doc-stag-pcap-render-xyz-points] from more_itertools import nth frames = nth(source, num) if not frames: print(f"ERROR: Frame # {num} in not present in pcap file") exit(1) frame = frames[0] assert frame is not None # transform data to 3d points and graph xyzlut = core.XYZLut(metadata) xyz = xyzlut(frame.field(core.ChanField.RANGE)) key = frame.field(core.ChanField.REFLECTIVITY) [x, y, z] = [c.flatten() for c in np.dsplit(xyz, 3)] colors = normalize(key.flatten()) # [doc-etag-pcap-render-xyz-points] if not plot: source.close() return x, y, z, colors # [doc-stag-pcap-plot-xyz-points] import matplotlib.pyplot as plt # type: ignore # set up figure plt.figure() ax = plt.axes(projection='3d') r = 6 ax.set_xlim3d([-r, r]) # type: ignore ax.set_ylim3d([-r, r]) # type: ignore ax.set_zlim3d([-r, r]) # type: ignore plt.title("3D Points XYZ for frame") ax.scatter(x, y, z, c=colors, s=0.2) # type: ignore plt.show() # [doc-etag-pcap-plot-xyz-points] source.close()
[docs] def pcap_to_las(source_file: str, num: int = 0, las_dir: str = ".", las_base: str = "las_out", las_ext: str = "las") -> None: "Write frames from a pcap to las files (one per lidar frame)." from itertools import islice import laspy # type: ignore # open source source = pcap.PcapFrameSetSource(source_file) metadata = source.sensor_info[0] if (metadata.format.udp_profile_lidar == core.UDPProfileLidar.RNG19_RFL8_SIG16_NIR16_DUAL): print("Note: You've selected to convert a dual returns pcap to LAS. " "Second returns are ignored in this conversion by this example " "for clarity reasons. You can modify the code as needed by " "accessing it through Github or the SDK documentation.") # precompute xyzlut to save computation in a loop xyzlut = core.XYZLut(metadata) # create an iterator of LidarFrames from pcap and bound it if num is specified frames = iter(source) if num: frames = islice(frames, num) for idx, frame_set in enumerate(frames): for frame in frame_set: if frame is None: continue xyz = xyzlut(frame.field(core.ChanField.RANGE)) las = laspy.create() las.x = xyz[:, :, 0].flatten() las.y = xyz[:, :, 1].flatten() las.z = xyz[:, :, 2].flatten() las_path = os.path.join(las_dir, f'{las_base}_{idx:06d}.{las_ext}') print(f'write frame #{idx} to file: {las_path}') las.write(las_path)
[docs] def pcap_to_pcd(source_file: str, num: int = 0, pcd_dir: str = ".", pcd_base: str = "pcd_out", pcd_ext: str = "pcd") -> None: "Write frames from a pcap to pcd files (one per lidar frame)." # open source source = pcap.PcapFrameSetSource(source_file) metadata = source.sensor_info[0] if (metadata.format.udp_profile_lidar == core.UDPProfileLidar.RNG19_RFL8_SIG16_NIR16_DUAL): print("Note: You've selected to convert a dual returns pcap. Second " "returns are ignored in this conversion by this example " "for clarity reasons. You can modify the code as needed by " "accessing it through github or the SDK documentation.") from itertools import islice try: import open3d as o3d # type: ignore except ModuleNotFoundError: print( "This example requires open3d, which may not be available on all " "platforms. Try running `pip3 install open3d` first.") exit(1) if not os.path.exists(pcd_dir): os.makedirs(pcd_dir) # precompute xyzlut to save computation in a loop xyzlut = core.XYZLut(metadata) # create an iterator of LidarFrames from pcap and bound it if num is specified frames = iter(source) if num: frames = islice(frames, num) for idx, frame_set in enumerate(frames): for frame in frame_set: if frame is None: continue xyz = xyzlut(frame.field(core.ChanField.RANGE)) pcd = o3d.geometry.PointCloud() # type: ignore pcd.points = o3d.utility.Vector3dVector(xyz.reshape(-1, 3)) # type: ignore pcd_path = os.path.join(pcd_dir, f'{pcd_base}_{idx:06d}.{pcd_ext}') print(f'write frame #{idx} to file: {pcd_path}') o3d.io.write_point_cloud(pcd_path, pcd) # type: ignore
[docs] def pcap_to_ply(source_file: str, num: int = 0, ply_dir: str = ".", ply_base: str = "ply_out", ply_ext: str = "ply") -> None: "Write frames from a pcap to ply files (one per lidar frame)." # Don't need to print warning about dual returns since this leverages pcap_to_pcd # We are reusing the same Open3d File IO function to write the PLY file out pcap_to_pcd(source_file, num=num, pcd_dir=ply_dir, pcd_base=ply_base, pcd_ext=ply_ext)
[docs] def pcap_query_frame(source_file: str, num: int = 0): """ Example: Query available fields in LidarFrame Args: source_file: Path to pcap file num: frame number in a given pcap file (satrs from *0*) """ # open source source = pcap.PcapFrameSetSource(source_file) frames = iter(source) frame_set = next(frames) print("Available fields and corresponding dtype in LidarFrame") # [doc-stag-pcap-query-frame] for frame in frame_set: if not frame: continue # noqa: E701 for field_name in frame.fields: field_data = frame.field(field_name) print('{0:15} {1}'.format(field_name, field_data.dtype))
# [doc-etag-pcap-query-frame]
[docs] def pcap_read_packets( source_file: str, num: int = 0): """Basic read packets example from pcap file. Args: source_file: Path to pcap file. num: Unused. Included for CLI parity. """ # [doc-stag-pcap-read-lidar-packets] # open source source = pcap.PcapPacketSource(source_file) metadata = source.sensor_info[0] packet_format = core.PacketFormat(metadata) for idx, packet in source: if isinstance(packet, core.LidarPacket): # Now we can process the LidarPacket. In this case, we access measurement_ids = packet_format.packet_header(core.ColHeader.MEASUREMENT_ID, packet.buf) timestamps = packet_format.packet_header(core.ColHeader.TIMESTAMP, packet.buf) ranges = packet_format.packet_field(core.ChanField.RANGE, packet.buf) print(f' encoder counts = {measurement_ids.shape}') print(f' timestamps = {timestamps.shape}') print(f' ranges = {ranges.shape}') # [doc-etag-pcap-read-lidar-packets] # [doc-stag-pcap-read-imu-packets] elif isinstance(packet, core.ImuPacket): # and access ImuPacket content ax = packet_format.imu_la_x(packet.buf) ay = packet_format.imu_la_y(packet.buf) az = packet_format.imu_la_z(packet.buf) wx = packet_format.imu_av_x(packet.buf) wy = packet_format.imu_av_y(packet.buf) wz = packet_format.imu_av_z(packet.buf) print(f' acceleration = {ax}, {ay}, {az}') print(f' angular_velocity = {wx}, {wy}, {wz}') # [doc-etag-pcap-read-imu-packets] source.close()
[docs] def pcap_to_csv( source: str, num: int = 0) -> None: # leave comment directing users to ouster-cli print("NOTICE: The pcap-to-csv example has been retired in favor of " "the ouster-cli utility installed with the Python Ouster SDK.\n" "To try: ouster-cli source <PCAP> save <OUT.CSV>")
[docs] def main(): """Pcap examples runner.""" examples = { "open3d-one-frame": pcap_3d_one_frame, "plot-xyz-points": pcap_display_xyz_points, "pcap-to-las": pcap_to_las, "pcap-to-pcd": pcap_to_pcd, "pcap-to-ply": pcap_to_ply, "pcap-to-csv": pcap_to_csv, "query-frame": pcap_query_frame, "read-packets": pcap_read_packets, } description = "Ouster Python SDK Pcap examples. The EXAMPLE must be one of:\n " + str.join( '\n ', examples.keys()) parser = argparse.ArgumentParser( description=description, formatter_class=argparse.RawTextHelpFormatter) parser.add_argument('pcap_path', metavar='PCAP', help='path to pcap file') parser.add_argument('example', metavar='EXAMPLE', choices=examples.keys(), help='name of the example to run') parser.add_argument('--frame-num', type=int, default=1, help='index of frame to use') args = parser.parse_args() try: example = examples[args.example] except KeyError: print(f"No such example: {args.example}") print(description) exit(1) print(f'example: {args.example}') example(args.pcap_path, args.frame_num)
if __name__ == "__main__": main()