# flake8: noqa: W293
import argparse
import os
[docs]
def osf_read_frames(osf_file: str, limit: int = 10) -> None:
"""Read Lidar Frames from an OSF file.
Shows frames for each sensor in time order stored in the OSF File.
Args:
osf_file: path to osf file.
"""
# [doc-stag-osf-read-imports]
import ouster.sdk.osf as osf
# [doc-etag-osf-read-imports]
# [doc-stag-osf-read-frames]
source = osf.OsfFrameSetSource(osf_file)
count = 0
for frame_set in source:
for frame in frame_set:
if frame is None:
continue
print(f'frame = {frame},'
f' WxH={frame.w}x{frame.h}')
count += 1
if count >= limit:
return
source.close()
# [doc-etag-osf-read-frames]
[docs]
def osf_get_sensors_info(osf_file: str) -> None:
"""Read Lidar Sensors info from an OSF file.
Shows metadata for all sensors found in an OSF file.
Args:
osf_file: path to osf file.
"""
# [doc-stag-osf-get-sensors-info]
from ouster.sdk import osf
frames = osf.OsfFrameSetSource(osf_file)
for sensor_id, info in enumerate(frames.sensor_info):
print(f"sensor[{sensor_id}] = ", info)
frames.close()
# [doc-etag-osf-get-sensors-info]
[docs]
def osf_slice_frames(osf_file: str) -> str:
"""Copy frames from input OSF file with reduction using the Writer API.
Slicing is done via saving only RANGE, SIGNAL and REFLECTIVITY fields into an output OSF files.
"""
from ouster.sdk import core
import ouster.sdk.osf as osf
def make_sliced_fname(f: str) -> str:
"""Generate sliced filename and remove it if it exists."""
output_file = os.path.splitext(os.path.basename(f))[0] + '_sliced.osf'
if os.path.exists(output_file):
os.remove(output_file)
return output_file
output_file = make_sliced_fname(osf_file)
# Frames reader from input OSF
# New field types should be a subset of fields in encoded LidarFrame so we just assume that
# RANGE, SIGNAL and REFLECTIVITY fields will be present in the input OSF file.
# [doc-stag-osf-slice-frames]
frames = osf.OsfFrameSetSource(osf_file)
fields_to_write = [
core.ChanField.RANGE,
core.ChanField.SIGNAL,
core.ChanField.REFLECTIVITY]
writer = osf.Writer(output_file,
frames.sensor_info,
fields_to_write)
# Read frames and write back
for frame_set in frames:
for idx, frame in enumerate(frame_set):
if frame is None:
continue
print(f"writing sliced frame with ts = \
{frame.get_first_valid_packet_timestamp()}")
writer.save(idx, frame)
writer.close()
# [doc-etag-osf-slice-frames]
return output_file
[docs]
def add_objects_to_frame(frame=None):
"""Populate a LidarFrame with example Object instances.
Args:
frame: optional LidarFrame to update directly.
"""
if frame is None:
from ouster.sdk import core
sensor_info = core.SensorInfo.from_default(core.LidarMode._1024x10)
frame = core.LidarFrame(sensor_info)
print(f"Original frame = {frame}, WxH={frame.w}x{frame.h}")
# [doc-stag-add-object]
from ouster.sdk import core
import numpy as np
objects = [core.Object(), core.Object()]
objects[0].id = 1
objects[0].creation_ts = 99
objects[0].timestamp = 199
objects[0].class_id = 1
objects[0].class_confidence = 0.9
objects[0].object_to_body.position = np.array([1, 2, 3])
objects[0].object_to_body.set_rotation(np.array([2, 2, 2]))
objects[0].body_to_world.position = np.array([10, 20, 30])
objects[0].body_to_world.set_rotation(np.array([0.1, 0.2, 0.3]))
objects[0].velocity = np.array([2, 3, 4])
objects[0].dimensions = np.array([1, 1, 1])
objects[0].properties["num_points"] = '[100]'
objects[0].properties["attributes"] = '["eats_icecream", "carries_bag"]'
objects[1].id = 2
objects[1].creation_ts = 100
objects[1].timestamp = 200
objects[1].class_id = 2
objects[1].class_confidence = 0.8
objects[1].object_to_body.position = np.array([3, 2, 1])
objects[1].object_to_body.set_rotation(np.array([1, 1, 1]))
objects[1].body_to_world.position = np.array([4, 5, 6])
objects[1].body_to_world.set_rotation(np.array([0.4, 0.5, 0.6]))
objects[1].velocity = np.array([4, 3, 2])
objects[1].dimensions = np.array([2, 2, 2])
objects[1].properties["num_points"] = '[50]'
objects[1].properties["attributes"] = '["parked_illegaly"]'
frame.objects["test_objects"] = objects
# [doc-etag-add-object]
print(f"Added {len(objects)} objects to frame under key 'test_objects'.")
print(f"Updated frame = {frame}, objects keys = {list(frame.objects.keys())}")
return objects
[docs]
def write_classmaps(osf_path, sensor_info=None):
"""Write ClassMap metadata to an OSF file."""
import ouster.sdk.osf as osf
from ouster.sdk import core
input_source = None
auto_close_writer = False
output_path = osf_path
if sensor_info is None:
input_source = osf.OsfFrameSetSource(str(osf_path))
if not input_source.sensor_info:
input_source.close()
raise ValueError(f"No sensor metadata found in {osf_path}")
sensor_info = input_source.sensor_info[0]
output_path = os.path.splitext(os.path.basename(str(osf_path)))[0] + '_classmaps.osf'
auto_close_writer = True
# [doc-stag-write-classmaps]
writer = osf.Writer(str(output_path), [sensor_info])
class_map1 = core.ClassMap({
1: 'dog',
2: 'cat'
})
class_map2 = core.ClassMap({
1: 'tree',
2: 'bush'
})
class_maps = core.ClassMapSet({
'four_legs': class_map1,
'zero_legs': class_map2
})
metadata = core.FrameSetSourceMetadataSet()
metadata['class_maps'] = class_maps
metadata['additional_info'] = "Test additional info"
writer.save(metadata)
# [doc-etag-write-classmaps]
print(f"Wrote class map metadata to {output_path}")
if auto_close_writer:
writer.close()
if input_source is not None:
input_source.close()
return writer, class_maps, metadata
[docs]
def read_classmaps(osf_path):
"""Read ClassMap metadata from an OSF FrameSetSource."""
# [doc-stag-read-classmaps]
from ouster.sdk import open_source
src = open_source(str(osf_path))
# Unlike C++, no .is<>) check is needed: metadata() returns a
# ClassMapSet directly (the bindings unwrap the stored type for you).
class_map_set = src.metadata('class_maps')
dog_class = class_map_set['four_legs'][1]
# [doc-etag-read-classmaps]
print(f"Example class label for key 1 in 'four_legs': {dog_class}")
src.close()
return src, class_map_set, dog_class
[docs]
def main():
"""OSF examples runner."""
examples = {
"read-frames": osf_read_frames,
"slice-frames": osf_slice_frames,
"get-sensors-info": osf_get_sensors_info,
"add-objects-to-frame": add_objects_to_frame,
"write-classmaps": write_classmaps,
"read-classmaps": read_classmaps,
}
description = "Ouster Python SDK OSF examples. The EXAMPLE must be one of:\n " + str.join(
'\n ', examples.keys())
parser = argparse.ArgumentParser(
description=description, formatter_class=argparse.RawTextHelpFormatter)
parser.add_argument('osf_path', metavar='OSF', nargs='?', help='path to osf file')
parser.add_argument('example',
metavar='EXAMPLE',
choices=examples.keys(),
help='name of the example to run')
args = parser.parse_args()
try:
example = examples[args.example]
except KeyError:
print(f"No such example: {args.example}")
print(description)
exit(1)
print(f'example: {args.example}')
if args.example != "add-objects-to-frame" and not args.osf_path:
parser.error("OSF path is required for this example.")
if args.example == "add-objects-to-frame":
example()
return
example(args.osf_path)
if __name__ == "__main__":
main()