Source code for ouster.sdk.core.reduced_frame_set_source
from typing import Optional, Iterator, List
from ouster.sdk._bindings.client import FrameSetSource
from ouster.sdk.core import SensorInfo, LidarFrame, FrameSet
from ouster.sdk.core.frame_ops import reduce_by_factor, reduce_by_factor_metadata
[docs]
class ReducedFrameSetSource(FrameSetSource):
"""
Takes a regular FrameSetSource and reduces the beams count to the specified values.
"""
def __init__(self, frame_set_source: FrameSetSource, beams: List[int]) -> None:
FrameSetSource.__init__(self)
if len(frame_set_source.sensor_info) != len(beams):
raise ValueError("beams should match the count of sensors")
factor_list = []
for b, m in zip(beams, frame_set_source.sensor_info):
f = m.format.pixels_per_column / b
if not (f.is_integer() and f > 0):
raise ValueError(f"beams {b} must be divisor of {m.format.pixels_per_column}")
factor_list.append(int(f))
self._frame_set_source = frame_set_source
self._factors = factor_list
self._metadata = self._generate_metadata(factor_list)
self._input_sensor_info = self._frame_set_source.sensor_info
def _generate_metadata(self, factor_list):
return [reduce_by_factor_metadata(m, f)
for m, f in zip(self._frame_set_source.sensor_info, factor_list)]
@property
def sensor_info(self) -> List[SensorInfo]:
return self._metadata
@property
def is_live(self) -> bool:
return self._frame_set_source.is_live
@property
def is_indexed(self) -> bool:
return self._frame_set_source.is_indexed
@property
def frames_num(self) -> List[int]:
return self._frame_set_source.frames_num
def __len__(self) -> int:
return len(self._frame_set_source)
def __length_hint__(self) -> int:
return self._frame_set_source.__length_hint__()
def __iter__(self) -> Iterator[FrameSet]:
def reduce_frame(frame, factor, sensor_info):
out = reduce_by_factor(frame, factor)
out.sensor_info = sensor_info
return out
for frames in self._frame_set_source:
out: List[Optional[LidarFrame]] = []
for frame in frames:
for idx, info in enumerate(self._input_sensor_info):
if frame is not None and info is frame.sensor_info:
break
if frame is None:
out.append(None)
else:
out.append(reduce_frame(frame, self._factors[idx], self._metadata[idx]))
yield FrameSet(out)
[docs]
def close(self) -> None:
pass
def __del__(self) -> None:
self.close()
def _reduce_fn(self: FrameSetSource, beams: List[int]) -> FrameSetSource:
"""
Takes a regular FrameSetSource and reduces the beams count to the specified values.
"""
return ReducedFrameSetSource(self, beams)
# allow assigning this
FrameSetSource.reduce = _reduce_fn # type: ignore