# type: ignore
from typing import Iterator, List, Tuple, Union, Optional
import numpy as np
import math
from threading import Lock
import logging
from ouster.sdk.core import (SensorInfo, PacketFormat, PacketValidationFailure,
LidarPacket, ImuPacket, Packet, ZonePacket)
from ouster.sdk.util import resolve_metadata_multi
from pathlib import Path
from ouster.sdk._bindings.client import populate_extrinsics
from ctypes import Structure, c_uint16, c_uint32, c_uint64
from ouster.sdk._bindings.client import PacketSource as _PacketSource
import sqlite3
from rosbags.highlevel import AnyReader # type: ignore
from rosbags.typesys import Stores, get_typestore, get_types_from_msg # type: ignore
logger = logging.getLogger("bag-logger")
# monkey patch sqlite connect to not enforce that it is called from only one thread
# if we don't do this we crash in the CLI when opening db3 bags
_old_connect = sqlite3.connect
def _new_connect(*args, **kwargs):
kwargs['check_same_thread'] = False
return _old_connect(*args, **kwargs)
sqlite3.connect = _new_connect
[docs]
class MessageCount(Structure):
_pack_ = 1
_fields_ = [
('id', c_uint16),
('count', c_uint64),
]
def _anybag_monkey(self, paths, default_typestore=None):
if ".mcap" not in str(paths[0]):
self.old_init(paths, default_typestore=default_typestore)
return
from rosbags.rosbag2 import Reader as Reader2
from rosbags.typesys import Stores, get_typestore # type: ignore
self.is2 = True
self.readers = [Reader2(paths, default_typestore=default_typestore)]
self.isopen = False
self.connections = []
self.typestore = get_typestore(Stores.EMPTY) if default_typestore is None else default_typestore
def _bag2_monkey(self, paths, default_typestore=None):
path = paths[0] if type(paths) is list else paths
if ".mcap" not in str(path):
self.old_init(paths)
return
from rosbags.interfaces import Connection, ConnectionExtRosbag2
from rosbags.rosbag2.storage_mcap import MCAPFile
f = MCAPFile(path)
f.open()
schemas = f.get_schema_definitions()
counts = {}
# read message counts for each stream
total_count = 0
for i in range(0, len(f.statistics.channel_message_counts) // 10):
item = f.statistics.channel_message_counts[i * 10:i * 10 + 10]
c = MessageCount.from_buffer_copy(item)
counts[c.id] = c.count
total_count = total_count + c.count
# read in metadata for each channel to get offered qos profiles
qos = {}
for i, c in f.channels.items():
# each metadata is a Map<string, string>
i = 0
while i < len(c.metadata):
key_len = ChannelMetadata.from_buffer_copy(c.metadata[i:i + 4]).len
i = i + 4
key = c.metadata[i:i + key_len].decode("utf-8")
i = i + key_len
value_len = ChannelMetadata.from_buffer_copy(c.metadata[i:i + 4]).len
i = i + 4
value = c.metadata[i:i + value_len].decode("utf-8")
i = i + value_len
if key == "offered_qos_profiles":
qos[c.schema] = value
conns = []
for id, c in f.channels.items():
con = Connection(id = id, topic=c.topic, msgtype=c.schema,
msgdef=schemas[c.schema][1],
msgcount = counts.get(id, 0),
ext = ConnectionExtRosbag2(serialization_format='cdr',
offered_qos_profiles=qos.get(c.schema, '')),
owner = self, digest = None)
conns.append(con)
self.isopen = True
self.is2 = True
self.metadata = {}
self.metadata["storage_identifier"] = "mcap"
self.metadata["starting_time"] = {'nanoseconds_since_epoch': f.statistics.start_time}
duration = f.statistics.end_time - f.statistics.start_time
self.metadata["duration"] = {'nanoseconds': duration}
self.metadata["message_count"] = total_count
self.paths = paths
self.storage = f
self.connections = conns
self.tmpdir = None
[docs]
class BagPacketSource(_PacketSource):
"""Read a sensors packet streams out of a bag file as an iterator."""
_metadata: List[SensorInfo]
def __init__(self,
bag_path: Union[str, List[str]],
*,
extrinsics_file: Optional[str] = None,
meta: Optional[List[str]] = None,
soft_id_check: bool = False,
extrinsics: List[np.ndarray] = []):
"""Read sensor data streams from a single bag file.
Args:
bag_path: path to bag file or folder containing ROS2 db3 and yaml file
meta: optional list of metadata files to load, if not provided metadata
is loaded from the bag instead
soft_id_check: if True, don't skip packets on init_id mismatch
"""
_PacketSource.__init__(self)
self._soft_id_check = soft_id_check
self._id_error_count = 0
self._size_error_count = 0
self._lock = Lock()
self._reset = False
self._typestore = get_typestore(Stores.ROS2_FOXY)
if type(bag_path) is list:
if len(bag_path) > 1:
raise ValueError("Only one bag file can be opened at a time per source.")
self._bag_path = bag_path[0]
else:
self._bag_path = bag_path
from rosbags.rosbag2 import Reader as Reader2
# lets monkeypatch AnyReader
if AnyReader.__init__ != _anybag_monkey:
AnyReader.old_init = AnyReader.__init__
AnyReader.__init__ = _anybag_monkey
if Reader2.__init__ != _bag2_monkey:
Reader2.old_init = Reader2.__init__
Reader2.__init__ = _bag2_monkey
msg_text = """
uint8[] buf
"""
self._typestore.register(get_types_from_msg(msg_text, "ouster_sensor_msgs/msg/PacketMsg"))
self._typestore.register(get_types_from_msg(msg_text, "ouster_msgs/msg/PacketMsg"))
self._reader = AnyReader([Path(self._bag_path)], default_typestore=self._typestore)
self._reader.open()
connections = self._reader.connections
pkt_msg_types = ['ouster_ros/msg/PacketMsg', "ouster_sensor_msgs/msg/PacketMsg", "ouster_msgs/msg/PacketMsg"]
pkt_connections = [x for x in connections if x.msgtype in pkt_msg_types]
imu_connections = [x for x in pkt_connections if "imu_packets" in x.topic]
lidar_connections = [x for x in pkt_connections if "lidar_packets" in x.topic]
zone_connections = [x for x in pkt_connections if "zone_packets" in x.topic]
metadata_connections = [x for x in connections if x.msgtype == 'std_msgs/msg/String' and "metadata" in x.topic]
metadata_paths = None
# now try and map topics to lidars,
self._id_map = {}
self._metadata = [None] * len(lidar_connections) # type: ignore
self._msg_connections = []
# to do this lets go through lidar topics and find matching imu and metadata
for idx, conn in enumerate(lidar_connections):
namespace = '/'.join(conn.topic.split('/')[0:-1]) + "/"
self._msg_connections.append(conn)
self._id_map[conn.topic] = (idx, 0)
for conn2 in imu_connections:
if namespace in conn2.topic:
self._id_map[conn2.topic] = (idx, 1)
self._msg_connections.append(conn2)
break
for conn2 in zone_connections:
if namespace in conn2.topic:
self._id_map[conn2.topic] = (idx, 3)
self._msg_connections.append(conn2)
break
if meta is None:
metadata_found = False
for conn2 in metadata_connections:
if namespace in conn2.topic:
self._id_map[conn2.topic] = (idx, 2)
metadata_found = True
break
if not metadata_found:
# try and fallback to metadata resolving if we couldnt find metadata in the bag
if metadata_paths is None:
metadata_paths = resolve_metadata_multi(bag_path)
if idx < len(metadata_paths):
meta = metadata_paths
else:
raise RuntimeError(f"ERROR could not find metadata for topic {conn.topic}")
if meta is None:
for connection, timestamp, rawdata in self._reader.messages(connections=metadata_connections):
if connection.topic in self._id_map:
msg = self._reader.deserialize(rawdata, connection.msgtype)
self._metadata[self._id_map[connection.topic][0]] = SensorInfo(msg.data) # type: ignore
else:
if len(meta) != len(self._metadata):
raise ValueError(f"Incorrect number of metadata files provided. Expected"
f" {len(self._metadata)} got {len(meta)}.")
for idx, m in enumerate(meta):
with open(m, 'r') as file:
self._metadata[idx] = SensorInfo(file.read())
# estimate the frame count from packet count
self._frame_count = 0
for con in lidar_connections:
ppf = self._metadata[self._id_map[con.topic][0]].format.lidar_packets_per_frame()
self._frame_count += math.ceil(con.msgcount / ppf)
self._pf = []
for m in self._metadata:
pf = PacketFormat(m)
self._pf.append(pf)
# populate extrinsics
populate_extrinsics(extrinsics_file or "", extrinsics or [], self._metadata)
def __length_hint__(self):
return self._frame_count
def __iter__(self) -> Iterator[Tuple[int, Packet]]:
with self._lock:
if self._reader is None:
raise ValueError("I/O operation on closed packet source")
self._reset = True
while self._reset:
self._reset = False
for connection, timestamp, rawdata in self._reader.messages(connections=self._msg_connections):
if self._reset:
break
msg = self._reader.deserialize(rawdata, connection.msgtype)
idx = self._id_map[connection.topic][0]
msg_type = self._id_map[connection.topic][1]
msg_len = len(msg.buf)
packet: Union[LidarPacket, ImuPacket, ZonePacket]
if msg_type == 0:
msg_len = len(msg.buf)
if msg_len != self._pf[idx].lidar_packet_size:
# are we off by one? (older ouster-ros bags are off by 1)
if msg_len == self._pf[idx].lidar_packet_size + 1:
msg_len -= 1
else:
print(f"got an unexpected lidar packet size {msg_len} != "
f"{self._pf[idx].lidar_packet_size} for sensor {idx}")
self._size_error_count += 1
continue
packet = LidarPacket(self._pf[idx])
packet.buf[:] = msg.buf[:msg_len]
elif msg_type == 1:
if msg_len != self._pf[idx].imu_packet_size:
# are we off by one? (older ouster-ros bags are off by 1)
if msg_len == self._pf[idx].imu_packet_size + 1:
msg_len -= 1
else:
print(f"got an unexpected imu packet size {msg_len} != "
f"{self._pf[idx].imu_packet_size} for sensor {idx}")
self._size_error_count += 1
continue
packet = ImuPacket(self._pf[idx])
packet.buf[:] = msg.buf[:msg_len]
elif msg_type == 3:
# this packet is new so does not have the off by one issue
if msg_len != self._pf[idx].zone_packet_size:
print(f"got an unexpected zone packet size {msg_len} != "
f"{self._pf[idx].zone_packet_size} for sensor {idx}")
self._size_error_count += 1
continue
packet = ZonePacket(self._pf[idx])
packet.buf[:] = msg.buf[:msg_len]
else:
continue
packet.host_timestamp = timestamp
packet.format = self._pf[idx]
res = packet.validate(self._metadata[idx])
if res == PacketValidationFailure.NONE:
yield (idx, packet)
# don't need to check for size since we validate that above
elif res == PacketValidationFailure.ID:
self._id_error_count += 1
if self._soft_id_check:
yield (idx, packet)
@property
def sensor_info(self) -> List[SensorInfo]:
"""Metadata associated with the packet."""
return self._metadata
@property
def is_live(self) -> bool:
return False
@property
def is_indexed(self) -> bool:
return False
# diagnostics
@property
def id_error_count(self) -> int:
return self._id_error_count
@property
def size_error_count(self) -> int:
return self._size_error_count
[docs]
def restart(self) -> None:
"""Restart playback, only relevant to non-live sources"""
with self._lock:
self._reset = True
[docs]
def close(self) -> None:
"""Release Pcap resources. Thread-safe."""
with self._lock:
self._reader.close()
self._reader = None # type: ignore
@property
def closed(self) -> bool:
"""Check if source is closed. Thread-safe."""
with self._lock:
return self._reader is None