Skip to navigation

Get the telemetry information

Get the sensor telemetry information

Response

Valid telemetry query result
timestamp_nsuint64Optional
Time at which the information was collected
phase_lock_statusenumOptional

The current phase-lock status will not indicate loss of lock if the time synchronization is lost.

Allowed values:
input_voltage_mvintegerOptional

Reports system input-voltage in millvolts

internal_temperature_deg_cintegerOptional

Reports system temperature in degrees C

Only available on Rev 06 and above sensors.

input_current_maintegerOptional

System input-current in milliamps