Skip to navigation

Get render time estimate for zone set

Returns an estimate of the time required to render STL files without corresponding ZRBs. Zones that have ZRBs already rendered are not counted, even if config have been changes made that will invalidate them.

Path parameters

zone_setenumRequired
Zone set identifier. Valid values are 'active' or 'staged'. The 'pending' set is a transient state and should not be used.
Allowed values:

Response

Render time estimate
estimate_msinteger>=0
Estimated render time in milliseconds
total_trianglesinteger>=0
Total number of triangles across zones needing rendering
zone_countinteger>=0
Number of zones that need rendering