Windows
Tested on Windows 10. The sensor hostname is os-991234567890.local (serial number on the sticker on top of the sensor).
Connecting the Sensor
- Connect the sensor to an available Ethernet port on the host machine or router.
- The sensor automatically obtains an IP address via link-local or DHCP, depending on network configuration.
It can take up to 60 seconds to obtain an IP address after initial power-up.
The Sensor Homepage
- Enter
http://os-991234567890.local/in your browser’s address bar to open the sensor homepage.
If the sensor homepage does not load, follow the steps in Determining the IPv4 Address of the Sensor to verify the sensor has a valid IP address.
Determining the IPv4 Address of the Sensor
-
Open a Command Prompt by pressing Win+X, then A.
-
Ping the sensor to find its IPv4 address:
Command
Example
If this command hangs, configure your interface to link-local first.
Response
In this example, the sensor IPv4 address is 192.0.2.130. An address of the form 169.254.x.x means it is connected via link-local.
- Alternatively, resolve the sensor IP using
dns-sd:
Command
Example
Response
An address of the form 169.254.x.x means the sensor is connected via link-local.
Determining the IPv4 Address of the Interface
-
Open a Command Prompt by pressing Win+X, then A.
-
View the IPv4 address of your interfaces:
Command
Example
Response
- In this example, the sensor is plugged into interface
"Local Area Connection". - The host IPv4 address is on the
IP Address:line — here,169.254.1.100.
An interface address of the form 169.254.x.x means Windows self-assigned a link-local address in the absence of a DHCP server.
Setting the Host Interface to DHCP
Set the interface to obtain an IP address automatically via DHCP. Useful for plug-and-play setups.
Command
Example — with interface name "Local Area Connection":
Response: (no output)
Setting the Host Interface to Static IP
Assign a static IPv4 address to the interface. Useful when the sensor must send data to a specific IP.
Command
Example — with interface name "Local Area Connection" and IPv4 address 192.0.2.1/24:
/24 is shorthand for Subnet Mask 255.255.255.0.
Response: (no output)
Finding a Sensor with mDNS Service Discovery
The sensor announces itself on the network via mDNS with service type _ouster-lidar._tcp. Use Bonjour Browser to locate all sensors on Windows.
Example using Bonjour Browser:
Step 1: Download Bonjour Browser.


Step 2: The sensor appears under _ouster-lidar._tcp. Click it to view all sensor details.