GPS/GNSS Synchronization
GPS/GNSS Synchronization
For GPS wiring instructions, see GPS/GNSS Synchronization in the hardware user manual.
Configuring the Ouster Sensor
With GPS connections in place, configure the following parameters to synchronize the sensor’s timestamp to the GPS signal:
Checking for Sync
After applying the configuration above, verify synchronization using GET /api/v1/time:
-
PPS lock — the response should include:
If not, recheck
sync_pulse_in_polarity. -
NMEA lock — the response should include:
If not, recheck
multipurpose_io_polarityandnmea_baud_rate. -
NMEA decoding —
last_read_messageshould contain a valid GPRMC sentence: -
Timestamp —
timestamp.modeshould beTIME_FROM_SYNC_PULSE_INandtimestamp.timeshould reflect valid GPS time.
Example Response
Full example output from GET /api/v1/time: