Tuning Process
This section covers the primary settings used to optimize Detect performance for specific environments and use cases. While the system includes numerous parameters, this guide focuses on the subset most effective for fine-tuning detection accuracy. See Settings for instructions on adjusting the settings through the Detect Viewer.
Profiles
By adjusting settings, Detect can be optimized for different use cases depending on the application. Detect provides predefined groups of settings values referred to as settings profiles. Detect ships with 6 preconfigured settings profiles:
Profile Name |
Best Use Case |
Hardware |
Background Subtraction |
Stationary Timeout |
|---|---|---|---|---|
people_settings |
High-precision pedestrian detection. Biased against vehicles. |
CPU |
Yes |
3 Minutes |
its_settings |
Balanced detection for people, bicycles, and vehicles. |
CPU |
Yes |
3 Minutes |
security_settings |
Detects crouching, crawling, or fast running. Note: Higher false positives for small objects. |
CPU |
Yes |
3 Minutes |
dl_people_settings |
High-accuracy pedestrian detection using Deep Learning. |
GPU |
Yes |
5.5 Hours |
dl_its_settings |
Mixed outdoor environments using Deep Learning. |
GPU |
Yes |
5.5 Hours |
dl_parking_settings |
Ideal for stationary vehicles. Detects objects immediately on startup. |
GPU |
No |
Persistent |
Note when switching profiles to one using background subtraction, objects will not be visible for 20 seconds until the background filter initializes. Profiles can be configured using the Detect Viewer. See Settings for instructions on switching profiles.
For details on the differences between the profiles please refer to Perception Tuning in the appendix.
Additional Changes
Improving Computation Time
In some cases, we may need to improve computation time. If the system is not keeping up with the sensor data it will sporadically drop frames to stay live, resulting in a diagnostic warning and reduced accuracy.
To check how close the system is to keeping up lowest_frame_rate fields is available in telemetry. If the lowest_frame_rate is lower than the configured sensor frame rate then data will sometimes be dropped.
Reducing the amount of data processed
The simplest way to improve computation is to reduce the amount of data that the system processes.
If a lidar is placed against a wall or poll removing the azimuths that point towards the near range blocking objects will improve computation and have no effect on performance.
If only close range objects are important, reduce the resolution of the lidar. For ranges less that 20 meters reducing to 512x10 will have minimal impact on detection.
If there are areas in the lidar field of view that are not of interest an exclusion zone can be used.
Improving computation through tuning
If the system is still running slow, the next step is to determine which part of the system is running too slow. To determine the cause, a user can use swagger and benchmark timer endpoint to pinpoint which section of the system is slowest. The benchmark timer lists the modules from slowest to fastest.
There are 2 circumstances that need to be handled differently:
object_pipelineslow due to a large number of people.lidar_pipelinedue to either slow ML inference or slowbackground_filter
For the Object Pipeline:
The user can adjust the data_association/distance_threshold
Setting |
Description |
Original |
Proposed |
|---|---|---|---|
/object_pipeline/ data_association/ distance_threshold |
This is the distance to check for associations between the predicted position, and the cluster positions. The smaller this value, the more likely we will fail to associate to the correct object, however the computation time will reduce as well. |
1.5 |
1.0 |
For the Lidar Pipeline:
When using ML profiles, the user should decrease the ML AOD, as shown in the Gemini Detect Viewer section of the guide.
When using profiles that make use of the background filter, the user should decrease the background filter settings as shown below.
Setting |
Description |
Original |
Proposed |
|---|---|---|---|
/lidar_pipeline/ background_filter/ range_resolution |
This is the depth of each bin in the range image. Each bin stores an occupancy percentage, and if it is less than that percentage, then it is considered to be typically not occupied. Increasing this range decreases the number of bins to update, decreasing the computation. This will result in lower resolution of the background, resulting in more points to be background. |
0.25 |
0.35 |
/lidar_pipeline/ background_filter/ max_range |
This is the maximum range used for analysis. Decreasing the range will reduce memory usage and computation. |
150 |
100 |
Track People and Vehicles
If the user does not want to track bicycles or large vehicles, it is recommended to switch to the heuristic classifier. The heuristic classifier will only classify people and vehicles, while the probabilistic classifiers will classify people, vehicles, bicycles, and large vehicles, because it needs to classify more types of objects, it’s accuracy will be lower.
Note
For heuristic classifier, bicycle classification is primarily based on speed since the size between people and bicycles are similar. Slow moving bicycles will likely show as people, and fast moving bicycles will likely show up as vehicles.
Setting |
Description |
Original |
Proposed |
|---|---|---|---|
/object_pipeline/ classifier/algorithm |
The classification algorithm to use. Supported algorithms are: |
|
|
Decreasing the Number of Unknowns
The user may want to decrease the number of unknowns within their scene. We can configure this with various settings, however some drawbacks to this:
Reason for the required minimum distance travelled for being classified, is to get a better understanding of the object’s speed. A moving object is easier to classify.
Minimum distance travelled also gives objects entering the scene enough time to potentially get better coverage within the scene, so that the object’s size is better captured.
There will be more objects misclassified throughout the scenes. Stationary objects like chairs, boxes, desks could all be classified since they no longer meet a required distance.
Setting |
Description |
Original |
Proposed |
|---|---|---|---|
/object_pipeline/ classifier/ heuristic/ person_min_duration and, /object_pipeline/ classifier/ heuristic/ vehicle_min_duration or, /object_pipeline/ classifier/bayes/ classification_min_duration |
The minimum time for a prospect to be detected before it is promoted to an unknown |
1 |
0 |
/object_pipeline/ classifier/heuristic/ person_min_distance_travelled and, /object_pipeline/ classifier/heuristic/ vehicle_min_distance_travelled or, /object_pipeline/ classifier/bayes/ classification_min_distance_travelled |
The minimum distance for a prospect to travel before it is promoted to an unknown |
2 |
0 |
Prevent Things Turning to Background
If an object is stationary in the scene for an extended period of time, you may not want objects to change as quickly to background. This is configurable, and we can increase the time objects persist in the object. Some drawbacks to this:
Moved stationary objects (chairs, boxes, desks) will stay as objects for a longer period of time
If the server is restarted, it will take much longer to initialize the background.
Setting |
Description |
Original |
Proposed |
|---|---|---|---|
/lidar_pipeline/ background_filter/ fade_time |
Maximum time in seconds for an object to fade to background |
200 |
6000 |
/lidar_pipeline/ background_filter/ fade_to_free_ratio |
How fast an occupied space changes to background vs an occupied space changes to be considered unoccupied. This ratio gets scaled by free_space_rate_doubling_frames so continuously unoccupied area free quickly. If vegetation is showing as objects turn this up to have it more likely to get filtered out. |
3 |
5 |
Improving Detections in Heavy Wind
In windy conditions resulting in sensor movement, Detect can create multiple false positive objects from clustering the ground together. The background filter can be made more aggressive to handle this. This will reduce false positive objects throughout the scene. However, with a more aggressive background filter the likelihood of some objects not being tracked is higher, meaning that there is a higher chance of false negative objects at farther ranges.
Setting |
Description |
Original |
Proposed |
|---|---|---|---|
/lidar_pipeline/ background_filter/ neighbour_check_range |
The background filter checks its neighbours to see if the return is typically occupied in the neighbouring cells. By increasing this, it increasing the tolerance of movement. |
1 |
2 |
/lidar_pipeline/ background_filter/ check_diagonal_neighbours |
Setting this to true will enable checking more neighbours for this occupancy threshold. Having this set will allow for more aggressive background filtering. |
false |
true |
Preventing Small (in any dimension) Objects from Disappearing
There is a ClusterFilter module, which filters clusters based on the number of points, the minimum side length, and minimum vertical size. This module exists to avoid small noisy foreground point clusters from appearing and being tracked, reducing the number of false positives.
Sometimes there is a need to track small clusters, such as as people laying down.
Setting |
Description |
Original |
Proposed |
|---|---|---|---|
/lidar_pipeline/ cluster_filter/ min_side_length |
The minimum side length for an object to be tracked. If a cluster has a side length smaller than this, it will be filtered. |
0.15 |
<0.15 |
/lidar_pipeline/ cluster_filter/ min_vertical_size |
The minimum height for a cluster. A cluster will height smaller than this will be filtered. |
0.3 |
<0.3 |
Increase Likelihood of Detection Small Objects at Far Ranges
There are several filters being used to reduce noisy detections in a general scene. In some cases it may be acceptable to increase the probability of false positive objects while simultaneously increasing the probability of detection for small objects at range.
Increasing the resolution of the sensor can often result in further detection ranges. The higher resolution increases the likelihood multiple beams hit a single object. Increasing from 1024 to 2048 is recommended.
The settings in Preventing Small (in any dimension) Objects from Disappearing should be applied as well as the following settings:
Setting |
Description |
Original |
Proposed |
|---|---|---|---|
/lidar_pipeline/ foreground_filter min_num_neighbours |
The number of directly adjacent points a given point must have to prevent it from being discarded as noise |
3 |
<3 |
/lidar_pipeline/ cluster_filter/ min_num_points |
The number of points a cluster must contain to prevent it from being discarded (as noise). |
7 |
<7 |
Increasing NearIR Image Publish Frequency
It may be preferred to increase the publish frequency for display.
Setting |
Description |
Original |
Proposed |
|---|---|---|---|
/image/image_publish_period |
The period of time for a image to be published (s) |
2 |
0.1 |
/image/image_channel |
The image to publish. Supports either reflectivity or near_ir |
reflectivity |
nearir |
Adjust sensor blockage detector
The table below lists the settings for adjusting the blockage detection functionality.
Setting |
Value range |
Default value |
Description |
|---|---|---|---|
max_range |
0 - 200 |
3.0 |
Limits the range where we consider something an obstruction. Points beyond this value are not considered for blockage detection. Can be increased if users care about obstructions beyond 3 meters. |
max_range_ratio_threshold |
1.0 - 3.0 |
1.2 |
Controls how sensitive the detector is to range changes. Represents the allowed ratio between the current max range measurements and average past measurements. Increasing this number will make the blockage detector less sensitive. |
max_return_ratio_threshold |
1.0 - 1.5 |
1.2 |
Controls how sensitive the detector is to measurement changes (i.e lack of return that might happen due to very close objects. Increasing this number will make the blockage detector less sensitive. |
memory_factor |
0.0 - 1.0 |
0.995 |
Controls how fast the system adjusts to changes in range measurements. If the value is close to 1, the blockage detector will slowly adjust to movements in the scene. If the value is close to 0, the blockage detector will quickly adjust to movements in the scene. If the blockage detector is giving false positives due to weather conditions (i.e., rain or fog), reducing this value may remove those false positives. |
Reducing the effect of reflections, wind or rain
Using different returns from the lidar can minimize the effect of reflections or environmental factors. The system can be configured for the return modes based on the /lidar_manager/return_selection settings. Changing this setting will only affect sensors once perception is reset or the lidar is removed + added.
The three return modes are:
Farthest: This is the default for outdoor profiles. It means that Gemini will process the furthest return from each detection. This is optimal for outdoor scenarios because it reduces the chance that snow, rain or dust prevent getting a return from objects of interest. It also helps see objects through partial obstructions such as light foilage or a wire fence. It does increase the chance that reflections (such as off wet ground or windows are detected as objects) but exclusion area can be used to filter those areas.
Nearest: This is the default for indoor profiles. It reduces the chance that reflection will affect the system.
Strongest: This is a compromise between Farthest and Nearest. It should be used when reflections areas cannot be filtered out but there is a risk that close returns prevent detections of the objects of interest.
Recovering Objects After Lidar Outages
In scenarios where lidar outages may occur, the refind_parking module can be
enabled to recover objects that have not moved during the outage. When the lidar
comes back online, objects may initially re-appear with different object IDs. The
refind_parking module recovers these objects to their original object IDs from
before the outage.
By default the module only recovers objects across brief, in-memory outages. Enabling persistent caching additionally writes the object cache to disk so that object IDs are recovered across perception restarts — including software updates, settings changes that reset perception, and server outages — up to the configured cache expiration.
To enable this, configure the following settings:
Setting |
Description |
Original |
Proposed |
|---|---|---|---|
/object_pipeline/ refind_algorithm |
The algorithm to use for recovering lost objects. |
|
|
/object_pipeline/ refind_parking/enable |
Whether to enable the refind_parking module. |
false |
true |
/object_pipeline/ refind_parking/ lost_object_expire_duration |
The maximum time, in seconds, that a lost object will be remembered for recovery. Set this to the maximum outage duration you want to recover from. Setting this too high can result in false positive refinds of objects that have actually left the scene. |
0 |
120 |
/object_pipeline/ refind_parking/ enable_persistent_caching |
Whether to write the refind cache to disk so recovered object IDs persist across perception restarts (software updates, settings resets, and server outages). |
false |
true |
The persistent cache is controlled by the following parameters under
object_pipeline/refind_parking. The defaults suit most deployments.
Parameter |
Description |
Default |
|---|---|---|
enable_persistent_caching |
Writes the refind cache to disk so recovered object IDs persist across perception restarts. When disabled, recovery is limited to in-memory outages. |
false |
cache_write_interval_s |
How often, in seconds, the object cache is written to disk while running. |
30 |
cached_object_expiration_s |
Maximum age, in seconds, of the on-disk cache. On startup, a cache older than this is rejected as stale and cached IDs are not reloaded. Increase this to recover IDs across longer outages. |
7200 |
boot_cache_alert_delay_s |
How long, in seconds, after startup to wait before checking whether cached objects re-matched and raising the “objects not matched” alert. |
10 |
boot_cache_unmatched_alert_count |
Number of unmatched cached objects that triggers the “objects not matched” alert. |
1 |
Removing person and bike false positives when using parking profile
When using dl_parking settings or other ml based detection security settings, sometimes smaller objects which are a similar size/profile as people or bikes can show up as a false positives. These can be eliminated by using the background filter to remove small objects that are stationary for a long period of time. This will increase computation. To do this the following settings should be applied:
Setting |
Description |
Original |
New |
|---|---|---|---|
/lidar_pipeline/enable_background_filter/ |
Whether to run the background filter |
false |
true |
/lidar_pipeline/filter_non_vehicles_using_background |
Whether to filter out people or bicycle objects that have been stationary for a long time. A smaller number will filter small stationary moved objects faster but also risk filtering stationary people. |
false |
true |
/lidar_pipeline/background_filter/fade_time |
How long before stationary small objects to start getting filtered out |
600 |
As desired. Should be larger that the maximum time a person will remain stationary. |