Frame Start Control
Supported in firmware v3.2 or later.
Configurable start-of-frame control is available through lidar_frame_azimuth_offset. This parameter rotates the lidar frame in millidegrees, shifting the azimuth at which each frame starts.
For example, setting lidar_frame_azimuth_offset to 90000 rotates the lidar frame by 90 degrees. Other angular configuration parameters, such as azimuth_window and phase_lock_offset, are applied relative to this offset.
Set the offset with POST /api/v1/sensor/config: