Get the telemetry information

Open in Claude
Get the sensor telemetry information

Response

Valid telemetry query result
timestamp_nsuint64Optional
Time at which the information was collected
phase_lock_statusenumOptional

The current phase-lock status will not indicate loss of lock if the time synchronization is lost.

input_voltage_mvintegerOptional

Reports system input-voltage in millvolts

internal_temperature_deg_cintegerOptional
Reports system temperature in degrees C Only available on Rev 06 and above sensors.
input_current_maintegerOptional

System input-current in milliamps