version.h

Version

struct ouster::util::version

Public Members

uint16_t major

Major version number.

uint16_t minor

Minor version number.

uint16_t patch

Patch(or revision) version number.

std::string ouster::util::to_string(const version &v)

Get string representation of a version.

Parameters

v – [in] version.

Returns

string representation of the version.

version ouster::util::version_of_string(const std::string &s)

Get version from string.

Parameters

s – [in] string.

Returns

version corresponding to the string, or invalid_version on error.

inline bool operator==(const version &u, const version &v)

Equality operation for version structs.

Parameters
  • u – [in] The first version to compare.

  • v – [in] The second version to compare.

Returns

If the versions are the same.

inline bool operator<(const version &u, const version &v)

Less than operation for version structs.

Parameters
  • u – [in] The first version to compare.

  • v – [in] The second version to compare.

Returns

If the first version is less than the second version.

inline bool operator<=(const version &u, const version &v)

Less than or equal to operation for version structs.

Parameters
  • u – [in] The first version to compare.

  • v – [in] The second version to compare.

Returns

If the first version is less than or equal to the second version.

inline bool operator!=(const version &u, const version &v)

In-equality operation for version structs.

Parameters
  • u – [in] The first version to compare.

  • v – [in] The second version to compare.

Returns

If the versions are not the same.

inline bool operator>=(const version &u, const version &v)

Greater than or equal to operation for version structs.

Parameters
  • u – [in] The first version to compare.

  • v – [in] The second version to compare.

Returns

If the first version is greater than or equal to the second version.

inline bool operator>(const version &u, const version &v)

Greater than operation for version structs.

Parameters
  • u – [in] The first version to compare.

  • v – [in] The second version to compare.

Returns

If the first version is greater than the second version.