client.h

Client Initialization

std::shared_ptr<client> init_client(const std::string &hostname, int lidar_port, int imu_port)

Listen for sensor data on the specified ports; do not configure the sensor.

Parameters
  • hostname – [in] The hostname to connect to.

  • lidar_port – [in] port on which the sensor will send lidar data.

  • imu_port – [in] port on which the sensor will send imu data.

Returns

pointer owning the resources associated with the connection.

std::shared_ptr<client> init_client(const std::string &hostname, const std::string &udp_dest_host, lidar_mode ld_mode = MODE_UNSPEC, timestamp_mode ts_mode = TIME_FROM_UNSPEC, int lidar_port = 0, int imu_port = 0, int timeout_sec = 60)

Connect to and configure the sensor and start listening for data.

Parameters
  • hostname – [in] hostname or ip of the sensor.

  • udp_dest_host – [in] hostname or ip where the sensor should send data or “” for automatic detection of destination.

  • ld_mode – [in] The lidar mode to use.

  • ts_mode – [in] The timestamp mode to use.

  • lidar_port – [in] port on which the sensor will send lidar data. When using zero the method will automatically acquire and assign any free port.

  • imu_port – [in] port on which the sensor will send imu data. When using zero the method will automatically acquire and assign any free port.

  • timeout_sec – [in] how long to wait for the sensor to initialize.

Returns

pointer owning the resources associated with the connection.

std::shared_ptr<client> mtp_init_client(const std::string &hostname, const sensor_config &config, const std::string &mtp_dest_host, bool main, int timeout_sec = 60)

[BETA] Connect to and configure the sensor and start listening for data via multicast.

Remark

when main flag is set the config object will be used to configure the sensor, otherwise only the port values within the config object will be used and the rest will be ignored.

Parameters
  • hostname – [in] hostname or ip of the sensor.

  • config – [in] sensor config to set on sensor.

  • mtp_dest_host – [in] multicast ip address where the sensor should send data.

  • main – [in] a flag that indicates this is the main connection to the sensor in an multicast setup.

  • timeout_sec – [in] how long to wait for the sensor to initialize.

Returns

pointer owning the resources associated with the connection.

Data Fetching

client_state ouster::sensor::poll_client(const client &cli, int timeout_sec = 1)

Block for up to timeout_sec until either data is ready or an error occurs.

NOTE: will return immediately if LIDAR_DATA or IMU_DATA are set and not cleared by read_lidar_data() and read_imu_data() before the next call.

Parameters
  • cli – [in] client returned by init_client associated with the connection.

  • timeout_sec – [in] seconds to block while waiting for data.

Returns

client_state s where (s & ERROR) is true if an error occured, (s & LIDAR_DATA) is true if lidar data is ready to read, and (s & IMU_DATA) is true if imu data is ready to read.

bool ouster::sensor::read_lidar_packet(const client &cli, uint8_t *buf, const packet_format &pf)

Read lidar data from the sensor. Will not block.

Parameters
  • cli – [in] client returned by init_client associated with the connection.

  • buf – [out] buffer to which to write lidar data. Must be at least lidar_packet_bytes + 1 bytes.

  • pf – [in] The packet format.

Returns

true if a lidar packet was successfully read.

bool ouster::sensor::read_imu_packet(const client &cli, uint8_t *buf, const packet_format &pf)

Read imu data from the sensor. Will not block.

Parameters
  • cli – [in] client returned by init_client associated with the connection.

  • buf – [out] buffer to which to write imu data. Must be at least imu_packet_bytes + 1 bytes.

  • pf – [in] The packet format.

Returns

true if an imu packet was successfully read.

Config And Metadata

std::string ouster::sensor::get_metadata(client &cli, int timeout_sec = 60, bool legacy_format = false)

Get metadata text blob from the sensor.

Will attempt to fetch from the network if not already populated.

Throws

runtime_error – if the sensor is in ERROR state, the firmware version used to initialize the HTTP or TCP client is invalid, the metadata could not be retrieved from the sensor, or the response could not be parsed.

Parameters
  • cli – [in] client returned by init_client associated with the connection.

  • timeout_sec – [in] how long to wait for the sensor to initialize.

  • legacy_format – [in] whether to use legacy format of metadata output.

Returns

a text blob of metadata parseable into a sensor_info struct.

bool ouster::sensor::get_config(const std::string &hostname, sensor_config &config, bool active = true)

Get sensor config from the sensor.

Populates passed in config with the results of get_config.

Parameters
  • hostname – [in] sensor hostname.

  • config – [out] sensor config to populate.

  • active – [in] whether to pull active or passive configs.

Returns

true if sensor config successfully populated.

bool ouster::sensor::set_config(const std::string &hostname, const sensor_config &config, uint8_t config_flags = 0)

Set sensor config on sensor.

Throws
  • runtime_error – on failure to communcate with the sensor.

  • invalid_argument – when config parameters fail validation.

Parameters
  • hostname – [in] sensor hostname.

  • config – [in] sensor config.

  • config_flags – [in] flags to pass in.

Returns

true if config params successfuly set on sensor.

enum ouster::sensor::config_flags

Flags for set_config()

Values:

enumerator CONFIG_UDP_DEST_AUTO

Set udp_dest automatically.

enumerator CONFIG_PERSIST

Make configuration persistent.

enumerator CONFIG_FORCE_REINIT

Forces the sensor to re-init during set_config even when config params have not changed

Network Operations

int ouster::sensor::get_lidar_port(client &cli)

Return the port used to listen for lidar UDP data.

Parameters

cli – [in] client returned by init_client associated with the connection.

Returns

the port number.

int ouster::sensor::get_imu_port(client &cli)

Return the port used to listen for imu UDP data.

Parameters

cli – [in] client returned by init_client associated with the connection.

Returns

the port number.

enum ouster::sensor::client_state

Returned by poll_client.

Values:

enumerator TIMEOUT

Client has timed out.

enumerator CLIENT_ERROR

Client has reported an error.

enumerator LIDAR_DATA

New lidar data available.

enumerator IMU_DATA

New IMU data available.

enumerator EXIT

Client has exited.