async_writer.h

Class

class AsyncWriter

OSF AsyncWriter wraps osf::Writer so that saving occurs in a background thread. Calls to save() return a std::future<void> instead of void to enable propagating exceptions from the save thread.

Public Functions

AsyncWriter(const std::string &filename, const std::vector<ouster::sensor::sensor_info> &info, const std::vector<std::string> &fields_to_write = std::vector<std::string>(), uint32_t chunk_size = 0, std::shared_ptr<Encoder> encoder = nullptr)
Parameters:
  • filename – [in] The filename to output to.

  • info – [in] The sensor info vector to use for a multi stream OSF file.

  • fields_to_write – [in] The fields from scans to actually save into the OSF. If not provided uses the fields from the first saved lidar scan for this sensor. This parameter is optional.

  • chunk_size – [in] The chunksize to use for the OSF file, this parameter is optional.

  • encoder – [in] An optional Encoder instance for configuring how the Writer should encode the OSF.

~AsyncWriter()

Closes the writer and finalizes any pending writes.

std::future<void> save(uint32_t stream_index, const LidarScan &scan)

Save a single scan to the specified stream_index in an OSF file.

The concept of the stream_index is related to the sensor_info vector. Consider the following:

sensor_info info1; // The first sensor in this OSF file
sensor_info info2; // The second sensor in this OSF file
sensor_info info3; // The third sensor in this OSF file

Writer output = Writer(filename, {info1, info2, info3});

LidarScan scan = RANDOM_SCAN_HERE;

// To save the LidarScan of scan to the first sensor, you would do the
// following
output.save(0, scan);

// To save the LidarScan of scan to the second sensor, you would do the
// following
output.save(1, scan);

// To save the LidarScan of scan to the third sensor, you would do the
// following
output.save(2, scan);

Throws:
  • std::logic_error – Will throw exception on writer being closed.

  • std::logic_error – ///< Will throw exception on ///< out of bound stream_index.

Parameters:
  • stream_index – [in] The index of the corrosponding sensor_info to use.

  • scan – [in] The scan to save.

Returns:

a future, which can propagate exceptions that may have occurred in the background from the save thread.

std::future<void> save(uint32_t stream_index, const LidarScan &scan, ouster::osf::ts_t timestamp)

Save a single scan with the specified timestamp to the specified stream_index in an OSF file.

Throws:
  • std::logic_error – Will throw exception on writer being closed.

  • std::logic_error – ///< Will throw exception on ///< out of bound stream_index.

Parameters:
  • stream_index – [in] The index of the corrosponding sensor_info to use.

  • scan – [in] The scan to save.

  • timestamp – [in] Receive timestamp to index this scan with.

Returns:

a future, which can propagate exceptions that may have occurred in the background from the save thread.

std::vector<std::future<void>> save(const std::vector<LidarScan> &scans)

Save multiple scans to the OSF file.

The concept of the stream_index is related to the sensor_info vector. Consider the following:

sensor_info info1; // The first sensor in this OSF file
sensor_info info2; // The second sensor in this OSF file
sensor_info info3; // The third sensor in this OSF file

Writer output = Writer(filename, {info1, info2, info3});

LidarScan sensor1_scan = RANDOM_SCAN_HERE;
LidarScan sensor2_scan = RANDOM_SCAN_HERE;
LidarScan sensor3_scan = RANDOM_SCAN_HERE;

// To save the scans matched appropriately to their sensors, you would do
// the following
output.save({sensor1_scan, sensor2_scan, sensor3_scan});

Throws:

std::logic_error – Will throw exception on writer being closed

Parameters:

scans – [in] The vector of scans to save.

Returns:

a vector of futures, which can propagate exceptions that may have occurred in the background from the save thread.

void close()

Finish file with a proper metadata object, and header. This method blocks until all remaining tasks generated by save() have been finalized.

Structs

struct LidarScanMessage

Encapsulates everything that’s needed to encode and save the provided lidar scan into the OSF.