types.h

Enums

enum ouster::sensor::lidar_mode

Constants used for configuration. Refer to the sensor documentation for the meaning of each option.

Values:

enumerator MODE_UNSPEC

lidar mode: unspecified

enumerator MODE_512x10

lidar mode: 10 scans of 512 columns per second

enumerator MODE_512x20

lidar mode: 20 scans of 512 columns per second

enumerator MODE_1024x10

lidar mode: 10 scans of 1024 columns per second

enumerator MODE_1024x20

lidar mode: 20 scans of 1024 columns per second

enumerator MODE_2048x10

lidar mode: 10 scans of 2048 columns per second

enumerator MODE_4096x5

lidar mode: 5 scans of 4096 columns per second. Only available on select sensors

enum ouster::sensor::timestamp_mode

Mode controlling timestamp method. Refer to the sensor documentation for the meaning of each option.

Values:

enumerator TIME_FROM_UNSPEC

Timestamp mode unspecified.

enumerator TIME_FROM_INTERNAL_OSC

Use the internal clock.

enumerator TIME_FROM_SYNC_PULSE_IN

A free running counter synced to the SYNC_PULSE_IN input counts seconds (# of pulses) and nanoseconds since sensor turn on.

enumerator TIME_FROM_PTP_1588

Synchronize with an external PTP master.

enum ouster::sensor::timestamp_mode

Mode controlling timestamp method. Refer to the sensor documentation for the meaning of each option.

Values:

enumerator TIME_FROM_UNSPEC

Timestamp mode unspecified.

enumerator TIME_FROM_INTERNAL_OSC

Use the internal clock.

enumerator TIME_FROM_SYNC_PULSE_IN

A free running counter synced to the SYNC_PULSE_IN input counts seconds (# of pulses) and nanoseconds since sensor turn on.

enumerator TIME_FROM_PTP_1588

Synchronize with an external PTP master.

enum ouster::sensor::OperatingMode

Mode controlling sensor operation. Refer to the sensor documentation for the meaning of each option.

Values:

enumerator OPERATING_UNSPEC

Unspecified sensor operation.

enumerator OPERATING_NORMAL

Normal sensor operation.

enumerator OPERATING_STANDBY

Standby.

enum ouster::sensor::MultipurposeIOMode

Mode controlling ways to input timesync information. Refer to the sensor documentation for the meaning of each option.

Values:

enumerator MULTIPURPOSE_OFF

Multipurpose IO is turned off (default)

enumerator MULTIPURPOSE_INPUT_NMEA_UART

Used in conjunction with timestamp_mode::TIME_FROM_SYNC_PULSE_IN to enable time pulses in on the multipurpose io input.

enumerator MULTIPURPOSE_OUTPUT_FROM_INTERNAL_OSC

Output a SYNC_PULSE_OUT signal synchronized with the internal clock.

enumerator MULTIPURPOSE_OUTPUT_FROM_SYNC_PULSE_IN

Output a SYNC_PULSE_OUT signal synchronized with a SYNC_PULSE_IN provided to the unit.

enumerator MULTIPURPOSE_OUTPUT_FROM_PTP_1588

Output a SYNC_PULSE_OUT signal synchronized with an external PTP IEEE 1588 master.

enumerator MULTIPURPOSE_OUTPUT_FROM_ENCODER_ANGLE

Output a SYNC_PULSE_OUT signal with a user defined rate in an integer number of degrees.

enum ouster::sensor::Polarity

Polarity represents polarity of NMEA UART and SYNC_PULSE inputs and outputs. See sensor docs for more details.

Values:

enumerator POLARITY_ACTIVE_LOW

ACTIVE_LOW.

enumerator POLARITY_ACTIVE_HIGH

ACTIVE_HIGH.

enum ouster::sensor::NMEABaudRate

Baud rate the sensor attempts for NMEA UART input $GPRMC messages See sensor docs for more details.

Values:

enumerator BAUD_9600

9600 bits per second UART baud rate

enumerator BAUD_115200

115200 bits per second UART baud rate

enum ouster::sensor::UDPProfileLidar

Profile indicating packet format of lidar data.

Values:

enumerator PROFILE_LIDAR_UNKNOWN
enumerator PROFILE_LIDAR_LEGACY

Legacy lidar data

enumerator PROFILE_RNG19_RFL8_SIG16_NIR16_DUAL

Dual Returns data

enumerator PROFILE_RNG19_RFL8_SIG16_NIR16

Single Returns data

enumerator PROFILE_RNG15_RFL8_NIR8

Single Returns Low Data Rate

enumerator PROFILE_FIVE_WORD_PIXEL

Five Word Profile

enumerator PROFILE_FUSA_RNG15_RFL8_NIR8_DUAL

FuSa two-word pixel

enum ouster::sensor::UDPProfileIMU

Profile indicating packet format of IMU data.

Values:

enumerator PROFILE_IMU_LEGACY

Legacy IMU data.

enum ouster::sensor::FullScaleRange

Full scale range for IMU data.

Values:

enumerator FSR_NORMAL

Higher precision lower range measurement mode

enumerator FSR_EXTENDED

Lower precision higher range measurement mode

enum ouster::sensor::ReturnOrder

Priority of returns for the lidar to output. Lidar can have more than 1 or 2 detected “returns”. This indicates to the lidar which ones it should output. See sensor docs for more details.

Values:

enumerator ORDER_STRONGEST_TO_WEAKEST

Lidar returns the strongest returns first

enumerator ORDER_FARTHEST_TO_NEAREST

Lidar returns the furthest returns first

enumerator ORDER_NEAREST_TO_FARTHEST

Lidar returns the nearest returns first

enumerator ORDER_DEPRECATED_STRONGEST_RETURN_FIRST

DEPRECATED: Only Present In Old Test Firmware

enumerator ORDER_DEPRECATED_LAST_RETURN_FIRST
enum ouster::sensor::ThermalShutdownStatus

Thermal Shutdown status.

Values:

enumerator THERMAL_SHUTDOWN_NORMAL

Normal operation.

enumerator THERMAL_SHUTDOWN_IMMINENT

Thermal Shutdown imminent.

enum ouster::sensor::ShotLimitingStatus

Shot Limiting status.

Values:

enumerator SHOT_LIMITING_NORMAL

Normal operation.

enumerator SHOT_LIMITING_IMMINENT

Shot limiting imminent.

enumerator SHOT_LIMITING_REDUCTION_0_10

Shot limiting reduction by 0 to 10%.

enumerator SHOT_LIMITING_REDUCTION_10_20

Shot limiting reduction by 10 to 20%.

enumerator SHOT_LIMITING_REDUCTION_20_30

Shot limiting reduction by 20 to 30%.

enumerator SHOT_LIMITING_REDUCTION_30_40

Shot limiting reduction by 30 to 40%.

enumerator SHOT_LIMITING_REDUCTION_40_50

Shot limiting reduction by 40 to 50%.

enumerator SHOT_LIMITING_REDUCTION_50_60

Shot limiting reduction by 50 to 60%.

enumerator SHOT_LIMITING_REDUCTION_60_70

Shot limiting reduction by 60 to 70%.

enumerator SHOT_LIMITING_REDUCTION_70_75

Shot limiting reduction by 70 to 80%.

enum ouster::sensor::ChanFieldType

Types of channel fields.

Values:

enumerator VOID
enumerator UINT8
enumerator UINT16
enumerator UINT32
enumerator UINT64
enumerator INT8
enumerator INT16
enumerator INT32
enumerator INT64
enumerator FLOAT32
enumerator FLOAT64
enumerator UNREGISTERED

Variables

double ouster::sensor::range_unit = 0.001

Unit of range from sensor packet, in meters.

const std::vector<double> ouster::sensor::gen1_altitude_angles

Design values for altitude and azimuth offset angles for gen1 sensors.

const std::vector<double> ouster::sensor::gen1_azimuth_angles

Design values for altitude and azimuth offset angles for gen1 sensors.

const mat4d ouster::sensor::default_imu_to_sensor_transform

Design values for imu and lidar to sensor-frame transforms.

const mat4d ouster::sensor::default_lidar_to_sensor_transform

Design values for imu and lidar to sensor-frame transforms.

Class

class packet_format

Table of accessors for extracting data from imu and lidar packets.

In the user guide, refer to section 9 for the lidar packet format and section 10 for imu packets.

For 0 <= n < columns_per_packet, nth_col(n, packet_buf) returns a pointer to the nth measurement block. For 0 <= m < pixels_per_column, nth_px(m, col_buf) returns the mth channel data block.

Use imu_la_{x,y,z} to access the acceleration in the corresponding direction. Use imu_av_{x,y,z} to read the angular velocity.

Public Types

FieldIter = decltype(field_types_)::const_iterator

iterator over field types of packet

Public Functions

uint16_t packet_type(const uint8_t *lidar_buf) const

Read the packet type packet header.

Parameters:

lidar_buf – [in] the lidar buf.

Returns:

the packet type.

uint32_t frame_id(const uint8_t *lidar_buf) const

Read the frame_id packet header.

Parameters:

lidar_buf – [in] the lidar buf.

Returns:

the frame id.

uint32_t init_id(const uint8_t *lidar_buf) const

Read the initialization id packet header.

Parameters:

lidar_buf – [in] the lidar buf.

Returns:

the init id.

uint64_t prod_sn(const uint8_t *lidar_buf) const

Read the packet serial number header.

Parameters:

lidar_buf – [in] the lidar buf.

Returns:

the serial number.

uint8_t alert_flags(const uint8_t *lidar_buf) const

Read the alert flags.

Parameters:

lidar_buf – [in] the lidar buf.

Returns:

the alert flags byte.

uint16_t countdown_thermal_shutdown(const uint8_t *lidar_buf) const

Read the packet thermal shutdown countdown

Parameters:

lidar_buf – [in] the lidar buf.

Returns:

the thermal shutdown countdown.

uint16_t countdown_shot_limiting(const uint8_t *lidar_buf) const

Read the packet shot limiting countdown

Parameters:

lidar_buf – [in] the lidar buf.

Returns:

the shot limiting countdown.

uint8_t thermal_shutdown(const uint8_t *lidar_buf) const

Read the packet thermal shutdown header.

Parameters:

lidar_buf – [in] the lidar buf.

Returns:

the thermal shutdown status

uint8_t shot_limiting(const uint8_t *lidar_buf) const

Read the packet shot limiting header.

Parameters:

lidar_buf – [in] the lidar buf.

Returns:

the shot limiting status

ChanFieldType field_type(const std::string &f) const

Get the bit width of the specified channel field.

Parameters:

f – [in] the channel field to query.

Returns:

a type tag specifying the bitwidth of the requested field or ChannelFieldType::VOID if it is not supported by the packet format.

FieldIter begin() const

A const forward iterator over field / type pairs.

Returns:

Iterator pointing to the first element in the field type of packets.

FieldIter end() const

A const forward iterator over field / type pairs.

Returns:

Iterator pointing to the last element in the field type of packets.

const uint8_t *footer(const uint8_t *lidar_buf) const

Get pointer to the packet footer of a lidar buffer.

Parameters:

lidar_buf – [in] the lidar buffer.

Returns:

pointer to packet footer of lidar buffer, can be nullptr if packet format doesn’t have packet footer.

const uint8_t *nth_col(int n, const uint8_t *lidar_buf) const

Get pointer to nth column of a lidar buffer.

Parameters:
  • n – [in] which column.

  • lidar_buf – [in] the lidar buffer.

Returns:

pointer to nth column of lidar buffer.

uint64_t col_timestamp(const uint8_t *col_buf) const

Read column timestamp from column buffer.

Parameters:

col_buf – [in] the column buffer.

Returns:

column timestamp.

uint16_t col_measurement_id(const uint8_t *col_buf) const

Read measurement id from column buffer.

Parameters:

col_buf – [in] the column buffer.

Returns:

column measurement id.

uint32_t col_status(const uint8_t *col_buf) const

Read column status from column buffer.

Parameters:

col_buf – [in] the column buffer.

Returns:

column status.

uint32_t col_encoder(const uint8_t *col_buf) const

Encodes the column value.

This function encodes the column value.

Deprecated:

Use col_measurement_id instead. This function will be removed in future versions.

Deprecated:

Encoder count is deprecated as it is redundant with measurement id, barring a multiplication factor which varies by lidar mode. Use col_measurement_id instead

Parameters:

col_buf – [in] A measurement block pointer returned by nth_col().

Returns:

Encoded column value.

uint16_t col_frame_id(const uint8_t *col_buf) const

Retrieves the current frame id.

This function returns the frame id of a column

Deprecated:

Use frame_id instead. This function will be removed in future versions.

Deprecated:

Use frame_id instead

Parameters:

col_buf – [in] A measurement block pointer returned by nth_col().

Returns:

The current frame id.

template<typename T>
void col_field(const uint8_t *col_buf, const std::string &f, T *dst, int dst_stride = 1) const

Copy the specified channel field out of a packet measurement block.

Template Parameters:

T – T should be a numeric type large enough to store values of the specified field. Otherwise, data will be truncated.

Parameters:
  • col_buf – [in] a measurement block pointer returned by nth_col().

  • f – [in] the channel field to copy.

  • dst – [out] destination array of size pixels_per_column * dst_stride.

  • dst_stride – [in] stride for writing to the destination array.

int block_parsable() const

Returns maximum available size of parsing block usable with block_field

Returns:

if packet format does not allow for block parsing, returns 0

template<typename T, int BlockDim>
void block_field(Eigen::Ref<img_t<T>> field, const std::string &f, const uint8_t *lidar_buf) const

Copy the specified channel field out of a packet measurement block. Faster traversal than col_field, but has to copy the entire packet all at once.

Template Parameters:

T – T should be a numeric type large enough to store values of the specified field. Otherwise, data will be truncated.

Parameters:
  • field – [out] destination eigen array

  • f – [in] the channel field to copy.

  • lidar_buf – [in] the lidar buffer.

const uint8_t *nth_px(int n, const uint8_t *col_buf) const

Get pointer to nth pixel of a column buffer.

Parameters:
  • n – [in] which pixel.

  • col_buf – [in] the column buffer.

Returns:

pointer to nth pixel of a column buffer.

uint64_t imu_sys_ts(const uint8_t *imu_buf) const

Read sys ts from imu packet buffer.

Parameters:

imu_buf – [in] the imu packet buffer.

Returns:

sys ts from imu pacet buffer.

uint64_t imu_accel_ts(const uint8_t *imu_buf) const

Read acceleration timestamp.

Parameters:

imu_buf – [in] the imu packet buffer.

Returns:

acceleration ts from imu packet buffer.

uint64_t imu_gyro_ts(const uint8_t *imu_buf) const

Read gyro timestamp.

Parameters:

imu_buf – [in] the imu packet buffer.

Returns:

gyro ts from imu packet buffer.

float imu_la_x(const uint8_t *imu_buf) const

Read acceleration in x.

Parameters:

imu_buf – [in] the imu packet buffer.

Returns:

acceleration in x.

float imu_la_y(const uint8_t *imu_buf) const

Read acceleration in y.

Parameters:

imu_buf – [in] the imu packet buffer.

Returns:

acceleration in y.

float imu_la_z(const uint8_t *imu_buf) const

Read acceleration in z.

Parameters:

imu_buf – [in] the imu packet buffer.

Returns:

acceleration in z.

float imu_av_x(const uint8_t *imu_buf) const

Read angular velocity in x.

Parameters:

imu_buf – [in] the imu packet buffer.

Returns:

angular velocity in x.

float imu_av_y(const uint8_t *imu_buf) const

Read angular velocity in y.

Parameters:

imu_buf – [in] the imu packet buffer.

Returns:

angular velocity in y.

float imu_av_z(const uint8_t *imu_buf) const

Read angular velocity in z.

Parameters:

imu_buf – [in] the imu packet buffer.

Returns:

angular velocity in z.

uint64_t field_value_mask(const std::string &f) const

Get the mask of possible values that can be parsed by the channel field

Parameters:

f – [in] the channel field

Returns:

mask of possible values

int field_bitness(const std::string &f) const

Get number of bits in the channel field

Parameters:

f – [in] the channel field

Returns:

number of bits

optional<uint64_t> crc(const uint8_t *lidar_buf) const

Return the CRC contained in the packet if present

Parameters:

lidar_buf – [in] the lidar buffer.

Returns:

crc contained in the packet if present

uint64_t calculate_crc(const uint8_t *lidar_buf) const

Calculate the CRC for the given packet.

Parameters:

lidar_buf – [in] the lidar buffer.

Returns:

calculated crc of the packet

Public Members

const UDPProfileLidar udp_profile_lidar

udp lidar profile of packet format

const size_t lidar_packet_size

lidar packet size

const size_t imu_packet_size

imu packet size

const int columns_per_packet

columns per lidar packet

const int pixels_per_column

pixels per column for lidar

class product_info

Stores parsed information about the prod line

Public Functions

product_info()

Default constructor for product_info that sets everything to blank.

Public Members

const std::string full_product_info

The original full product line string.

const std::string form_factor

The form factor of the sensor. This will look like: “OS1” or “OS2” and such.

const bool short_range

Is the sensor a short range build or not.

const std::string beam_config

The beam configuration of the sensor.

const int beam_count

The number of beams on the sensor.

Public Static Functions

static product_info create_product_info(std::string product_info_string)

Static method used to create product_info classes.

Throws:

std::runtime_error – on a bad product info line.

Parameters:

product_info_string – [in] The product info string to create the product_info class from.

Returns:

The new product_info class.

class sensor_info

Stores parsed information from metadata.

Public Functions

std::string to_json_string() const

Return an updated version of the metadata string reflecting any changes to the sensor_info. Errors out if changes are incompatible but does not check for validity

Returns:

json serialized version of this object

ouster::util::version get_version() const

Parse and return version info about this sensor.

Returns:

sensor version info

int num_returns() const

Get the number of returns output by the sensor in its current setup.

Returns:

number of returns

decltype(format.columns_per_frame) w() const

returns the width of a frame (equivalent to format.columns_per_frame)

Retrieves the width of a frame

Returns:

width of a frame.

decltype(format.pixels_per_column) h() const

returns the height of a frame (equivalent to format.pixels_per_column)

Retrieves the height of a frame

Returns:

height of a frame.

Public Members

uint64_t sn = {}

sensor serial number corresponding to prod_sn in metadata.json

std::string fw_rev = {}

fw revision corresponding to build_rev in metadata.json

std::string prod_line = {}

prod line

data_format format = {}

data format of sensor

std::vector<double> beam_azimuth_angles = {}

beam azimuth angles for 3D projection

std::vector<double> beam_altitude_angles = {}

beam altitude angles for 3D projection

double lidar_origin_to_beam_origin_mm = {}

distance between lidar origin and beam origin in mm

mat4d beam_to_lidar_transform = mat4d::Zero()

transform between beam and lidar frame

mat4d imu_to_sensor_transform = mat4d::Zero()

transform between sensor coordinate frame and imu

mat4d lidar_to_sensor_transform = mat4d::Zero()

transform between lidar and sensor coordinate frames

mat4d extrinsic = mat4d::Zero()

user-convenience client-side assignable extrinsic matrix, currently is not read from metadata.json

uint32_t init_id = {}

initialization ID updated every reinit

std::string build_date = {}

build date from FW sensor_info

std::string image_rev = {}

image rev from FW sensor_info

std::string prod_pn = {}

prod pn

std::string status = {}

sensor status at time of pulling metadata

calibration_status cal = {}

sensor calibration

sensor_config config = {}

parsed sensor config if available from metadata

std::string user_data = {}

userdata from sensor if available

Structs

struct calibration_status

Stores from-sensor calibration information

struct data_format

Stores data format information.

Public Functions

int valid_columns_per_frame() const

Return the number of valid columns per complete frame of data with the column_window applied.

Returns:

the number of columns

int packets_per_frame() const

Return the number of valid packets actually sent per frame of data with the column_window applied.

Returns:

the number of packets

Public Members

uint32_t pixels_per_column

pixels per column

uint32_t columns_per_packet

columns per packet

uint32_t columns_per_frame

columns per frame, should match with lidar mode

std::vector<int> pixel_shift_by_row

shift of pixels by row to enable destagger

ColumnWindow column_window

window of columns over which sensor fires

UDPProfileLidar udp_profile_lidar = {}

profile of lidar packet

UDPProfileIMU udp_profile_imu = {}

profile of imu packet

uint16_t fps

frames per second

struct sensor_config

Struct for sensor configuration parameters.

Public Members

optional<std::string> udp_dest

The destination address for the lidar/imu data to be sent to

optional<uint16_t> udp_port_lidar

The destination port for the lidar data to be sent to

optional<uint16_t> udp_port_imu

The destination port for the imu data to be sent to

optional<sensor::timestamp_mode> timestamp_mode

The timestamp mode for the sensor to use. Refer to timestamp_mode for more details.

optional<sensor::lidar_mode> lidar_mode

The lidar mode for the sensor to use. Refer to lidar_mode for more details.

optional<OperatingMode> operating_mode

The operating mode for the sensor to use. Refer to OperatingMode for more details.

optional<MultipurposeIOMode> multipurpose_io_mode

The multipurpose io mode for the sensor to use. Refer to MultipurposeIOMode for more details.

optional<AzimuthWindow> azimuth_window

The azimuth window for the sensor to use. Refer to AzimuthWindow for more details.

optional<double> signal_multiplier

Multiplier for signal strength of sensor. See the sensor docs for more details on usage.

optional<Polarity> nmea_in_polarity

The nmea polarity for the sensor to use. Refer to Polarity for more details.

optional<bool> nmea_ignore_valid_char

Whether NMEA UART input $GPRMC messages should be ignored. Refer to the sensor docs for more details.

optional<NMEABaudRate> nmea_baud_rate

The nmea baud rate for the sensor to use. Refer to Polarity> for more details.

optional<int> nmea_leap_seconds

Number of leap seconds added to UDP timestamp. See the sensor docs for more details.

optional<Polarity> sync_pulse_in_polarity

Polarity of SYNC_PULSE_IN input. See Polarity for more details.

optional<Polarity> sync_pulse_out_polarity

Polarity of SYNC_PULSE_OUT output. See Polarity for more details.

optional<int> sync_pulse_out_angle

Angle in degrees that sensor traverses between each SYNC_PULSE_OUT pulse. See senor docs for more details.

optional<int> sync_pulse_out_pulse_width

Width of SYNC_PULSE_OUT pulse in ms. See sensor docs for more details.

optional<int> sync_pulse_out_frequency

Frequency of SYNC_PULSE_OUT pulse in Hz. See sensor docs for more details.

optional<bool> phase_lock_enable

Whether phase locking is enabled. See sensor docs for more details.

optional<int> phase_lock_offset

Angle that sensors are locked to in millidegrees. See sensor docs for more details.

optional<int> columns_per_packet

Columns per packet. See sensor docs for more details.

optional<UDPProfileLidar> udp_profile_lidar

The lidar profile for the sensor to use. Refer to UDPProfileLidar for more details.

optional<UDPProfileIMU> udp_profile_imu

The imu profile for the sensor to use. Refer to UDPProfileIMU for more details.

optional<FullScaleRange> gyro_fsr

The gyro full scale measurement range to use. Refer to FullScaleRange for more details.

optional<FullScaleRange> accel_fsr

The accelerometer full scale measurement range to use. Refer to FullScaleRange for more details.

optional<ReturnOrder> return_order

The priority of returns for the lidar to output. Refer to ReturnOrder for more details.

optional<int> min_range_threshold_cm

The minimum detection range of the lidar in cm.

std::map<std::string, std::string> extra_options

Extra config options to apply that arent in the standard set. Each value should be stringized json

Namespaces

namespace ChanField

Tag to identitify a paricular value reported in the sensor channel data block.

namespace ChanField

Variables

static cf_type RANGE = "RANGE"

1st return range in mm

static cf_type RANGE2 = "RANGE2"

2nd return range in mm

static cf_type SIGNAL = "SIGNAL"

1st return signal in photons

static cf_type SIGNAL2 = "SIGNAL2"

2nd return signal in photons

static cf_type REFLECTIVITY = "REFLECTIVITY"

sensitivity in FW 2.1+. See sensor docs for more details

1st return reflectivity, calibrated by range and sensor

static cf_type REFLECTIVITY2 = "REFLECTIVITY2"

sensitivity in FW 2.1+. See sensor docs for more details

2nd return reflectivity, calibrated by range and sensor

static cf_type NEAR_IR = "NEAR_IR"

near_ir in photons

static cf_type FLAGS = "FLAGS"

1st return flags

static cf_type FLAGS2 = "FLAGS2"

2nd return flags

static cf_type RAW_HEADERS = "RAW_HEADERS"

raw headers for packet/footer/column for dev use

static cf_type RAW32_WORD5 = "RAW32_WORD5"

raw word access to packet for dev use

static cf_type RAW32_WORD6 = "RAW32_WORD6"

raw word access to packet for dev use

static cf_type RAW32_WORD7 = "RAW32_WORD7"

raw word access to packet for dev use

static cf_type RAW32_WORD8 = "RAW32_WORD8"

raw word access to packet for dev use

static cf_type RAW32_WORD9 = "RAW32_WORD9"

raw word access to packet for dev use

static cf_type RAW32_WORD1 = "RAW32_WORD1"

raw word access to packet for dev use

static cf_type RAW32_WORD2 = "RAW32_WORD2"

raw word access to packet for dev use

static cf_type RAW32_WORD3 = "RAW32_WORD3"

raw word access to packet for dev use

static cf_type RAW32_WORD4 = "RAW32_WORD4"

raw word access to packet for dev use

Typedefs

template<typename T>
using ouster::img_t = Eigen::Array<T, -1, -1, Eigen::RowMajor>

For image operations.

Template Parameters:

T – The data type for the array.

using ouster::mat4d = Eigen::Matrix<double, 4, 4, Eigen::DontAlign>

Used for transformations.

using ouster::PointsD = PointsT<double>
using ouster::PointsF = PointsT<float>

Functions

Warning

doxygenfunction: Unable to resolve function “ouster::sensor::to_string” with arguments (const ouster::sensor::product_info&) in doxygen xml output for project “cpp_api” from directory: /ouster-sdk/docs/_build/latest/doctrees/xml. Potential matches:

- std::string to_string(AzimuthWindow azimuth_window)
- std::string to_string(ChanFieldType ft)
- std::string to_string(FullScaleRange full_scale_range)
- std::string to_string(MultipurposeIOMode mode)
- std::string to_string(NMEABaudRate rate)
- std::string to_string(OperatingMode mode)
- std::string to_string(Polarity polarity)
- std::string to_string(ReturnOrder return_order)
- std::string to_string(ShotLimitingStatus shot_limiting_status)
- std::string to_string(ThermalShutdownStatus thermal_shutdown_status)
- std::string to_string(UDPProfileIMU profile)
- std::string to_string(UDPProfileLidar profile)
- std::string to_string(const calibration_status &cal)
- std::string to_string(const product_info &info)
- std::string to_string(const sensor_config &config)
- std::string to_string(const sensor_info &info)
- std::string to_string(lidar_mode mode)
- std::string to_string(timestamp_mode mode)
std::string ouster::sensor::to_string(lidar_mode mode)

Get string representation of a lidar mode.

Parameters:

mode – [in] lidar_mode to get the string representation for.

Returns:

string representation of the lidar mode, or “UNKNOWN”.

lidar_mode ouster::sensor::lidar_mode_of_string(const std::string &s)

Get lidar mode from string.

Parameters:

s – [in] String to decode.

Returns:

lidar mode corresponding to the string, or 0 on error.

uint32_t ouster::sensor::n_cols_of_lidar_mode(lidar_mode mode)

Get number of columns in a scan for a lidar mode.

Parameters:

mode – [in] lidar_mode to get the number of columns for.

Returns:

number of columns per rotation for the mode.

int ouster::sensor::frequency_of_lidar_mode(lidar_mode mode)

Get the lidar rotation frequency from lidar mode.

Parameters:

mode – [in] Lidar mode to get the rotation frequency from.

Returns:

lidar rotation frequency in Hz.

std::string ouster::sensor::to_string(timestamp_mode mode)

Get string representation of a timestamp mode.

Parameters:

mode – [in] timestamp_mode to get the string representation for.

Returns:

string representation of the timestamp mode, or “UNKNOWN”.

timestamp_mode ouster::sensor::timestamp_mode_of_string(const std::string &s)

Get timestamp mode from string.

Parameters:

s – [in] String to decode into a timestamp mode.

Returns:

timestamp mode corresponding to the string, or 0 on error.

std::string ouster::sensor::to_string(OperatingMode mode)

Get string representation of an operating mode.

Parameters:

mode – [in] Operating mode to get the string representation from.

Returns:

string representation of the operating mode, or “UNKNOWN”.

optional<OperatingMode> ouster::sensor::operating_mode_of_string(const std::string &s)

Get operating mode from string.

Parameters:

s – [in] String to get the operating mode from.

Returns:

operating mode corresponding to the string, or 0 on error.

std::string ouster::sensor::to_string(MultipurposeIOMode mode)

Get string representation of a multipurpose io mode.

Parameters:

mode – [in] Multipurpose io mode to get a string representation from.

Returns:

string representation of the multipurpose io mode, or “UNKNOWN”.

optional<MultipurposeIOMode> ouster::sensor::multipurpose_io_mode_of_string(const std::string &s)

Get multipurpose io mode from string.

Parameters:

s – [in] String to decode into a multipurpose io mode.

Returns:

multipurpose io mode corresponding to the string, or 0 on error.

std::string ouster::sensor::to_string(Polarity polarity)

Get string representation of a polarity.

Parameters:

polarity – [in] The polarity to get the string representation of.

Returns:

string representation of the polarity, or “UNKNOWN”.

optional<Polarity> ouster::sensor::polarity_of_string(const std::string &s)

Get polarity from string.

Parameters:

s – [in] The string to decode into a polarity.

Returns:

polarity corresponding to the string, or 0 on error.

std::string ouster::sensor::to_string(NMEABaudRate rate)

Get string representation of a NMEA Baud Rate.

Parameters:

rate – [in] The NNEABaudRate to get the string representation of.

Returns:

string representation of the NMEA baud rate, or “UNKNOWN”.

optional<NMEABaudRate> ouster::sensor::nmea_baud_rate_of_string(const std::string &s)

Get nmea baud rate from string.

Parameters:

s – [in] The string to decode into a NMEA baud rate.

Returns:

nmea baud rate corresponding to the string, or 0 on error.

std::string ouster::sensor::to_string(AzimuthWindow azimuth_window)

Get string representation of an Azimuth Window.

Parameters:

azimuth_window – [in] The azimuth window to get the string representation. of

Returns:

string representation of the azimuth window.

std::string ouster::sensor::to_string(UDPProfileLidar profile)

Get string representation of a lidar profile.

Parameters:

profile – [in] The profile to get the string representation of.

Returns:

string representation of the lidar profile.

optional<UDPProfileLidar> ouster::sensor::udp_profile_lidar_of_string(const std::string &s)

Get lidar profile from string.

Parameters:

s – [in] The string to decode into a lidar profile.

Returns:

lidar profile corresponding to the string, or nullopt on error.

std::string ouster::sensor::to_string(UDPProfileIMU profile)

Get string representation of an IMU profile.

Parameters:

profile – [in] The profile to get the string representation of.

Returns:

string representation of the lidar profile.

optional<UDPProfileIMU> ouster::sensor::udp_profile_imu_of_string(const std::string &s)

Get imu profile from string

Parameters:

s – [in] The string to decode into an imu profile.

Returns:

imu profile corresponding to the string, or nullopt on error.

std::string ouster::sensor::to_string(FullScaleRange full_scale_range)

Get string representation of a Full Scale Range.

Parameters:

full_scale_range – [in] The shot limiting status to get the string representation of.

Returns:

string representation of the full scale range.

optional<FullScaleRange> ouster::sensor::full_scale_range_of_string(const std::string &s)

Get full scale range setting from string

Parameters:

s – [in] The string to decode into a full scale range.

Returns:

full scale range corresponding to the string, or nullopt on error.

optional<ReturnOrder> ouster::sensor::return_order_of_string(const std::string &s)

Get return order setting from string

Parameters:

s – [in] The string to decode into a return order.

Returns:

return order corresponding to the string, or nullopt on error.

std::string ouster::sensor::to_string(ReturnOrder return_order)

Get string representation of a Return Order.

Parameters:

return_order – [in] The return order to get the string representation of.

Returns:

string representation of the return order.

std::string ouster::sensor::to_string(ShotLimitingStatus shot_limiting_status)

Get string representation of a Shot Limiting Status.

Parameters:

shot_limiting_status – [in] The shot limiting status to get the string representation of.

Returns:

string representation of the shot limiting status.

std::string ouster::sensor::to_string(ThermalShutdownStatus thermal_shutdown_status)

Get string representation of Thermal Shutdown Status.

Parameters:

thermal_shutdown_status – [in] The thermal shutdown status to get the string representation of.

Returns:

string representation of thermal shutdown status.

void ouster::sensor::check_signal_multiplier(const double signal_multiplier)

Determine validity of provided signal multiplier value

Parameters:

signal_multiplier – [in] Signal multiplier value.

sensor_info ouster::sensor::metadata_from_json(const std::string &json_file, bool skip_beam_validation = false)

Parse metadata given path to a json file.

Throws:

runtime_error – if json file does not exist or is malformed.

Parameters:
  • json_file – [in] path to a json file containing sensor metadata.

  • skip_beam_validation – [in] whether to skip validation on metadata - not for use on recorded data or metadata from sensors

Returns:

a sensor_info struct populated with a subset of the metadata.

sensor_config ouster::sensor::parse_config(const std::string &config)

Parse config text blob from the sensor into a sensor_config struct.

All fields are optional, and will only be set if found.

Throws:

runtime_error – if the text is not valid json.

Parameters:

config – [in] a text blob given by get_config from client.h.

Returns:

a sensor_config struct populated with the sensor config. parameters.

Warning

doxygenfunction: Unable to resolve function “ouster::sensor::to_string” with arguments (const ouster::sensor::sensor_config&) in doxygen xml output for project “cpp_api” from directory: /ouster-sdk/docs/_build/latest/doctrees/xml. Potential matches:

- std::string to_string(AzimuthWindow azimuth_window)
- std::string to_string(ChanFieldType ft)
- std::string to_string(FullScaleRange full_scale_range)
- std::string to_string(MultipurposeIOMode mode)
- std::string to_string(NMEABaudRate rate)
- std::string to_string(OperatingMode mode)
- std::string to_string(Polarity polarity)
- std::string to_string(ReturnOrder return_order)
- std::string to_string(ShotLimitingStatus shot_limiting_status)
- std::string to_string(ThermalShutdownStatus thermal_shutdown_status)
- std::string to_string(UDPProfileIMU profile)
- std::string to_string(UDPProfileLidar profile)
- std::string to_string(const calibration_status &cal)
- std::string to_string(const product_info &info)
- std::string to_string(const sensor_config &config)
- std::string to_string(const sensor_info &info)
- std::string to_string(lidar_mode mode)
- std::string to_string(timestamp_mode mode)

Warning

doxygenfunction: Unable to resolve function “ouster::sensor::to_string” with arguments (const ouster::sensor::calibration_status&) in doxygen xml output for project “cpp_api” from directory: /ouster-sdk/docs/_build/latest/doctrees/xml. Potential matches:

- std::string to_string(AzimuthWindow azimuth_window)
- std::string to_string(ChanFieldType ft)
- std::string to_string(FullScaleRange full_scale_range)
- std::string to_string(MultipurposeIOMode mode)
- std::string to_string(NMEABaudRate rate)
- std::string to_string(OperatingMode mode)
- std::string to_string(Polarity polarity)
- std::string to_string(ReturnOrder return_order)
- std::string to_string(ShotLimitingStatus shot_limiting_status)
- std::string to_string(ThermalShutdownStatus thermal_shutdown_status)
- std::string to_string(UDPProfileIMU profile)
- std::string to_string(UDPProfileLidar profile)
- std::string to_string(const calibration_status &cal)
- std::string to_string(const product_info &info)
- std::string to_string(const sensor_config &config)
- std::string to_string(const sensor_info &info)
- std::string to_string(lidar_mode mode)
- std::string to_string(timestamp_mode mode)
std::string ouster::sensor::client_version()

Get client version.

Returns:

client version string

ouster::util::version ouster::sensor::firmware_version_from_metadata(const std::string &metadata)

Get version information from the metadata.

Parameters:

metadata – [in] string.

Returns:

version corresponding to the string, or invalid_version on error.

size_t ouster::sensor::field_type_size(ChanFieldType ft)

Get the size of the ChanFieldType in bytes.

Parameters:

ft – [in] the field type

Returns:

size of the field type in bytes

uint64_t ouster::sensor::field_type_mask(ChanFieldType ft)

Get the bit mask of the ChanFieldType.

Parameters:

ft – [in] the field type

Returns:

64 bit mask

std::string ouster::sensor::to_string(ChanFieldType ft)

Get string representation of a channel field.

Parameters:

ft – [in] The field type to get the string representation of.

Returns:

string representation of the channel field type.

Warning

doxygenfunction: Cannot find function “ouster::sensor::get_format” in doxygen xml output for project “cpp_api” from directory: /ouster-sdk/docs/_build/latest/doctrees/xml

Warning

doxygenfunction: Cannot find function “ouster::sensor::get_format” in doxygen xml output for project “cpp_api” from directory: /ouster-sdk/docs/_build/latest/doctrees/xml