meta_streaming_info.h

ChunkInfo

struct ChunkInfo

Class for keeping track of OSF chunks.

Flat Buffer Reference: fb/streaming/streaming_info.fbs :: ChunkInfo

Public Members

uint64_t offset

The offset in the flatbuffer where the chunk is located.

Flat Buffer Reference: fb/streaming/streaming_info.fbs :: ChunkInfo :: offset

uint32_t stream_id

The specific stream the chunk is associated with.

Flat Buffer Reference: fb/streaming/streaming_info.fbs :: ChunkInfo :: stream_id

uint32_t message_count

The number of messages in the chunk

Flat Buffer Reference: fb/streaming/streaming_info.fbs :: ChunkInfo :: message_count

std::string ouster::osf::to_string(const ChunkInfo &chunk_info)

Get the string representation for a ChunkInfo object.

Parameters:

chunk_info – [in] ChunkInfo object to be converted to string

Returns:

The string representation for a ChunkInfo object.