> This page is for Hardware, version Rev 7 (default).
> For other versions, use one of these documentation indexes:
> - Rev 7 (default): https://docs.ouster.com/sensor-docs/hardware/rev7/llms.txt
> - Rev 8: https://docs.ouster.com/sensor-docs/hardware/rev8/llms.txt

> For clean Markdown of any page, append .md to the page URL.
> For a complete documentation index, see https://docs.ouster.com/sensor-docs/llms.txt.
> For AI client integration (Claude Code, Cursor, etc.), connect to the MCP server at https://docs.ouster.com/sensor-docs/_mcp/server.

# Digital IO

> SYNC_PULSE_IN and MULTIPURPOSE_IO electrical interface requirements for Rev7 sensors.

## SYNC_PULSE_IN

`SYNC_PULSE_IN` is a dedicated input channel that is accessible from the Interface Box. This channel expects an input pulse sequence which can be used for time synchronization. Refer to the [Firmware User Manual](/sensor-docs/firmware) for more information on configuring this input. Any references to pulse polarity in this document references the signal polarity on the `SYNC_PULSE_IN` pin of the sensor. This input channel is protected by an opto-isolator which will draw 5mA at full operation.

*SYNC_PULSE_IN Interface Requirements*

| Parameter  | Min Voltage | Max Voltage | Min Driver Current                   |
| ---------- | ----------- | ----------- | ------------------------------------ |
| LOGIC LOW  | -30 V       | 2 V         | N/A                                  |
| LOGIC HIGH | 2.9 V       | 30 V        | 3mA @3.3V\~5V, 5mA at 24V and higher |

SYNC_PULSE_IN Interface requirements were tested with 2 m cable Interface Box connection at 2 MHz.

* When GPIO has 5 mA drive strength minimum, GPIO can be directly connected to the `SYNC_PULSE_IN` pin of the Interface Box header. This is the most common case and has been tested to work on common Arduino microcontroller series. Typical common logic levels of 3.3 V, 5 V GPIO of microcontrollers can produce drive strength of 5 mA min (Arduino, MSP430, etc.).
* If the 5 mA drive strength minimum cannot be met, a buffer circuit is required to drive `SYNC_PULSE_IN`. Example circuits are provided for common 3.3 V and 5 V logic.

![Example Circuit for 3.3 V](/sensor-docs/_fern-files/_img/05debaf96363ee9f1351648a46de5bef798b2e315a929b0271ad5701bbffdd88.webp)

Example Circuit for 3.3 V

![Example Circuit for 5 V logic](/sensor-docs/_fern-files/_img/f2cf437479975caab1bc144d262c5ff1613b028578387ea0b78e52cdaa902278.webp)

Example Circuit for 5 V logic

## MULTIPURPOSE_IO (MIO)

`MULTIPURPOSE_IO` (`MIO`) is a configurable input or output channel accessible from the Interface Box. Detailed information on how to configure this channel using the sensor TCP interface can be found in the [API guide](/sensor-docs/firmware/api-reference). By default this channel is disabled.

When this channel is configured as an **OUTPUT**, the `MIO` sends a pulse sequence that can be used for time synchronization or event triggering outside the sensor. For a full description of output pulse triggering options, refer to the [Firmware User Manual](/sensor-docs/firmware) for more information. This output is an opto-isolated open collector circuit, relying on an externally provided pull-up resistor. This resistor is provided for a typical 3.3V/5V application as part of the Interface Box circuitry.

*MULTIPURPOSE_IO - OUTPUT Interface Requirements*

| Parameter       | Min   | Max   |
| --------------- | ----- | ----- |
| Pull Up Voltage | 3.3 V | 24 V  |
| Sinking Current | N/A   | 25 mA |

When this channel is configured as an **INPUT**, the `MIO` can accept a standard NMEA \$GPRMC UART message. These messages are a common way for GPS systems to share timestamp information in UTC time format. More information on this packet structure and supported baud rates can be found in the [Time Synchronization](/sensor-docs/firmware/time-synchronization) section of the [Firmware User Manual](/sensor-docs/firmware).

*MULTIPURPOSE_IO - INPUT Interface Requirements*

| Parameter  | Min Voltage | Max Voltage | Min Driver Current                   |
| ---------- | ----------- | ----------- | ------------------------------------ |
| LOGIC LOW  | -30 V       | 2 V         | N/A                                  |
| LOGIC HIGH | 2.9 V       | 30 V        | 3mA @3.3V\~5V, 5mA at 24V and higher |

*Above are tested with a 35m (200uH inductance) Interface Box at 115200 Baud.*