> This page is for Integration Guides, version Rev 7 (default).
> For other versions, use one of these documentation indexes:
> - Rev 7 (default): https://docs.ouster.com/sensor-docs/guides/rev7/llms.txt
> - Rev 8: https://docs.ouster.com/sensor-docs/guides/rev8/llms.txt

> For clean Markdown of any page, append .md to the page URL.
> For a complete documentation index, see https://docs.ouster.com/sensor-docs/llms.txt.
> For AI client integration (Claude Code, Cursor, etc.), connect to the MCP server at https://docs.ouster.com/sensor-docs/_mcp/server.

# Thermal Integration Guide

> Overview and terminology for integrating Ouster sensors with custom heatsinks.

## Overview

The Ouster lidar sensors offers an industry-leading combination of price, performance, reliability, size, weight, and power. It is designed for indoor/outdoor all-weather environments and a long operating lifetime.

The Ouster family of sensors consist of three models, the OS0, OS1, and OS2, with differing beam configuration and vertical resolution, but identical mechanical dimensions.

The contents of this manual are applicable only to Rev 06 sensors. Please contact [support@ouster.io](mailto:support@ouster.io) with the sensor serial number to find out your sensor Rev information. For all other sensor hardware revisions, please refer to the respective [hardware user manual](https://ouster.com/downloads/).

### Terminology

For the purposes of this document, let us first establish some common terminology that will be used in this guide.

![The Sensor without any heatsink or mounting plates](/sensor-docs/_fern-files/_img/35b1cf020723f744b48be36e26cf659c00ebe778979a6a7ffe8c2a833807dbdf.webp)

**The Sensor** without any heatsink or mounting plates

![Heatsink Base](/sensor-docs/_fern-files/_img/1e43d0a45c42f018246114346ab25430ac9df263efeb4baa6025298e6ec0be37.webp)

**Heatsink Base** which doubles as the standard mounting plate.

![Heatsink Radial](/sensor-docs/_fern-files/_img/6eb888c27b247d59450f30607a73714c131a07831888372adfb7f3cc41d16bd8.webp)

**Heatsink Radial** is the radial finned heatsink modular cap.

![Heatsink Halo](/sensor-docs/_fern-files/_img/e92c021e93a7eda644a89f9799a09a96c639edfc10fcfac368ff52761be9f374.webp)

**Heatsink Halo** The halo finned heatsink modular cap. *Preferred* when application needs to reduce sharp edges.

![Heatsink Clamshell](/sensor-docs/_fern-files/_img/58d6587aefe500629fdf9e68b411b35fd96ab2910a97301af3b212ebd28adead.webp)

**Heatsink Clamshell** Is a reference heatsink for integrating into vehicles in locations that require tighter integration.

![Heatsink Clamshell with an Ouster Sensor](/sensor-docs/_fern-files/_img/15fd0e6f1d4577f1c7ed1a1df5aca30ba3ccece46e49c6404d5ef957e04f2fa0.webp)

**Heatsink Clamshell** with an Ouster Sensor.

![Top Cap, Window and Sensor Base](/sensor-docs/_fern-files/_img/c28d03dae5eace931b0121765d3ab1a3056f690ed75328493d3fb306cd4808c8.webp)

Top Cap, Window and Sensor Base

* **Top Cap** The top of the sensor, which accepts modular heatsinks such as the Heatsink-Radial, Heatsink-Halo and has mounting features for seamless integrations.

* **Window** The window through which the lasers are emitted.

* **Sensor Base** The base of the sensor which has the connector mounted to it.

| Term                  | Definition                                                                                                                                                                                                                   |
| --------------------- | ---------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------- |
| **Free Convection**   | The movement caused within a fluid by the tendency of hotter and therefore less denser material to rise, and colder, denser material to sink under the influence of gravity, which consequently results in transfer of heat. |
| **Stagnant Air**      | Air that is not moving other than by Free Convection.                                                                                                                                                                        |
| **Forced Convection** | The transfer of heat due to the bulk movement of fluid molecules over an object. The bulk movement can be due to wind, fan, vehicle motion, etc.                                                                             |

For the following reference tests in the [Thermotron SE-1000-6-6 Environmental Chamber](https://thermotron.com/equipment/se-series-detail/se-1000-6-6-environmental-chamber/), our **FORCED CONVECTION** flow rate is 1000 cubic feet per minute (CFM). This is approximately 0.5 m/s or 1.8 km/h of air speed. The air in this chamber flows from top to bottom.