> This page is for Integration Guides, version Rev 7 (default).
> For other versions, use one of these documentation indexes:
> - Rev 7 (default): https://docs.ouster.com/sensor-docs/guides/rev7/llms.txt
> - Rev 8: https://docs.ouster.com/sensor-docs/guides/rev8/llms.txt

> For clean Markdown of any page, append .md to the page URL.
> For a complete documentation index, see https://docs.ouster.com/sensor-docs/llms.txt.
> For AI client integration (Claude Code, Cursor, etc.), connect to the MCP server at https://docs.ouster.com/sensor-docs/_mcp/server.

# Performance Of Standard Design

> Where heat originates in Ouster sensors and how it dissipates through standard and clamshell heatsinks.

## Where does the heat come from?

There are two primary heat-dissipating assemblies in the sensor.

* The **Optical Turret** - containing the lasers and receivers.

* The **Base Assembly** - containing the computing, communication, and power.

The **Optical Turret** dissipates heat to both the `TOP CAP` and the `SENSOR BASE`. While, the `BASE ASSEMBLY` conducts most of its heat to the `SENSOR BASE`.

It is important in any sensor mounting integration design to accept heat from both the `TOP CAP` and `SENSOR BASE`.

Another important heat source factor to consider is the Sun. If the sensor will be operating in full sun you will need to account for the solar load (\~1000 W/m2). In our testing, solar load reduces the maximum operating temperature by approximately 8ºC.

Please see the [Sunshade Concept Design](/sensor-docs/guides/thermal-alerts#sunshade-concept-design) for inspiration on possible solutions.

## Where does the heat go?

### Standard Heatsinks

The sensor comes with two standard heatsinks attached to it.

* The base heatsink and mounting plate. (referred to as **HEATSINK-BASE**)

* The radial finned or halo heatsink modular caps. (referred to as **HEATSINK-RADIAL**, **HEATSINK-HALO**)

> **Note**
>
> Both have the same thermal performance.

It is also possible to create your own custom heatsinks for your specific integration, given that it adequately dissipates the heat from the sensor. For more information contact our [Support team](https://ouster.atlassian.net/servicedesk/customer/portal/8).

In the reference test conducted in the thermal chamber under **FORCED CONVECTION** (0.5 m/s) with the standard heatsinks, 38% of the heat is conducted into the **HEATSINK-BASE**.

While the remaining 62% of the heat convects to the air through the **HEATSINK-RADIAL**, **SENSOR BASE**, and **WINDOW**.

![Forced Convection With Standard Heatsink Heat Path](/sensor-docs/_fern-files/_img/61c26ae8b5bbdb1b20782718cc42588a28bfe02acd68bda10eae04807e39ab86.webp)

Forced Convection With Standard Heatsink Heat Path

Similarly, for **FREE CONVECTION** (Stagnant Air) in the thermal chamber with the standard heatsinks, 45% of the heat is conducted into the **HEATSINK-BASE**.

While the remaining 55% of the heat convects to the air through the **HEATSINK-RADIAL**, **SENSOR BASE**, and **WINDOW**.

![Stagnant Air with standard heatsink heat path](/sensor-docs/_fern-files/_img/a323b5c490547fe612ff6a247489dedf8cc12768680a8e8ae4d7fa5ccb3919b4.webp)

Stagnant Air with standard heatsink heat path

### Clamshell heatsink

The clamshell design was created to give you a reference of an integrated installation where heat dissipation is accomplished primarily through conduction into a vehicle chassis.

In the reference test conducted in the thermal chamber under **FREE CONVECTION** (Stagnant Air) with the clamshell heatsink, 87% of the heat is conducted into the **HEATSINK-CLAMSHELL**. While the remaining 13% of the heat convects to the air through the **HEATSINK-CLAMSHELL**, **SENSOR BASE** and **WINDOW**.

![Clamshell Heat Path](/sensor-docs/_fern-files/_img/c5b4f51ded533a1e93f2852d4eaa26a28a693f9c648f5e1ef8435adee3d106f6.webp)

Clamshell Heat Path

Now that you have a good understanding of where the heat goes, we will discuss some best practices when designing your own heatsinks and integrations.