# Validate zone set configuration

GET http://os-992244000006.local/api/v1/zone_monitor/{zone_set}/valid

Reference: https://docs.ouster.com/sensor-docs/firmware/api-reference/ouster-http-api/zone-monitor/validate-zone-set-configuration

## Request

### Path parameters

- `zone_set` (enum, required) — Zone set identifier. Valid values are 'active' or 'staged'. The 'pending' set is a transient state and should not be used.
  - Allowed values: `active`, `staged`

## Response

### 200

Validation result

- `valid` (boolean, optional, nullable) — True if valid, false if invalid, null if not configured
- `message` (string, optional) — Validation message or error details

## Examples

**Response**

```json
{
  "valid": true,
  "message": "Zone set 'active' configuration is valid with 12 zones configured."
}
```

**SDK Code**

```python
import requests

url = "http://os-992244000006.local/api/v1/zone_monitor/active/valid"

response = requests.get(url)

print(response.json())
```

```javascript
const url = 'http://os-992244000006.local/api/v1/zone_monitor/active/valid';
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
	url := "http://os-992244000006.local/api/v1/zone_monitor/active/valid"
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
url = URI("http://os-992244000006.local/api/v1/zone_monitor/active/valid")
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
HttpResponse<String> response = Unirest.get("http://os-992244000006.local/api/v1/zone_monitor/active/valid")
  .asString();
```

```php
<?php
require_once('vendor/autoload.php');

$client = new \GuzzleHttp\Client();

$response = $client->request('GET', 'http://os-992244000006.local/api/v1/zone_monitor/active/valid');

echo $response->getBody();
```

```csharp
using RestSharp;

var client = new RestClient("http://os-992244000006.local/api/v1/zone_monitor/active/valid");
var request = new RestRequest(Method.GET);
IRestResponse response = client.Execute(request);
```

```swift
import Foundation

let request = NSMutableURLRequest(url: NSURL(string: "http://os-992244000006.local/api/v1/zone_monitor/active/valid")! as URL,